Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
System Clock Management

See Quick Start Guide for the System Clock Management service (UC3L).

The sysclk API covers the system clock and all clocks derived from it. The system clock is a chip-internal clock on which all synchronous clocks, i.e. CPU and bus/peripheral clocks, are based. The system clock is typically generated from one of a variety of sources, which may include crystal and RC oscillators as well as PLLs. The clocks derived from the system clock are sometimes also known as synchronous clocks, since they always run synchronously with respect to each other, as opposed to generic clocks which may run from different oscillators or PLLs.

Most applications should simply call sysclk_init() to initialize everything related to the system clock and its source (oscillator, PLL or DFLL), and leave it at that. More advanced applications, and platform-specific drivers, may require additional services from the clock system, some of which may be platform-specific.

Platform Dependencies

The sysclk API is partially chip- or platform-specific. While all platforms provide mostly the same functionality, there are some variations around how different bus types and clock tree structures are handled.

The following functions are available on all platforms with the same parameters and functionality. These functions may be called freely by portable applications, drivers and services:

The following functions are available on all platforms, but there may be variations in the function signature (i.e. parameters) and behavior. These functions are typically called by platform-specific parts of drivers, and applications that aren't intended to be portable:

All other functions should be considered platform-specific. Enabling/disabling clocks to specific peripherals as well as determining the speed of these clocks should be done by calling functions provided by the driver for that peripheral.

Modules

 System Clock internals
 

Macros

#define CONFIG_SYSCLK_CPU_DIV   0
 Configuration symbol for dividing the CPU clock frequency by \(2^{CONFIG\_SYSCLK\_CPU\_DIV}\). More...
 
#define CONFIG_SYSCLK_INIT_CPUMASK
 Configuration symbol for the CPU clocks enabled at power-on after the sysclock module has been initialized. More...
 
#define CONFIG_SYSCLK_INIT_HSBMASK
 Configuration symbol for the HSB clocks enabled at power-on after the sysclock module has been initialized. More...
 
#define CONFIG_SYSCLK_INIT_PBAMASK
 Configuration symbol for the PBA clocks enabled at power-on after the sysclock module has been initialized. More...
 
#define CONFIG_SYSCLK_INIT_PBBMASK
 Configuration symbol for the PBB clocks enabled at power-on after the sysclock module has been initialized. More...
 
#define CONFIG_SYSCLK_PBA_DIV   0
 Configuration symbol for dividing the PBA clock frequency by \(2^{CONFIG\_SYSCLK\_PBA\_DIV}\). More...
 
#define CONFIG_SYSCLK_PBB_DIV   0
 Configuration symbol for dividing the PBB clock frequency by \(2^{CONFIG\_SYSCLK\_PBB\_DIV}\). More...
 
#define CONFIG_SYSCLK_SOURCE   SYSCLK_SRC_RCSYS
 
#define CONFIG_USBCLK_DIV
 Configuration symbol for the USB generic clock divider setting. More...
 
#define CONFIG_USBCLK_SOURCE
 Configuration symbol for the USB generic clock source. More...
 

Functions

void sysclk_priv_disable_module (unsigned int bus_id, unsigned int module_index)
 Disable a maskable module clock. More...
 
void sysclk_priv_enable_module (unsigned int bus_id, unsigned int module_index)
 Enable a maskable module clock. More...
 

System Clock Initialization

void sysclk_init (void)
 Initialize the synchronous clock system. More...
 

System clock source

#define SYSCLK_SRC_RCSYS   AVR32_PM_MCSEL_SLOW
 System RC oscillator. More...
 
#define SYSCLK_SRC_OSC0   AVR32_PM_MCSEL_OSC0
 Oscillator 0. More...
 
#define SYSCLK_SRC_DFLL   AVR32_PM_MCSEL_DFLL0
 Digital Frequency Locked Loop. More...
 
#define SYSCLK_SRC_RC120M   AVR32_PM_MCSEL_RC120M
 120 MHz RC oscillator More...
 

Clocks derived from the CPU clock

#define SYSCLK_OCD   AVR32_OCD_CLK_CPU
 On-Chip Debug system. More...
 
#define SYSCLK_SYSTIMER   AVR32_CORE_CLK_CPU_COUNT
 COUNT/COMPARE registers. More...
 

Clocks derived from the HSB clock

#define SYSCLK_PDCA_HSB   (AVR32_PDCA_CLK_HSB % 32)
 PDCA memory interface. More...
 
#define SYSCLK_FLASHCDW_DATA   (AVR32_FLASHCDW_CLK_HSB % 32)
 Flash data interface. More...
 
#define SYSCLK_SAU_HSB   (AVR32_SAU_CLK_HSB % 32)
 Secure Access Unit HSB interface. More...
 
#define SYSCLK_PBA_BRIDGE   (AVR32_HMATRIX_CLK_HSB_PBA_BRIDGE % 32)
 HSB<->PBA bridge. More...
 
#define SYSCLK_PBB_BRIDGE   (AVR32_HMATRIX_CLK_HSB_PBB_BRIDGE % 32)
 HSB<->PBB bridge. More...
 
#define SYSCLK_EVENT   (AVR32_PES_CLK_HSB % 32)
 Peripheral Event System. More...
 

Clocks derived from the PBA clock

#define SYSCLK_PDCA_PB   (AVR32_PDCA_CLK_PBA % 32)
 PDCA peripheral bus interface. More...
 
#define SYSCLK_INTC   (AVR32_INTC_CLK_PBA % 32)
 Internal interrupt controller. More...
 
#define SYSCLK_PM   (AVR32_PM_CLK_PBA % 32)
 PM/RTC/EIM configuration. More...
 
#define SYSCLK_SCIF   (AVR32_SCIF_CLK_PBA % 32)
 System Control Interface. More...
 
#define SYSCLK_AST   (AVR32_AST_CLK_PBA % 32)
 Asynchronous Timer. More...
 
#define SYSCLK_WDT   (AVR32_WDT_CLK_PBA % 32)
 Watchdog Timer. More...
 
#define SYSCLK_EIC   (AVR32_EIC_CLK_PBA % 32)
 External Interrupt Controller. More...
 
#define SYSCLK_FREQM   (AVR32_FREQM_CLK_PBA % 32)
 Frequency Meter. More...
 
#define SYSCLK_GPIO   (AVR32_GPIO_CLK_PBA % 32)
 General-Purpose I/O. More...
 
#define SYSCLK_USART0   (AVR32_USART0_CLK_PBA % 32)
 USART 0. More...
 
#define SYSCLK_USART1   (AVR32_USART1_CLK_PBA % 32)
 USART 1. More...
 
#define SYSCLK_USART2   (AVR32_USART2_CLK_PBA % 32)
 USART 2. More...
 
#define SYSCLK_USART3   (AVR32_USART3_CLK_PBA % 32)
 USART 3. More...
 
#define SYSCLK_SPI   (AVR32_SPI_CLK_PBA % 32)
 SPI Controller. More...
 
#define SYSCLK_TWIM0   (AVR32_TWIM0_CLK_PBA % 32)
 TWI Master 0. More...
 
#define SYSCLK_TWIM1   (AVR32_TWIM1_CLK_PBA % 32)
 TWI Master 1. More...
 
#define SYSCLK_TWIS0   (AVR32_TWIS0_CLK_PBA % 32)
 TWI Slave 0. More...
 
#define SYSCLK_TWIS1   (AVR32_TWIS1_CLK_PBA % 32)
 TWI Slave 1. More...
 
#define SYSCLK_PWMA   (AVR32_PWMA_CLK_PBA % 32)
 Pulse Width Modulator. More...
 
#define SYSCLK_TC0   (AVR32_TC0_CLK_PBA % 32)
 Timer/Counter 0. More...
 
#define SYSCLK_TC1   (AVR32_TC1_CLK_PBA % 32)
 Timer/Counter 1. More...
 
#define SYSCLK_ADCIFB   (AVR32_ADCIFB_CLK_PBA % 32)
 A/D Converter. More...
 
#define SYSCLK_ACIFB   (AVR32_ACIFB_CLK_PBA % 32)
 Analog Comparator. More...
 
#define SYSCLK_CAT   (AVR32_CAT_CLK_PBA % 32)
 Capacitive Touch. More...
 
#define SYSCLK_GLOC   (AVR32_GLOC_CLK_PBA % 32)
 Glue Logic Controller. More...
 
#define SYSCLK_AW   (AVR32_AW_CLK_PBA % 32)
 aWire UART More...
 

Clocks derived from the PBB clock

#define SYSCLK_FLASHCDW_REGS   (AVR32_FLASHC_CLK_PBB % 32)
 Flash Controller registers. More...
 
#define SYSCLK_HMATRIX   (AVR32_HMATRIX_CLK_PBB % 32)
 HSB Matrix configuration. More...
 
#define SYSCLK_SAU_REGS   (AVR32_SAU_CLK_PBB % 32)
 Secure Access Unit register. More...
 

Querying the system clock and its derived clocks

The following functions may be used to query the current frequency of the system clock and the CPU and bus clocks derived from it.

sysclk_get_main_hz() and sysclk_get_cpu_hz() can be assumed to be available on all platforms, although some platforms may define additional accessors for various chip-internal bus clocks. These are usually not intended to be queried directly by generic code.

static uint32_t sysclk_get_main_hz (void)
 Return the current rate in Hz of the main system clock. More...
 
static uint32_t sysclk_get_cpu_hz (void)
 Return the current rate in Hz of the CPU clock. More...
 
static uint32_t sysclk_get_hsb_hz (void)
 Return the current rate in Hz of the High-Speed Bus clock. More...
 
static uint32_t sysclk_get_pba_hz (void)
 Return the current rate in Hz of the Peripheral Bus A clock. More...
 
static uint32_t sysclk_get_pbb_hz (void)
 Return the current rate in Hz of the Peripheral Bus B clock. More...
 
static uint32_t sysclk_get_peripheral_bus_hz (const volatile void *module)
 Retrieves the current rate in Hz of the Peripheral Bus clock attached to the specified peripheral. More...
 

Enabling and disabling synchronous clocks

void sysclk_enable_pbb_module (unsigned int index)
 Enable a module clock derived from the PBB clock. More...
 
void sysclk_disable_pbb_module (unsigned int index)
 Disable a module clock derived from the PBB clock. More...
 
static void sysclk_enable_cpu_module (unsigned int index)
 Enable a module clock derived from the CPU clock. More...
 
static void sysclk_disable_cpu_module (unsigned int index)
 Disable a module clock derived from the CPU clock. More...
 
static void sysclk_enable_hsb_module (unsigned int index)
 Enable a module clock derived from the HSB clock. More...
 
static void sysclk_disable_hsb_module (unsigned int index)
 Disable a module clock derived from the HSB clock. More...
 
static void sysclk_enable_pba_module (unsigned int index)
 Enable a module clock derived from the PBA clock. More...
 
static void sysclk_disable_pba_module (unsigned int index)
 Disable a module clock derived from the PBA clock. More...
 
static void sysclk_enable_peripheral_clock (const volatile void *module)
 Enable a peripheral's clock from its base address. More...
 
static void sysclk_disable_peripheral_clock (const volatile void *module)
 Disable a peripheral's clock from its base address. More...
 

System Clock Source and Prescaler configuration

void sysclk_set_prescalers (unsigned int cpu_shift, unsigned int pba_shift, unsigned int pbb_shift)
 Set system clock prescaler configuration. More...
 
void sysclk_set_source (uint_fast8_t src)
 Change the source of the main system clock. More...
 

#define CONFIG_SYSCLK_CPU_DIV   0

Configuration symbol for dividing the CPU clock frequency by \(2^{CONFIG\_SYSCLK\_CPU\_DIV}\).

If this symbol is not defined, the CPU clock frequency is not divided.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_get_cpu_hz(), and sysclk_get_hsb_hz().

#define CONFIG_SYSCLK_INIT_CPUMASK

Configuration symbol for the CPU clocks enabled at power-on after the sysclock module has been initialized.

By default, all CPU clocks are left enabled, however to save power these can be automatically disabled by defining this value to a mask of SYSCLOCK_xxx settings.

If this symbol is not defined, then all CPU clocks are left enabled.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_init().

#define CONFIG_SYSCLK_INIT_HSBMASK

Configuration symbol for the HSB clocks enabled at power-on after the sysclock module has been initialized.

By default, all HSB clocks are left enabled, however to save power these can be automatically disabled by defining this value to a mask of SYSCLOCK_xxx settings.

If this symbol is not defined, then all HSB clocks are left enabled.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_init().

#define CONFIG_SYSCLK_INIT_PBAMASK

Configuration symbol for the PBA clocks enabled at power-on after the sysclock module has been initialized.

By default, all PBA clocks are left enabled, however to save power these can be automatically disabled by defining this value to a mask of SYSCLOCK_xxx settings.

If this symbol is not defined, then all PBA clocks are left enabled.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_init().

#define CONFIG_SYSCLK_INIT_PBBMASK

Configuration symbol for the PBB clocks enabled at power-on after the sysclock module has been initialized.

By default, all PBB clocks are left enabled, however to save power these can be automatically disabled by defining this value to a mask of SYSCLOCK_xxx settings.

If this symbol is not defined, then all PBB clocks are left enabled.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_init().

#define CONFIG_SYSCLK_PBA_DIV   0

Configuration symbol for dividing the PBA clock frequency by \(2^{CONFIG\_SYSCLK\_PBA\_DIV}\).

If this symbol is not defined, the PBA clock frequency is not divided.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_get_pba_hz().

#define CONFIG_SYSCLK_PBB_DIV   0

Configuration symbol for dividing the PBB clock frequency by \(2^{CONFIG\_SYSCLK\_PBB\_DIV}\).

If this symbol is not defined, the PBB clock frequency is not divided.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_get_pbb_hz().

#define CONFIG_SYSCLK_SOURCE   SYSCLK_SRC_RCSYS

Referenced by sysclk_get_main_hz().

#define CONFIG_USBCLK_DIV

Configuration symbol for the USB generic clock divider setting.

Sets the clock division for the USB generic clock. If a USB clock source is selected with CONFIG_USBCLK_SOURCE, this configuration symbol must also be defined.

Define this as any value that does not exceed GENCLK_DIV_MAX, and which will give a 48 MHz clock frequency from the selected source.

#define CONFIG_USBCLK_SOURCE

Configuration symbol for the USB generic clock source.

Sets the clock source to use for the USB. The source must also be properly configured.

Define this to one of the USBCLK_SRC_xxx settings. Leave it undefined if USB is not required.

#define SYSCLK_ACIFB   (AVR32_ACIFB_CLK_PBA % 32)
#define SYSCLK_ADCIFB   (AVR32_ADCIFB_CLK_PBA % 32)
#define SYSCLK_AST   (AVR32_AST_CLK_PBA % 32)
#define SYSCLK_AW   (AVR32_AW_CLK_PBA % 32)
#define SYSCLK_CAT   (AVR32_CAT_CLK_PBA % 32)
#define SYSCLK_EIC   (AVR32_EIC_CLK_PBA % 32)

External Interrupt Controller.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_EVENT   (AVR32_PES_CLK_HSB % 32)

Peripheral Event System.

#define SYSCLK_FLASHCDW_DATA   (AVR32_FLASHCDW_CLK_HSB % 32)

Flash data interface.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_FLASHCDW_REGS   (AVR32_FLASHC_CLK_PBB % 32)

Flash Controller registers.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_FREQM   (AVR32_FREQM_CLK_PBA % 32)
#define SYSCLK_GLOC   (AVR32_GLOC_CLK_PBA % 32)

Glue Logic Controller.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_GPIO   (AVR32_GPIO_CLK_PBA % 32)

General-Purpose I/O.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_HMATRIX   (AVR32_HMATRIX_CLK_PBB % 32)

HSB Matrix configuration.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_INTC   (AVR32_INTC_CLK_PBA % 32)

Internal interrupt controller.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_OCD   AVR32_OCD_CLK_CPU

On-Chip Debug system.

#define SYSCLK_PBA_BRIDGE   (AVR32_HMATRIX_CLK_HSB_PBA_BRIDGE % 32)

HSB<->PBA bridge.

#define SYSCLK_PBB_BRIDGE   (AVR32_HMATRIX_CLK_HSB_PBB_BRIDGE % 32)

HSB<->PBB bridge.

Referenced by sysclk_disable_pbb_module(), and sysclk_enable_pbb_module().

#define SYSCLK_PDCA_HSB   (AVR32_PDCA_CLK_HSB % 32)

PDCA memory interface.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_PDCA_PB   (AVR32_PDCA_CLK_PBA % 32)

PDCA peripheral bus interface.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_PM   (AVR32_PM_CLK_PBA % 32)

PM/RTC/EIM configuration.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_PWMA   (AVR32_PWMA_CLK_PBA % 32)

Pulse Width Modulator.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_SAU_HSB   (AVR32_SAU_CLK_HSB % 32)

Secure Access Unit HSB interface.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_SAU_REGS   (AVR32_SAU_CLK_PBB % 32)

Secure Access Unit register.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_SCIF   (AVR32_SCIF_CLK_PBA % 32)

System Control Interface.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_SPI   (AVR32_SPI_CLK_PBA % 32)
#define SYSCLK_SRC_DFLL   AVR32_PM_MCSEL_DFLL0

Digital Frequency Locked Loop.

Referenced by sysclk_get_main_hz(), and sysclk_init().

#define SYSCLK_SRC_OSC0   AVR32_PM_MCSEL_OSC0

Oscillator 0.

Referenced by sysclk_get_main_hz(), and sysclk_init().

#define SYSCLK_SRC_RC120M   AVR32_PM_MCSEL_RC120M

120 MHz RC oscillator

Referenced by sysclk_get_main_hz(), sysclk_init(), and sysclk_set_source().

#define SYSCLK_SRC_RCSYS   AVR32_PM_MCSEL_SLOW

System RC oscillator.

Referenced by sysclk_get_main_hz(), and sysclk_init().

#define SYSCLK_SYSTIMER   AVR32_CORE_CLK_CPU_COUNT

COUNT/COMPARE registers.

#define SYSCLK_TC0   (AVR32_TC0_CLK_PBA % 32)
#define SYSCLK_TC1   (AVR32_TC1_CLK_PBA % 32)
#define SYSCLK_TWIM0   (AVR32_TWIM0_CLK_PBA % 32)
#define SYSCLK_TWIM1   (AVR32_TWIM1_CLK_PBA % 32)
#define SYSCLK_TWIS0   (AVR32_TWIS0_CLK_PBA % 32)
#define SYSCLK_TWIS1   (AVR32_TWIS1_CLK_PBA % 32)
#define SYSCLK_USART0   (AVR32_USART0_CLK_PBA % 32)
#define SYSCLK_USART1   (AVR32_USART1_CLK_PBA % 32)
#define SYSCLK_USART2   (AVR32_USART2_CLK_PBA % 32)
#define SYSCLK_USART3   (AVR32_USART3_CLK_PBA % 32)
#define SYSCLK_WDT   (AVR32_WDT_CLK_PBA % 32)

static void sysclk_disable_cpu_module ( unsigned int  index)
inlinestatic

Disable a module clock derived from the CPU clock.

Parameters
indexIndex of the module clock in the CPUMASK register

References sysclk_priv_disable_module().

static void sysclk_disable_hsb_module ( unsigned int  index)
inlinestatic

Disable a module clock derived from the HSB clock.

Parameters
indexIndex of the module clock in the HSBMASK register

References sysclk_priv_disable_module().

Referenced by sysclk_disable_pbb_module(), and sysclk_disable_peripheral_clock().

static void sysclk_disable_pba_module ( unsigned int  index)
inlinestatic

Disable a module clock derived from the PBA clock.

Parameters
indexIndex of the module clock in the PBAMASK register

References sysclk_priv_disable_module().

Referenced by sysclk_disable_peripheral_clock().

void sysclk_disable_pbb_module ( unsigned int  index)

Disable a module clock derived from the PBB clock.

Parameters
indexIndex of the module clock in the PBBMASK register

References cpu_irq_restore(), cpu_irq_save(), sysclk_disable_hsb_module(), SYSCLK_PBB_BRIDGE, sysclk_pbb_refcount, and sysclk_priv_disable_module().

Referenced by sysclk_disable_peripheral_clock().

static void sysclk_disable_peripheral_clock ( const volatile void *  module)
inlinestatic

Disable a peripheral's clock from its base address.

Disables the clock to a peripheral, given its base address. If the peripheral has an associated clock on the HSB bus, this will be disabled also.

Parameters
modulePointer to the module's base address.

References Assert, AVR32_AW_ADDRESS, SYSCLK_ACIFB, SYSCLK_ADCIFB, SYSCLK_AST, SYSCLK_AW, SYSCLK_CAT, sysclk_disable_hsb_module(), sysclk_disable_pba_module(), sysclk_disable_pbb_module(), SYSCLK_EIC, SYSCLK_FLASHCDW_DATA, SYSCLK_FLASHCDW_REGS, SYSCLK_FREQM, SYSCLK_GLOC, SYSCLK_GPIO, SYSCLK_HMATRIX, SYSCLK_INTC, SYSCLK_PDCA_HSB, SYSCLK_PDCA_PB, SYSCLK_PM, SYSCLK_PWMA, SYSCLK_SAU_HSB, SYSCLK_SAU_REGS, SYSCLK_SCIF, SYSCLK_SPI, SYSCLK_TC0, SYSCLK_TC1, SYSCLK_TWIM0, SYSCLK_TWIM1, SYSCLK_TWIS0, SYSCLK_TWIS1, SYSCLK_USART0, SYSCLK_USART1, SYSCLK_USART2, SYSCLK_USART3, and SYSCLK_WDT.

static void sysclk_enable_cpu_module ( unsigned int  index)
inlinestatic

Enable a module clock derived from the CPU clock.

Parameters
indexIndex of the module clock in the CPUMASK register

References sysclk_priv_enable_module().

static void sysclk_enable_hsb_module ( unsigned int  index)
inlinestatic

Enable a module clock derived from the HSB clock.

Parameters
indexIndex of the module clock in the HSBMASK register

References sysclk_priv_enable_module().

Referenced by sysclk_enable_pbb_module(), and sysclk_enable_peripheral_clock().

static void sysclk_enable_pba_module ( unsigned int  index)
inlinestatic

Enable a module clock derived from the PBA clock.

Parameters
indexIndex of the module clock in the PBAMASK register

References sysclk_priv_enable_module().

Referenced by spi_master_init(), and sysclk_enable_peripheral_clock().

void sysclk_enable_pbb_module ( unsigned int  index)

Enable a module clock derived from the PBB clock.

Parameters
indexIndex of the module clock in the PBBMASK register

References cpu_irq_restore(), cpu_irq_save(), sysclk_enable_hsb_module(), SYSCLK_PBB_BRIDGE, sysclk_pbb_refcount, and sysclk_priv_enable_module().

Referenced by sysclk_enable_peripheral_clock().

static void sysclk_enable_peripheral_clock ( const volatile void *  module)
inlinestatic

Enable a peripheral's clock from its base address.

Enables the clock to a peripheral, given its base address. If the peripheral has an associated clock on the HSB bus, this will be enabled also.

Parameters
modulePointer to the module's base address.

References Assert, AVR32_AW_ADDRESS, SYSCLK_ACIFB, SYSCLK_ADCIFB, SYSCLK_AST, SYSCLK_AW, SYSCLK_CAT, SYSCLK_EIC, sysclk_enable_hsb_module(), sysclk_enable_pba_module(), sysclk_enable_pbb_module(), SYSCLK_FLASHCDW_DATA, SYSCLK_FLASHCDW_REGS, SYSCLK_FREQM, SYSCLK_GLOC, SYSCLK_GPIO, SYSCLK_HMATRIX, SYSCLK_INTC, SYSCLK_PDCA_HSB, SYSCLK_PDCA_PB, SYSCLK_PM, SYSCLK_PWMA, SYSCLK_SAU_HSB, SYSCLK_SAU_REGS, SYSCLK_SCIF, SYSCLK_SPI, SYSCLK_TC0, SYSCLK_TC1, SYSCLK_TWIM0, SYSCLK_TWIM1, SYSCLK_TWIS0, SYSCLK_TWIS1, SYSCLK_USART0, SYSCLK_USART1, SYSCLK_USART2, SYSCLK_USART3, and SYSCLK_WDT.

static uint32_t sysclk_get_cpu_hz ( void  )
inlinestatic

Return the current rate in Hz of the CPU clock.

Todo:
This function assumes that the CPU always runs at the system clock frequency. We want to support at least two more scenarios: Fixed CPU/bus clock dividers (config symbols) and dynamic CPU/bus clock dividers (which may change at run time). Ditto for all the bus clocks.
Returns
Frequency of the CPU clock, in Hz.

References CONFIG_SYSCLK_CPU_DIV, and sysclk_get_main_hz().

Referenced by sysclk_init().

static uint32_t sysclk_get_hsb_hz ( void  )
inlinestatic

Return the current rate in Hz of the High-Speed Bus clock.

Returns
Frequency of the High Speed Peripheral Bus clock, in Hz.

References CONFIG_SYSCLK_CPU_DIV, and sysclk_get_main_hz().

static uint32_t sysclk_get_main_hz ( void  )
inlinestatic

Return the current rate in Hz of the main system clock.

Todo:
This function assumes that the main clock source never changes once it's been set up, and that PLL0 always runs at the compile-time configured default rate. While this is probably the most common configuration, which we want to support as a special case for performance reasons, we will at some point need to support more dynamic setups as well.

References CONFIG_SYSCLK_SOURCE, dfll_get_default_rate, OSC_RC120M_NOMINAL_HZ, OSC_RCSYS_NOMINAL_HZ, SYSCLK_SRC_DFLL, SYSCLK_SRC_OSC0, SYSCLK_SRC_RC120M, and SYSCLK_SRC_RCSYS.

Referenced by sysclk_get_cpu_hz(), sysclk_get_hsb_hz(), sysclk_get_pba_hz(), and sysclk_get_pbb_hz().

static uint32_t sysclk_get_pba_hz ( void  )
inlinestatic

Return the current rate in Hz of the Peripheral Bus A clock.

Returns
Frequency of the Peripheral Bus A clock, in Hz.

References CONFIG_SYSCLK_PBA_DIV, and sysclk_get_main_hz().

Referenced by sysclk_get_peripheral_bus_hz().

static uint32_t sysclk_get_pbb_hz ( void  )
inlinestatic

Return the current rate in Hz of the Peripheral Bus B clock.

Returns
Frequency of the Peripheral Bus B clock, in Hz.

References CONFIG_SYSCLK_PBB_DIV, and sysclk_get_main_hz().

Referenced by sysclk_get_peripheral_bus_hz().

static uint32_t sysclk_get_peripheral_bus_hz ( const volatile void *  module)
inlinestatic

Retrieves the current rate in Hz of the Peripheral Bus clock attached to the specified peripheral.

Parameters
modulePointer to the module's base address.
Returns
Frequency of the bus attached to the specified peripheral, in Hz.

References Assert, AVR32_AW_ADDRESS, sysclk_get_pba_hz(), and sysclk_get_pbb_hz().

Referenced by spi_master_setup_device().

void sysclk_init ( void  )

Initialize the synchronous clock system.

This function will initialize the system clock and its source. This includes:

  • Mask all synchronous clocks except for any clocks which are essential for normal operation (for example internal memory clocks).
  • Set up the system clock prescalers as specified by the application's configuration file.
  • Enable the clock source specified by the application's configuration file (oscillator or PLL) and wait for it to become stable.
  • Set the main system clock source to the clock specified by the application's configuration file.

Since all non-essential peripheral clocks are initially disabled, it is the responsibility of the peripheral driver to re-enable any clocks that are needed for normal operation.

References Assert, CONFIG_SYSCLK_CPU_DIV, CONFIG_SYSCLK_INIT_CPUMASK, CONFIG_SYSCLK_INIT_HSBMASK, CONFIG_SYSCLK_INIT_PBAMASK, CONFIG_SYSCLK_INIT_PBBMASK, CONFIG_SYSCLK_PBA_DIV, CONFIG_SYSCLK_PBB_DIV, CONFIG_SYSCLK_SOURCE, cpu_irq_restore(), cpu_irq_save(), dfll_enable_config_defaults(), flash_set_bus_freq, osc_enable(), OSC_ID_OSC0, OSC_ID_RC120M, osc_wait_ready(), sysclk_get_cpu_hz(), SYSCLK_INIT_MINIMAL_CPUMASK, SYSCLK_INIT_MINIMAL_HSBMASK, SYSCLK_INIT_MINIMAL_PBAMASK, SYSCLK_INIT_MINIMAL_PBBMASK, sysclk_set_prescalers(), sysclk_set_source(), SYSCLK_SRC_DFLL, SYSCLK_SRC_OSC0, SYSCLK_SRC_RC120M, and SYSCLK_SRC_RCSYS.

Referenced by main().

void sysclk_priv_disable_module ( unsigned int  bus_id,
unsigned int  module_index 
)

Disable a maskable module clock.

Parameters
bus_idBus index, given by the AVR32_PM_CLK_GRP_xxx definitions.
module_indexIndex of the module to be disabled. This is the bit number in the corresponding xxxMASK register.

References cpu_irq_restore(), and cpu_irq_save().

Referenced by sysclk_disable_cpu_module(), sysclk_disable_hsb_module(), sysclk_disable_pba_module(), and sysclk_disable_pbb_module().

void sysclk_priv_enable_module ( unsigned int  bus_id,
unsigned int  module_index 
)

Enable a maskable module clock.

Parameters
bus_idBus index, given by the AVR32_PM_CLK_GRP_xxx definitions.
module_indexIndex of the module to be enabled. This is the bit number in the corresponding xxxMASK register.

References cpu_irq_restore(), and cpu_irq_save().

Referenced by sysclk_enable_cpu_module(), sysclk_enable_hsb_module(), sysclk_enable_pba_module(), and sysclk_enable_pbb_module().

void sysclk_set_prescalers ( unsigned int  cpu_shift,
unsigned int  pba_shift,
unsigned int  pbb_shift 
)

Set system clock prescaler configuration.

This function will change the system clock prescaler configuration to match the parameters.

Note
The parameters to this function are device-specific.
Parameters
cpu_shiftThe CPU clock will be divided by \(2^{cpu\_shift}\)
pba_shiftThe PBA clock will be divided by \(2^{pba\_shift}\)
pbb_shiftThe PBB clock will be divided by \(2^{pbb\_shift}\)

References Assert, cpu_irq_restore(), and cpu_irq_save().

Referenced by sysclk_init().

void sysclk_set_source ( uint_fast8_t  src)

Change the source of the main system clock.

Parameters
srcThe new system clock source. Must be one of the constants from the System Clock Sources section.

References Assert, cpu_irq_restore(), cpu_irq_save(), and SYSCLK_SRC_RC120M.

Referenced by sysclk_init().