TWIM Configuration.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
Configuration | |
#define | TWI_EXAMPLE TWIM3 |
Use the TWI in EXT2. More... | |
#define | EEPROM_BUS_ADDR 0x57 |
Default address of the EEPROM in IO1 Xplained Pro board. More... | |
#define EEPROM_BUS_ADDR 0x57 |
Default address of the EEPROM in IO1 Xplained Pro board.
#define TWI_EXAMPLE TWIM3 |
Use the TWI in EXT2.
Referenced by main().