Driver for the TWIM (Two-Wire Master Interface).
This driver provides access to the main features of the TWIM controller. The TWIM interconnects components on a unique two-wire bus. The TWIM is programmable as a master with sequential or single-byte access. Multiple master capability is supported.
Data Structures | |
struct | twim_config |
Input parameters when initializing the TWIM module mode. More... | |
struct | twim_package |
Information concerning the data transmission. More... | |
Macros | |
#define | TWIM_IER_NAK_MASK (TWIM_IER_ANAK | TWIM_IER_DNAK) |
Interrupt Enable Register Mask for No Acknowledgements. More... | |
#define | TWIM_IER_STD_MASK (TWIM_IER_ANAK | TWIM_IER_ARBLST) |
Frequently used Interrupt Enable Register Mask. More... | |
#define | TWIM_LOW_POWER_ENABLE 1 |
Enable TWIM Low Power Transfer in default. More... | |
#define | TWIM_SCR_NAK_MASK (TWIM_SCR_ANAK | TWIM_SCR_DNAK) |
Status Clear Register Mask for No Acknowledgements. More... | |
#define | TWIM_SR_NAK_MASK (TWIM_SR_ANAK | TWIM_SR_DNAK) |
Status Register Mask for No Acknowledgements. More... | |
#define | TWIM_SR_STD_MASK (TWIM_SR_ANAK | TWIM_SR_ARBLST) |
Frequently used Status Clear Register Mask. More... | |
Typedefs | |
typedef void(* | twim_callback_t )(Twim *) |
Functions | |
status_code_t | twi_master_read (Twim *twim, struct twim_package *package) |
Read multiple bytes from a TWI compatible slave device. More... | |
status_code_t | twi_master_write (Twim *twim, struct twim_package *package) |
Write multiple bytes to a TWI compatible slave device. More... | |
void | twim_clear_status (Twim *twim, uint32_t clear_status) |
Clear the current status of the TWIM. More... | |
void | twim_default_callback (Twim *twim) |
TWIM default callback function. More... | |
static void | twim_disable (Twim *twim) |
Disable Master Mode of the TWI. More... | |
void | twim_disable_interrupt (Twim *twim, uint32_t interrupt_source) |
Disable the TWIM interrupts and clear their status. More... | |
static void | twim_enable (Twim *twim) |
Enable Master Mode of the TWI. More... | |
void | twim_enable_interrupt (Twim *twim, uint32_t interrupt_source) |
Enable the TWIM interrupts. More... | |
uint32_t | twim_get_interrupt_mask (Twim *twim) |
Get the TWIM interrupt mask. More... | |
uint32_t | twim_get_status (Twim *twim) |
Information about the current status of the TWIM. More... | |
void | twim_pdca_transfer_prepare (Twim *twim, twi_package_t *package, bool read) |
Set TWIM for PDCA transfer. More... | |
status_code_t | twim_probe (Twim *twim, uint32_t chip_addr) |
Test if a chip answers for a given TWI address. More... | |
void | twim_set_callback (Twim *twim, uint32_t interrupt_source, twim_callback_t callback, uint8_t irq_level) |
Set callback for TWIM. More... | |
status_code_t | twim_set_config (Twim *twim, struct twim_config *config) |
Initialize the TWIM module. More... | |
status_code_t | twim_set_hsmode_speed (Twim *twim, uint32_t speed, uint32_t clk, uint8_t cycles) |
Set the TWI bus speed in conjunction with the clock frequency in high speed mode. More... | |
status_code_t | twim_set_speed (Twim *twim, uint32_t speed, uint32_t clk, uint8_t cycles) |
Set the TWI bus speed in conjunction with the clock frequency. More... | |
TWI transfer speed definitions | |
#define | TWI_STD_MODE_SPEED ( 100000 /* kbit/s */) |
TWI Standard Mode. More... | |
#define | TWI_FAST_MODE_SPEED ( 400000 /* kbit/s */) |
TWI Fast Mode. More... | |
#define | TWI_FAST_MODE_PLUS_SPEED (1000000 /* kbit/s */) |
TWI Fast Mode Plus. More... | |
#define | TWI_HIGH_SPEED_MODE_SPEED (3400000 /* kbit/s */) |
TWI High Speed Mode. More... | |
enum | twim_transfer_status { TWI_SUCCESS = 0, TWI_INVALID_ARGUMENT = -1, TWI_ARBITRATION_LOST = -2, TWI_NO_CHIP_FOUND = -3, TWI_RECEIVE_NACK = -4, TWI_SEND_NACK = -5, TWI_INVALID_CLOCK_DIV = -6 } |
Status Codes for TWI Transfer. More... | |
typedef enum twim_transfer_status | twim_transfer_status_t |
TWI Driver Compatibility | |
Codes for SAM devices using TWI modules can easily be ported to SAM devices with TWIM module | |
#define | twi_options_t struct twim_config |
#define | twi_package_t struct twim_package |
#define | twi_master_init twim_set_config |
#define | twi_probe twim_probe |
#define TWI_FAST_MODE_PLUS_SPEED (1000000 /* kbit/s */) |
TWI Fast Mode Plus.
Referenced by twim_set_config().
#define TWI_FAST_MODE_SPEED ( 400000 /* kbit/s */) |
TWI Fast Mode.
#define TWI_HIGH_SPEED_MODE_SPEED (3400000 /* kbit/s */) |
TWI High Speed Mode.
#define twi_master_init twim_set_config |
Referenced by twi_master_setup().
#define twi_options_t struct twim_config |
#define twi_package_t struct twim_package |
Referenced by main().
#define twi_probe twim_probe |
#define TWI_STD_MODE_SPEED ( 100000 /* kbit/s */) |
TWI Standard Mode.
#define TWIM_IER_NAK_MASK (TWIM_IER_ANAK | TWIM_IER_DNAK) |
Interrupt Enable Register Mask for No Acknowledgements.
#define TWIM_IER_STD_MASK (TWIM_IER_ANAK | TWIM_IER_ARBLST) |
Frequently used Interrupt Enable Register Mask.
Referenced by twi_master_read(), and twi_master_write().
#define TWIM_LOW_POWER_ENABLE 1 |
Enable TWIM Low Power Transfer in default.
#define TWIM_SCR_NAK_MASK (TWIM_SCR_ANAK | TWIM_SCR_DNAK) |
Status Clear Register Mask for No Acknowledgements.
#define TWIM_SR_NAK_MASK (TWIM_SR_ANAK | TWIM_SR_DNAK) |
Status Register Mask for No Acknowledgements.
#define TWIM_SR_STD_MASK (TWIM_SR_ANAK | TWIM_SR_ARBLST) |
Frequently used Status Clear Register Mask.
Referenced by twim_default_callback().
typedef void(* twim_callback_t)(Twim *) |
typedef enum twim_transfer_status twim_transfer_status_t |
enum twim_transfer_status |
Status Codes for TWI Transfer.
status_code_t twi_master_read | ( | Twim * | twim, |
struct twim_package * | package | ||
) |
Read multiple bytes from a TWI compatible slave device.
twim | Base address of the TWIM |
package | Package information and data |
STATUS_OK | If all bytes were read successfully |
ERR_IO_ERROR | NACK received or Bus Arbitration lost |
References twim_package::addr, twim_package::addr_length, twim_package::buffer, twim_package::chip, ERR_IO_ERROR, find_twim_channel_num(), twim_package::high_speed, twim_package::high_speed_code, twim_package::length, p_twim_next_rx_data, p_twim_rx_data, p_twim_tx_data, sleepmgr_enter_sleep(), sleepmgr_lock_mode(), SLEEPMGR_SLEEP_1, sleepmgr_unlock_mode(), STATUS_OK, twim_package::ten_bit, transfer_status, TWI_ARBITRATION_LOST, TWI_RECEIVE_NACK, TWI_SUCCESS, twim_get_status(), TWIM_IER_STD_MASK, twim_it_mask, TWIM_MAX_NBYTES_PER_XFER, twim_next_cmd_xfer_valid, twim_next_rx_nb_bytes, twim_next_tx_nb_bytes, twim_rx_nb_bytes, and twim_tx_nb_bytes.
Referenced by main(), and twim_probe().
status_code_t twi_master_write | ( | Twim * | twim, |
struct twim_package * | package | ||
) |
Write multiple bytes to a TWI compatible slave device.
twim | Base address of the TWIM |
*package | Package information and data |
STATUS_OK | If all bytes were send successfully |
ERR_IO_ERROR | NACK received or Bus Arbitration lost |
References twim_package::addr, twim_package::addr_length, twim_package::buffer, twim_package::chip, ERR_IO_ERROR, find_twim_channel_num(), twim_package::high_speed, twim_package::high_speed_code, twim_package::length, p_twim_next_tx_data, p_twim_tx_data, sleepmgr_enter_sleep(), sleepmgr_lock_mode(), SLEEPMGR_SLEEP_1, sleepmgr_unlock_mode(), STATUS_OK, twim_package::ten_bit, transfer_status, TWI_ARBITRATION_LOST, TWI_RECEIVE_NACK, TWI_SUCCESS, twim_get_status(), TWIM_IER_STD_MASK, twim_it_mask, TWIM_MAX_NBYTES_PER_XFER, twim_next_cmd_xfer_valid, twim_next_rx_nb_bytes, twim_next_tx_nb_bytes, and twim_tx_nb_bytes.
Referenced by main().
void twim_clear_status | ( | Twim * | twim, |
uint32_t | clear_status | ||
) |
Clear the current status of the TWIM.
twim | Base address of the TWIM |
clear_status | The TWIM status to be clear |
void twim_default_callback | ( | Twim * | twim | ) |
TWIM default callback function.
References find_twim_channel_num(), NCMDR_FREE_WAIT, p_twim_next_rx_data, p_twim_next_tx_data, p_twim_rx_data, p_twim_tx_data, transfer_status, TWI_ARBITRATION_LOST, TWI_RECEIVE_NACK, twim_it_mask, TWIM_MAX_NBYTES_PER_XFER, twim_next_cmd_xfer_valid, twim_next_rx_nb_bytes, twim_next_tx_nb_bytes, twim_rx_nb_bytes, TWIM_SR_STD_MASK, and twim_tx_nb_bytes.
Referenced by twi_master_setup().
|
inlinestatic |
Disable Master Mode of the TWI.
twim | Base address of the TWIM instance. |
void twim_disable_interrupt | ( | Twim * | twim, |
uint32_t | interrupt_source | ||
) |
Disable the TWIM interrupts and clear their status.
twim | Base address of the TWIM. |
interrupt_source | The TWI interrupt to be disabled |
|
inlinestatic |
Enable Master Mode of the TWI.
twim | Base address of the TWIM instance. |
void twim_enable_interrupt | ( | Twim * | twim, |
uint32_t | interrupt_source | ||
) |
Enable the TWIM interrupts.
twim | Base address of the TWIM |
interrupt_source | The TWI interrupt to be enabled |
Referenced by twim_set_callback().
uint32_t twim_get_interrupt_mask | ( | Twim * | twim | ) |
Get the TWIM interrupt mask.
twim | Base address of the TWIM |
TWIM | interrupt mask |
uint32_t twim_get_status | ( | Twim * | twim | ) |
Information about the current status of the TWIM.
twim | Base address of the TWIM |
Referenced by twi_master_read(), and twi_master_write().
void twim_pdca_transfer_prepare | ( | Twim * | twim, |
twi_package_t * | package, | ||
bool | read | ||
) |
Set TWIM for PDCA transfer.
twim | Base address of the TWIM |
package | Package information and data (see twim_package_t) |
read | True if it's a read trasnfer |
status_code_t twim_probe | ( | Twim * | twim, |
uint32_t | chip_addr | ||
) |
Test if a chip answers for a given TWI address.
twim | Base address of the TWIM |
chip_addr | Address of the chip which is searched for |
STATUS_OK | Slave Found |
ERR_IO_ERROR | ANAK received or Bus Arbitration lost |
References twim_package::addr_length, twim_package::buffer, twim_package::chip, twim_package::length, and twi_master_read().
void twim_set_callback | ( | Twim * | twim, |
uint32_t | interrupt_source, | ||
twim_callback_t | callback, | ||
uint8_t | irq_level | ||
) |
Set callback for TWIM.
twim | Base address of the TWIM |
interrupt_source | TWIM interrupt source |
callback | Callback function pointer |
irq_level | Interrupt level |
References find_twim_channel_num(), twim_callback_pointer, and twim_enable_interrupt().
Referenced by twi_master_setup().
status_code_t twim_set_config | ( | Twim * | twim, |
struct twim_config * | config | ||
) |
Initialize the TWIM module.
twim | Base address of the TWIM |
config | Options for initializing the TWIM module |
STATUS_OK | Transaction is successful |
ERR_INVALID_ARG | Invalid arg resulting in wrong CWGR Exponential |
References twim_config::clock_drive_strength_low, twim_config::clock_slew_limit, twim_config::data_drive_strength_low, twim_config::data_setup_cycles, twim_config::data_slew_limit, ERR_INVALID_ARG, twim_config::hs_clock_drive_strength_high, twim_config::hs_clock_drive_strength_low, twim_config::hs_clock_slew_limit, twim_config::hs_data_drive_strength_low, twim_config::hs_data_slew_limit, twim_config::hsmode_data_setup_cycles, twim_config::hsmode_speed, sleepmgr_init(), twim_config::smbus, twim_config::speed, STATUS_OK, sysclk_enable_peripheral_clock(), TWI_FAST_MODE_PLUS_SPEED, twim_config::twim_clk, twim_set_hsmode_speed(), and twim_set_speed().
status_code_t twim_set_hsmode_speed | ( | Twim * | twim, |
uint32_t | speed, | ||
uint32_t | clk, | ||
uint8_t | cycles | ||
) |
Set the TWI bus speed in conjunction with the clock frequency in high speed mode.
twim | Base address of the TWIM |
speed | The desired twim bus speed |
clk | The current running system clock frequency |
cycles | Clock cycles for data setup count |
STATUS_OK | Transaction is successful |
ERR_INVALID_ARG | Invalid arg resulting in wrong CWGR Exponential |
References ERR_INVALID_ARG, and STATUS_OK.
Referenced by twim_set_config().
status_code_t twim_set_speed | ( | Twim * | twim, |
uint32_t | speed, | ||
uint32_t | clk, | ||
uint8_t | cycles | ||
) |
Set the TWI bus speed in conjunction with the clock frequency.
twim | Base address of the TWIM |
speed | The desired twim bus speed |
clk | The current running system clock frequency |
cycles | Clock cycles for data setup count |
STATUS_OK | Transaction is successful |
ERR_INVALID_ARG | Invalid arg resulting in wrong CWGR Exponential |
References ERR_INVALID_ARG, and STATUS_OK.
Referenced by twim_set_config().