![]() | Copyright (c) 2012-2018 Microchip Technology Inc |
![]() | Service (SAM4E) |
![]() | Management (SAM4E) |
![]() | This is the quick start guide for the PMC module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
![]() | This is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases |
![]() ![]() | In this case we will read out the pins from one whole port and write the read value to another port |
![]() | This is the quick start guide for the USART module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
![]() ![]() | In this use case, the USART module is configured for: |
![]() ![]() | In this use case, the USART module is configured for: |
![]() | This page lists several definition related to the board operating frequency |
![]() | This page lists several definition related to the board description |
![]() | |
![]() | This page lists the definitions related to external on-board components located in the board.h file for the SAM4E-EK |
![]() | This page lists definitions related to internal & external on-board memories |
![]() | This page lists definitions related to CAN0 and CAN1 |
![]() |