This example demonstrates how to use the USART_SPI Master Mode Basic Services.
The usart_spi API can be found here.
This example can be used on all SAM EK boards with external AT45DBX data flash component. Connect the board and external component with the following paired pins.
This software was written for the GNU GCC and IAR. Other compilers may or may not work.
For further information, visit Microchip.