Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Calendar service example 2 for UC3-L0 Xplained Documentation

Introduction

This is an example application for the calendar functionality.

Device Info

All AVR devices can be used. This example has been tested with the following setup:

  • XMEGA-A1 Xplain
  • UC3-L0 Xplained
  • STK600+RCUC3L4
  • STK600 with RCUC3D extension board (Connect STK600.PORTA.PA4 -> STK600.LEDS.LED0)

Description of the example application

This application will calculate the time difference in years, months, days, hours, minutes and seconds between two dates and turn on a LED if it is correct.

Dependencies

Relevant module dependencies for this application are:

Compilation info

This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.

Contact Information

For further information, visit Microchip.
Support and FAQ: https://www.microchip.com/support/