This is an example application for the calendar functionality.
All AVR devices can be used. This example has been tested with the following setup:
This application will calculate the time difference in years, months, days, hours, minutes and seconds between two dates and turn on a LED if it is correct.
Relevant module dependencies for this application are:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.
Support and FAQ: https://www.microchip.com/support/