![]() | The tickless feature of FreeRTOS allows the device to sleep for peroids longer than the predefined OS tick rate |
![]() | Compiler abstraction layer and code utilities for Cortex-M0+ based Atmel SAM devices |
![]() | This is a driver for global enabling and disabling of interrupts |
![]() | This collection of macros identify which series and families that the various Atmel parts belong to |
![]() | The generic board support module includes board-specific definitions and function prototypes, such as the board initialization function |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's General Purpose Input/Output (GPIO) pin functionality, for manual pin state reading and writing |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's physical I/O Pins, to alter the direction and input/drive characteristics as well as to configure the pin peripheral multiplexer selection |
![]() | The demo tasks demonstrate basic use of FreeRTOS, with inter-task communication using queues and mutexes |
![]() | Simple driver for receiving from the EDBG Virtual COM Port via SERCOM USART |
![]() | This is a simple driver for manipulating LEDs and reading buttons on any number of OLED1 Xplained Pro wing boards |
![]() | See Quick Start Guide for the mono graphics service |
![]() | This is a low level driver for the SSD1306 OLED controller through 4-wire SPI |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's system relation functionality, necessary for the basic device operation |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's clocking related functions |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of internal software and hardware interrupts/exceptions |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the SERCOM module in its SPI mode to transfer SPI data frames |
![]() | This module provides simple loop-based delay routines for those applications requiring a brief wait during execution |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the SERCOM module in its USART mode to transfer or receive USART data frames |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the timer modules within the device, for waveform generation and timing operations |
![]() | Croutine |
![]() | Croutine |
![]() | Croutine |
![]() | Croutine |
![]() | |
![]() | Croutine |
![]() | Croutine |
![]() | Croutine |
![]() | An event group is a collection of bits to which an application can assign a meaning |
![]() | Message_buffer.h |
![]() | Message_buffer.h |
![]() | Message_buffer.h |
![]() | Message_buffer.h |
![]() | Message_buffer.h |
![]() | Message_buffer.h |
![]() | Message_buffer.h |
![]() | Message_buffer.h |
![]() | Message_buffer.h |
![]() | Message_buffer.h |
![]() | Queue |
![]() | Queue |
![]() | Queue |
![]() | Queue |
![]() | Queue |
![]() | Queue |
![]() | Queue |
![]() | Queue |
![]() | Queue |
![]() | Queue |
![]() | Queue |
![]() | Queue |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Message_buffer.h |
![]() | Stream_buffer.h |
![]() | Stream_buffer.h |
![]() | Stream_buffer.h |
![]() | Stream_buffer.h |
![]() | Stream_buffer.h |
![]() | Stream_buffer.h |
![]() | Stream_buffer.h |
![]() | Stream_buffer.h |
![]() | Stream_buffer.h |
![]() | Stream_buffer.h |
![]() | Stream_buffer.h |
![]() | Stream_buffer.h |
![]() | Stream_buffer.h |
![]() | Stream_buffer.h |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() |