Compiler abstraction layer and code utilities | Compiler abstraction layer and code utilities for Cortex-M0+ based Atmel SAM devices |
Global interrupt management | This is a driver for global enabling and disabling of interrupts |
Atmel part identification macros | This collection of macros identify which series and families that the various Atmel parts belong to |
Generic board support | The generic board support module includes board-specific definitions and function prototypes, such as the board initialization function |
SAM Port (PORT) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's General Purpose Input/Output (GPIO) pin functionality, for manual pin state reading and writing |
SAM System Pin Multiplexer (SYSTEM PINMUX) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's physical I/O Pins, to alter the direction and input/drive characteristics as well as to configure the pin peripheral multiplexer selection |
FreeRTOS demo tasks | The demo tasks demonstrate basic use of FreeRTOS, with inter-task communication using queues and mutexes |
Embedded Debugger (EDBG) Virtual COM Port driver | Simple driver for receiving from the EDBG Virtual COM Port via SERCOM USART |
OLED1 Xplained Pro LED and button driver | This is a simple driver for manipulating LEDs and reading buttons on any number of OLED1 Xplained Pro wing boards |
Monochrome graphical display system | See Quick Start Guide for the mono graphics service |
SSD1306 OLED Controller Low-level driver | This is a low level driver for the SSD1306 OLED controller through 4-wire SPI |
SAM System (SYSTEM) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's system relation functionality, necessary for the basic device operation |
SAM System Clock Management (SYSTEM CLOCK) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's clocking related functions |
SAM System Interrupt (SYSTEM INTERRUPT) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of internal software and hardware interrupts/exceptions |
SAM Serial Peripheral Interface (SERCOM SPI) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the SERCOM module in its SPI mode to transfer SPI data frames |
Busy-Wait Delay Routines | This module provides simple loop-based delay routines for those applications requiring a brief wait during execution |
SAM Serial USART (SERCOM USART) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the SERCOM module in its USART mode to transfer or receive USART data frames |
xCoRoutineCreate | Croutine |
vCoRoutineSchedule | Croutine |
crSTART | Croutine |
crDELAY | Croutine |
crQUEUE_SEND | |
crQUEUE_RECEIVE | Croutine |
crQUEUE_SEND_FROM_ISR | Croutine |
crQUEUE_RECEIVE_FROM_ISR | Croutine |
EventGroup | An event group is a collection of bits to which an application can assign a meaning |
xMessageBufferCreate | Message_buffer.h |
xMessageBufferCreateStatic | Message_buffer.h |
xMessageBufferSend | Message_buffer.h |
xMessageBufferSendFromISR | Message_buffer.h |
xMessageBufferReceive | Message_buffer.h |
xMessageBufferReceiveFromISR | Message_buffer.h |
xMessageBufferReset | Message_buffer.h |
xMessageBufferSpaceAvailable | Message_buffer.h |
xMessageBufferSendCompletedFromISR | Message_buffer.h |
xMessageBufferReceiveCompletedFromISR | Message_buffer.h |
xQueueCreate | Queue |
xQueueCreateStatic | Queue |
xQueueSend | Queue |
xQueueOverwrite | Queue |
xQueuePeek | Queue |
xQueuePeekFromISR | Queue |
xQueueReceive | Queue |
uxQueueMessagesWaiting | Queue |
vQueueDelete | Queue |
xQueueSendFromISR | Queue |
xQueueOverwriteFromISR | Queue |
xQueueReceiveFromISR | Queue |
vSemaphoreCreateBinary | Semphr |
xSemaphoreCreateBinary | Semphr |
xSemaphoreCreateBinaryStatic | Semphr |
xSemaphoreTake | Semphr |
xSemaphoreTakeRecursive | Semphr |
xSemaphoreGive | Semphr |
xSemaphoreGiveRecursive | Semphr |
xSemaphoreGiveFromISR | Semphr |
xSemaphoreCreateMutex | Semphr |
xSemaphoreCreateMutexStatic | Semphr |
xSemaphoreCreateRecursiveMutex | Semphr |
xSemaphoreCreateRecursiveMutexStatic | Semphr |
xSemaphoreCreateCounting | Semphr |
xSemaphoreCreateCountingStatic | Semphr |
vSemaphoreDelete | Semphr |
xStreamBufferCreate | Message_buffer.h |
xStreamBufferCreateStatic | Stream_buffer.h |
xStreamBufferSend | Stream_buffer.h |
xStreamBufferSendFromISR | Stream_buffer.h |
xStreamBufferReceive | Stream_buffer.h |
xStreamBufferReceiveFromISR | Stream_buffer.h |
vStreamBufferDelete | Stream_buffer.h |
xStreamBufferIsFull | Stream_buffer.h |
xStreamBufferIsEmpty | Stream_buffer.h |
xStreamBufferReset | Stream_buffer.h |
xStreamBufferSpacesAvailable | Stream_buffer.h |
xStreamBufferBytesAvailable | Stream_buffer.h |
xStreamBufferSetTriggerLevel | Stream_buffer.h |
xStreamBufferSendCompletedFromISR | Stream_buffer.h |
xStreamBufferReceiveCompletedFromISR | Stream_buffer.h |
TaskHandle_t | Task |
taskYIELD | Task |
taskENTER_CRITICAL | Task |
taskEXIT_CRITICAL | Task |
taskDISABLE_INTERRUPTS | Task |
taskENABLE_INTERRUPTS | Task |
xTaskCreate | Task |
xTaskCreateStatic | Task |
xTaskCreateRestricted | Task |
xTaskCreateRestrictedStatic | Task |
vTaskDelete | Task |
vTaskDelay | Task |
vTaskDelayUntil | Task |
xTaskAbortDelay | Task |
uxTaskPriorityGet | Task |
vTaskGetInfo | Task |
vTaskPrioritySet | Task |
vTaskSuspend | Task |
vTaskResume | Task |
vTaskResumeFromISR | Task |
vTaskStartScheduler | Task |
vTaskEndScheduler | Task |
vTaskSuspendAll | Task |
xTaskResumeAll | Task |
xTaskGetTickCount | Task |
xTaskGetTickCountFromISR | Task |
uxTaskGetNumberOfTasks | Task |
pcTaskGetName | Task |
pcTaskGetHandle | Task |
vTaskList | Task |
vTaskGetRunTimeStats | Task |
xTaskNotify | Task |
xTaskNotifyWait | Task |
xTaskNotifyGive | Task |
ulTaskNotifyTake | Task |
xTaskNotifyStateClear | Task |
Gfx_sysfont |