Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Related Pages
Here is a list of all related documentation pages:
[detail level 12]
oLicenseSubject to your compliance with these terms, you may use Microchip software and any derivatives exclusively with Microchip products
oQuick start guide for the SAM PMC moduleThis is the quick start guide for the PMC module, with step-by-step instructions on how to configure and use the driver in a selection of use cases
oQuick Start Guide for the System Clock Management service (SAM3A)This is the quick start guide for the System Clock Management service, with step-by-step instructions on how to configure and use the service for specific use cases
oQuick start guide for Serial Interface serviceThis is the quick start guide for the Serial Interface module, with step-by-step instructions on how to configure and use the serial in a selection of use cases
|\Advanced use case - Send a packet of serial dataIn this use case, the USART module is configured for:
oQuick start guide for the SAM USART moduleThis is the quick start guide for the USART module, with step-by-step instructions on how to configure and use the driver in a selection of use cases
|oUSART receive character and echo backIn this use case, the USART module is configured for:
|\USART receive character and echo back via interruptsIn this use case, the USART module is configured for:
oQuick start guide for the common IOPORT serviceThis is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases
|\Advanced use case doing port accessIn this case we will read out the pins from one whole port and write the read value to another port
oExtra Information for Peripheral DMA Controller
oExamples for Peripheral DMA ControllerThis is a list of the available Quick Start guides (QSGs) and example applications for SAM3A/3N/3S/3U/3X/4E/4N/4S/G Peripheral DMA Controller (PDC) Driver
|oQuick Start Guide for PDC - BasicThis is the quickstart guide for SAM3A/3N/3S/3U/3X/4E/4N/4S/G Peripheral DMA Controller (PDC) Driver with step-by-step instructions on how to configure and use the driver
|\Peripheral DMA Controller Example
oDocument Revision History
oQuick start guide for USB device Communication Class Device module (UDI CDC)This is the quick start guide for the USB device interface CDC module (UDI CDC) with step-by-step instructions on how to configure and use the modules in a selection of use cases
|oCDC in a composite deviceA USB Composite Device is a USB Device which uses more than one USB class
|oChange USB speedIn this use case, the USB device is used with different USB speeds
|oUse USB stringsIn this use case, the usual USB strings is added in the USB device
|oUse USB remote wakeup featureIn this use case, the USB remote wakeup feature is enabled
|oBus power application recommendationsIn this use case, the USB device BUS power feature is enabled
|\USB dynamic serial numberIn this use case, the USB serial strings is dynamic
oconf_clock.h examples with USB supportContent of XMEGA conf_clock.h:
oQuick Start Guide for the SAM PIO driverThis is the quick start guide for the PIO Driver, with step-by-step instructions on how to configure and use the driver for specific use cases
oAdvanced use case - Interrupt driven edge detection
oQuick start guide forFreeRTOS TWI peripheral control functions
|oInitializing the FreeRTOS TWI driverFor standard operation
|oTransmitting using the FreeRTOS TWI driver inStandard mode
|oReceiving using the FreeRTOS TWI driver inStandard mode
|oInitializing the FreeRTOS TWI driverFor asynchronous operation
|oTransmitting using the FreeRTOS TWI driver inFully asynchronous mode
|\Receiving using the FreeRTOS TWI driver in fullyAsynchronous mode
oQuickstart guide for Common service TWIThis is the quickstart guide for the Common service TWI, with step-by-step instructions on how to configure and use the driver in a selection of use cases
oQuick start guide forFreeRTOS USART peripheral control functions
|oInitializing the FreeRTOS USARTDriver for standard operation
|oTransmitting using the FreeRTOS USART driver inStandard mode
|oInitializing the FreeRTOS USARTDriver for asynchronous operation
|oTransmitting using the FreeRTOS USART driver inFully asynchronous mode
|\Receiving using the FreeRTOS USART driverThis example demonstrates using the FreeRTOS USART API to receive data
oQuick start guide forFreeRTOS UART peripheral control functions
|oInitializing the FreeRTOS UARTDriver for standard operation
|oTransmitting using the FreeRTOS UART driver inStandard mode
|oInitializing the FreeRTOS UARTDriver for asynchronous operation
|oTransmitting using the FreeRTOS UART driver inFully asynchronous mode
|\Receiving using the FreeRTOS UART driverThis example demonstrates using the FreeRTOS UART API to receive data
o"SAM3X-EK - Operating frequencies"This page lists several definition related to the board operating frequency
o"SAM3X-EK - Board informations"This page lists several definition related to the board description
o"SAM3X-EK - PIO definitions"This pages lists all the pio definitions
o"SAM3X-EK - USB device"
o"SAM3X-EK - External components"This page lists the definitions related to external on-board components located in the board.h file for the SAM3X-EK
o"SAM3X-EK - Memories"This page lists definitions related to internal & external on-board memories
\Todo List