task.
h
TaskHandle_t xTaskGetHandle( const char *pcNameToQuery );
NOTE: This function takes a relatively long time to complete and should be used sparingly.
- Returns
- The handle of the task that has the human readable name pcNameToQuery. NULL is returned if no matching name is found. INCLUDE_xTaskGetHandle must be set to 1 in FreeRTOSConfig.h for pcTaskGetHandle() to be available.