This is the unit test application for the FreeRTOS TWI Interface Layer. It consists of test cases for the following functionality:
All SAM devices can be used. This example has been tested with the following setup:
Note: this unit test takes about 20 seconds to finish.
This software was written for the GNU GCC and IAR for ARM. Other compilers may or may not work.
For further information, visit Microchip.
Support and FAQ: https://www.microchip.com/support/