CTRL_ACCESS interface for the AT45DBX data flash driver.
Copyright (c) 2010-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
Control Interface | |
Ctrl_status | at45dbx_test_unit_ready (void) |
Tests the memory state and initializes the memory if required. More... | |
Ctrl_status | at45dbx_read_capacity (U32 *u32_nb_sector) |
Returns the address of the last valid sector in the memory. More... | |
bool | at45dbx_wr_protect (void) |
Returns the write-protection state of the memory. More... | |
bool | at45dbx_removal (void) |
Tells whether the memory is removable. More... | |
bool | at45dbx_unload (bool unload) |
Unload/load the memory. More... | |
MEM <-> RAM Interface | |
Ctrl_status | at45dbx_df_2_ram (U32 addr, void *ram) |
Copies 1 data sector from the memory to RAM. More... | |
Ctrl_status | at45dbx_ram_2_df (U32 addr, const void *ram) |
Copies 1 data sector from RAM to the memory. More... | |
Ctrl_status at45dbx_df_2_ram | ( | U32 | addr, |
void * | ram | ||
) |
Copies 1 data sector from the memory to RAM.
addr | Address of first memory sector to read. |
ram | Pointer to RAM buffer to write. |
Ctrl_status at45dbx_ram_2_df | ( | U32 | addr, |
const void * | ram | ||
) |
Copies 1 data sector from RAM to the memory.
addr | Address of first memory sector to write. |
ram | Pointer to RAM buffer to read. |
Ctrl_status at45dbx_read_capacity | ( | U32 * | u32_nb_sector | ) |
Returns the address of the last valid sector in the memory.
u32_nb_sector | Pointer to the address of the last valid sector. |
bool at45dbx_removal | ( | void | ) |
Tells whether the memory is removable.
true
if the memory is removable, else false
. Ctrl_status at45dbx_test_unit_ready | ( | void | ) |
Tests the memory state and initializes the memory if required.
The TEST UNIT READY SCSI primary command allows an application client to poll a LUN until it is ready without having to allocate memory for returned data.
This command may be used to check the media status of LUNs with removable media.
Unload/load the memory.
unload | true to unload, false to load. |
true
if the operation is success, else false
. bool at45dbx_wr_protect | ( | void | ) |
Returns the write-protection state of the memory.
true
if the memory is write-protected, else false
.