Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
90_00028_A0 display using ILI9488 display controller

This is hardware specific configuration that configures the graphical service for use with the ILI9488 display controller and the 90-00028-A0 display.

All the drawing functionality in this configuration is provided by the Generic Implementation of Graphics Primitives driver. This configuration includes information about the panel size, data type used for coordinates and color and functionality to convert RGB color to the color format native to the display.

Macros

#define gfx_color(r, g, b)   gfx_ili9488_color(r, g, b)
 ILI9488 display driver specific function, see gfx_ili9488_color. More...
 
#define gfx_copy_pixels_from_screen(pixels, count)   ili9488_copy_pixels_from_screen(pixels, count)
 ILI9488 display driver specific function, see ili9488_copy_pixels_from_screen. More...
 
#define gfx_copy_pixels_to_screen(pixels, count)   ili9488_copy_pixels_to_screen(pixels, count)
 ILI9488 display driver specific function, see ili9488_copy_pixels_to_screen. More...
 
#define gfx_copy_progmem_pixels_to_screen(pixels, count)   ili9488_copy_progmem_pixels_to_screen(pixels, count)
 ILI9488 display driver specific function available for ATmega and ATXmega devices, see ili9488_copy_progmem_pixels_to_screen. More...
 
#define gfx_draw_bitmap(bmp, x, y)   gfx_generic_draw_bitmap(bmp, x, y)
 ILI9488 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_bitmap_tiled(bmp, x1, y1, x2, y2, tile_origin_x, tile_origin_y)
 ILI9488 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_line_pixel(x, y, color)
 ILI9488 display driver specific function, see gfx_ili9488_draw_line_pixel. More...
 
#define gfx_draw_pixel(x, y, color)   gfx_ili9488_draw_pixel(x, y, color)
 ILI9488 display driver specific function, see gfx_ili9488_draw_pixel. More...
 
#define gfx_duplicate_pixel(color, count)   ili9488_duplicate_pixel(color, count)
 ILI9488 display driver specific function, see ili9488_duplicate_pixel. More...
 
#define gfx_get_pixel(x, y)   gfx_ili9488_get_pixel(x, y)
 ILI9488 display driver specific function, see gfx_ili9488_get_pixel. More...
 
#define gfx_init()   gfx_ili9488_init()
 ILI9488 display driver specific function, see gfx_ili9488_init. More...
 
#define gfx_put_bitmap(bmp, map_x, map_y, x, y, width, height)   gfx_generic_put_bitmap(bmp, map_x, map_y, x, y, width, height)
 ILI9488 display driver uses generic gfx implementation for this function. More...
 
#define gfx_set_bottom_right_limit(x, y)   ili9488_set_bottom_right_limit(x, y)
 ILI9488 display driver specific function, see ili9488_set_bottom_right_limit. More...
 
#define gfx_set_ext_handler(ext_draw_handler)   gfx_generic_set_ext_handler(ext_draw_handler)
 ILI9488 display driver uses generic gfx implementation for this function. More...
 
#define gfx_set_limits(x1, y1, x2, y2)   ili9488_set_limits(x1, y1, x2, y2)
 ILI9488 display driver specific function, see ili9488_set_limits. More...
 
#define gfx_set_orientation(flags)   gfx_ili9488_set_orientation(flags)
 ILI9488 display driver specific function, see gfx_ili9488_set_orientation. More...
 
#define gfx_set_top_left_limit(x, y)   ili9488_set_top_left_limit(x, y)
 ILI9488 display driver specific function, see ili9488_set_top_left_limit. More...
 
#define gfx_sync()   gfx_generic_sync()
 ILI9488 display driver uses generic gfx implementation for this function. More...
 

Functions

gfx_color_t gfx_ili9488_color (uint8_t r, uint8_t g, uint8_t b)
 Generate native color value from R/G/B values. More...
 
void gfx_ili9488_draw_line_pixel (gfx_coord_t x, gfx_coord_t y, gfx_color_t color)
 Draw a single pixel on the screen. More...
 
void gfx_ili9488_draw_pixel (gfx_coord_t x, gfx_coord_t y, gfx_color_t color)
 Draw a single pixel on the screen. More...
 
gfx_color_t gfx_ili9488_get_pixel (gfx_coord_t x, gfx_coord_t y)
 Get the color of a pixel on the display. More...
 
void gfx_ili9488_init (void)
 Initialize the ili9488 display controller. More...
 
void gfx_ili9488_set_orientation (uint8_t flags)
 Set display orientation. More...
 
gfx_coord_t gfx_height
 Current height of screen. More...
 
gfx_coord_t gfx_width
 Current width of screen. More...
 
gfx_coord_t gfx_min_x
 Minimum X of current clipping region. More...
 
gfx_coord_t gfx_min_y
 Maximum Y of current clipping region. More...
 
gfx_coord_t gfx_max_x
 Minimum X of current clipping region. More...
 
gfx_coord_t gfx_max_y
 Maximum Y of current clipping region. More...
 

Driver-specific Definitions

typedef uint16_t gfx_color_t
 Data type for color values native to the display. More...
 
typedef ili9488_coord_t gfx_coord_t
 Data type representing a coordinate on the screen. More...
 

Graphics Drawing Primitives

#define gfx_draw_horizontal_line(x, y, length, color)   gfx_generic_draw_horizontal_line(x, y, length, color)
 Draw a horizontal line, one pixel wide. More...
 
#define gfx_draw_vertical_line(x, y, length, color)   gfx_generic_draw_vertical_line(x, y, length, color)
 Draw a vertical line, one pixel wide. More...
 
#define gfx_draw_line(x1, y1, x2, y2, color)   gfx_generic_draw_line(x1, y1, x2, y2, color)
 Draw a line between two arbitrary points. More...
 
#define gfx_draw_rect(x, y, width, height, color)   gfx_generic_draw_rect(x, y, width, height, color)
 Draw an outline of a rectangle. More...
 
#define gfx_draw_filled_rect(x, y, width, height, color)   gfx_generic_draw_filled_rect(x, y, width, height, color)
 Draw a filled rectangle. More...
 
#define gfx_draw_circle(x, y, radius, color, octant_mask)   gfx_generic_draw_circle(x, y, radius, color, octant_mask)
 Draw an outline of a circle or arc. More...
 
#define gfx_draw_filled_circle(x, y, radius, color, quadrant_mask)
 Draw a filled circle or sector. More...
 
#define gfx_get_pixmap(pixmap, map_width, map_x, map_y, x, y, width, height)
 Read a rectangular block of pixels from the screen into data memory. More...
 
#define gfx_put_pixmap(pixmap, map_width, map_x, map_y, x, y, width, height)
 Write a rectangular block of pixels stored in data memory to the screen. More...
 

#define gfx_color (   r,
  g,
 
)    gfx_ili9488_color(r, g, b)

ILI9488 display driver specific function, see gfx_ili9488_color.

#define gfx_copy_pixels_from_screen (   pixels,
  count 
)    ili9488_copy_pixels_from_screen(pixels, count)

ILI9488 display driver specific function, see ili9488_copy_pixels_from_screen.

#define gfx_copy_pixels_to_screen (   pixels,
  count 
)    ili9488_copy_pixels_to_screen(pixels, count)

ILI9488 display driver specific function, see ili9488_copy_pixels_to_screen.

#define gfx_copy_progmem_pixels_to_screen (   pixels,
  count 
)    ili9488_copy_progmem_pixels_to_screen(pixels, count)

ILI9488 display driver specific function available for ATmega and ATXmega devices, see ili9488_copy_progmem_pixels_to_screen.

#define gfx_draw_bitmap (   bmp,
  x,
 
)    gfx_generic_draw_bitmap(bmp, x, y)

ILI9488 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_bitmap

#define gfx_draw_bitmap_tiled (   bmp,
  x1,
  y1,
  x2,
  y2,
  tile_origin_x,
  tile_origin_y 
)
Value:
gfx_generic_draw_bitmap_tiled(bmp, x1, y1, x2, y2,\
tile_origin_x, tile_origin_y)
void gfx_generic_draw_bitmap_tiled(const struct gfx_bitmap *bmp, gfx_coord_t x1, gfx_coord_t y1, gfx_coord_t x2, gfx_coord_t y2, gfx_coord_t tile_origin_x, gfx_coord_t tile_origin_y)
Definition: gfx_generic.c:546

ILI9488 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_bitmap_tiled

#define gfx_draw_circle (   x,
  y,
  radius,
  color,
  octant_mask 
)    gfx_generic_draw_circle(x, y, radius, color, octant_mask)

Draw an outline of a circle or arc.

ILI9488 display driver uses generic gfx implementation for this function.

The radius is the distance from the center to the circumference, which means that the total width or height of a circle will be (radius*2+1).

The octant_mask parameter is a bitmask that decides which octants of the circle to draw. Use the GFX_OCTANTn, GFX_QUADRANTn, GFX_xHALF and GFX_WHOLE constants and OR them together if required. Radius equal to zero gives a single pixel.

Parameters
xX coordinate of center.
yY coordinate of center.
radiusCircle radius in pixels.
colorCircle color in display native format.
octant_maskBitmask indicating which octants to draw.

See gfx_generic_draw_circle

Referenced by main().

#define gfx_draw_filled_circle (   x,
  y,
  radius,
  color,
  quadrant_mask 
)
Value:
gfx_generic_draw_filled_circle(x, y, radius, color,\
quadrant_mask)
void gfx_generic_draw_filled_circle(gfx_coord_t x, gfx_coord_t y, gfx_coord_t radius, gfx_color_t color, uint8_t quadrant_mask)
Definition: gfx_generic.c:296

Draw a filled circle or sector.

ILI9488 display driver uses generic gfx implementation for this function.

The radius is the distance from the center to the circumference, which means that the total width or height of a circle will be (radius*2+1).

The quadrant_mask parameter is a bitmask that decides which quadrants of the circle to draw. Use the GFX_QUADRANTn, GFX_xHALF and GFX_WHOLE constants and OR them together if required. Radius equal to zero gives a single pixel.

Note
This function only supports quadrants while gfx_draw_circle() supports octants. This is to improve performance on drawing filled circles.
Parameters
xX coordinate of center.
yY coordinate of center.
radiusCircle radius in pixels.
colorCircle color in display native format.
quadrant_maskBitmask indicating which quadrants to draw.

See gfx_generic_draw_filled_circle

Referenced by main().

#define gfx_draw_filled_rect (   x,
  y,
  width,
  height,
  color 
)    gfx_generic_draw_filled_rect(x, y, width, height, color)

Draw a filled rectangle.

ILI9488 display driver uses generic gfx implementation for this function.

Parameters
xX coordinate of the left side.
yY coordinate of the top side.
widthWidth of the rectangle.
heightHeight of the rectangle.
colorColor of the rectangle, in display native format.

See gfx_generic_draw_filled_rect

Referenced by gfx_draw_char(), gfx_generic_draw_bitmap_tiled(), gfx_generic_draw_horizontal_line(), gfx_generic_draw_vertical_line(), gfx_generic_put_bitmap(), gfx_ili9488_init(), and main().

#define gfx_draw_horizontal_line (   x,
  y,
  length,
  color 
)    gfx_generic_draw_horizontal_line(x, y, length, color)

Draw a horizontal line, one pixel wide.

ILI9488 display driver uses generic gfx implementation for this function.

Parameters
xX coordinate of leftmost pixel.
yY coordinate of the line.
lengthLength of the line in pixels.
colorColor of the line, in display native format.

See gfx_generic_draw_horizontal_line

Referenced by gfx_generic_draw_rect(), and main().

#define gfx_draw_line (   x1,
  y1,
  x2,
  y2,
  color 
)    gfx_generic_draw_line(x1, y1, x2, y2, color)

Draw a line between two arbitrary points.

ILI9488 display driver uses generic gfx implementation for this function.

Parameters
x1Start X coordinate.
y1Start Y coordinate.
x2End X coordinate.
y2End Y coordinate.
colorColor of the line, in display native format.

See gfx_generic_draw_line

Referenced by main().

#define gfx_draw_line_pixel (   x,
  y,
  color 
)
Value:
color)
void gfx_ili9488_draw_line_pixel(gfx_coord_t x, gfx_coord_t y, gfx_color_t color)
Draw a single pixel on the screen.
Definition: gfx_ili9488_90_00028_a0.c:106

ILI9488 display driver specific function, see gfx_ili9488_draw_line_pixel.

#define gfx_draw_pixel (   x,
  y,
  color 
)    gfx_ili9488_draw_pixel(x, y, color)

ILI9488 display driver specific function, see gfx_ili9488_draw_pixel.

#define gfx_draw_rect (   x,
  y,
  width,
  height,
  color 
)    gfx_generic_draw_rect(x, y, width, height, color)

Draw an outline of a rectangle.

ILI9488 display driver uses generic gfx implementation for this function.

Parameters
xX coordinate of the left side.
yY coordinate of the top side.
widthWidth of the rectangle.
heightHeight of the rectangle.
colorColor of the rectangle, in display native format.

See gfx_generic_draw_rect

Referenced by main().

#define gfx_draw_vertical_line (   x,
  y,
  length,
  color 
)    gfx_generic_draw_vertical_line(x, y, length, color)

Draw a vertical line, one pixel wide.

ILI9488 display driver uses generic gfx implementation for this function.

Parameters
xX coordinate of the line.
yY coordinate of the topmost pixel.
lengthLength of the line in pixels.
colorColor of the line, in display native format.

See gfx_generic_draw_vertical_line

Referenced by gfx_generic_draw_filled_circle(), gfx_generic_draw_rect(), and main().

#define gfx_duplicate_pixel (   color,
  count 
)    ili9488_duplicate_pixel(color, count)

ILI9488 display driver specific function, see ili9488_duplicate_pixel.

#define gfx_get_pixel (   x,
 
)    gfx_ili9488_get_pixel(x, y)

ILI9488 display driver specific function, see gfx_ili9488_get_pixel.

#define gfx_get_pixmap (   pixmap,
  map_width,
  map_x,
  map_y,
  x,
  y,
  width,
  height 
)
Value:
gfx_generic_get_pixmap(pixmap, map_width, map_x, map_y, x, y,\
uint8_t height
Definition: gfx_text.h:130
void gfx_generic_get_pixmap(gfx_color_t *pixmap, gfx_coord_t map_width, gfx_coord_t map_x, gfx_coord_t map_y, gfx_coord_t x, gfx_coord_t y, gfx_coord_t width, gfx_coord_t height)
Definition: gfx_generic.c:358
uint8_t width
Definition: gfx_text.h:128

Read a rectangular block of pixels from the screen into data memory.

ILI9488 display driver uses generic gfx implementation for this function.

If the area to read is outside the clipping region, those pixels will not be read, and the corresponding data memory will be left untouched. Note that this function fails if width or height is negative or the pixel rectangle is outside the pixmap buffer extents. Clipping is only performed on the screen, not inside the pixmap buffer itself. Note that there is no checking if the pixel rectangle exceeds the bottom of the pixmap buffer.

Parameters
pixmapPointer to pixel buffer in data memory.
map_widthWidth of the pixel buffer.
map_xX coordinate inside pixel buffer.
map_yY coordinate inside pixel buffer.
xX coordinate on screen.
yY coordinate on screen.
widthWidth of pixel rectangle to copy.
heightHeight of pixel rectangle to copy.

See gfx_generic_get_pixmap

#define gfx_init ( )    gfx_ili9488_init()

ILI9488 display driver specific function, see gfx_ili9488_init.

Referenced by main().

#define gfx_put_bitmap (   bmp,
  map_x,
  map_y,
  x,
  y,
  width,
  height 
)    gfx_generic_put_bitmap(bmp, map_x, map_y, x, y, width, height)

ILI9488 display driver uses generic gfx implementation for this function.

See gfx_generic_put_bitmap

#define gfx_put_pixmap (   pixmap,
  map_width,
  map_x,
  map_y,
  x,
  y,
  width,
  height 
)
Value:
gfx_generic_put_pixmap(pixmap, map_width, map_x, map_y, x, y,\
uint8_t height
Definition: gfx_text.h:130
void gfx_generic_put_pixmap(const gfx_color_t *pixmap, gfx_coord_t map_width, gfx_coord_t map_x, gfx_coord_t map_y, gfx_coord_t x, gfx_coord_t y, gfx_coord_t width, gfx_coord_t height)
Definition: gfx_generic.c:452
uint8_t width
Definition: gfx_text.h:128

Write a rectangular block of pixels stored in data memory to the screen.

ILI9488 display driver uses generic gfx implementation for this function.

If the area to write is outside the clipping region, those pixels will not be written. Note that this function fails if the width or height is negative or the pixel rectangle is outside the pixmap buffer extents. Clipping is only performed on the screen, not inside the pixmap buffer itself. Note that there is no checking if the pixel rectangle exceeds the bottom of the pixmap buffer.

Parameters
pixmapPointer to pixel buffer in data memory.
map_widthWidth of the pixel buffer.
map_xX coordinate inside pixel buffer.
map_yY coordinate inside pixel buffer.
xX coordinate on screen.
yY coordinate on screen.
widthWidth of pixel rectangle to copy.
heightHeight of pixel rectangle to copy.

See gfx_generic_put_pixmap

#define gfx_set_bottom_right_limit (   x,
 
)    ili9488_set_bottom_right_limit(x, y)

ILI9488 display driver specific function, see ili9488_set_bottom_right_limit.

#define gfx_set_ext_handler (   ext_draw_handler)    gfx_generic_set_ext_handler(ext_draw_handler)

ILI9488 display driver uses generic gfx implementation for this function.

See gfx_generic_set_ext_handler

#define gfx_set_limits (   x1,
  y1,
  x2,
  y2 
)    ili9488_set_limits(x1, y1, x2, y2)

ILI9488 display driver specific function, see ili9488_set_limits.

#define gfx_set_orientation (   flags)    gfx_ili9488_set_orientation(flags)

ILI9488 display driver specific function, see gfx_ili9488_set_orientation.

#define gfx_set_top_left_limit (   x,
 
)    ili9488_set_top_left_limit(x, y)

ILI9488 display driver specific function, see ili9488_set_top_left_limit.

#define gfx_sync (   void)    gfx_generic_sync()

ILI9488 display driver uses generic gfx implementation for this function.

See gfx_generic_sync

Data type for color values native to the display.

Data type representing a coordinate on the screen.

gfx_color_t gfx_ili9488_color ( uint8_t  r,
uint8_t  g,
uint8_t  b 
)

Generate native color value from R/G/B values.

Converts 8-bit R/G/B values to a color value native to the display.

The macro GFX_COLOR does the same, only allows the preprocessor to handle the calculations.

Parameters
r8-bit red value.
g8-bit green value.
b8-bit blue value.
Returns
Color value in display native format.

References GFX_COLOR.

void gfx_ili9488_draw_line_pixel ( gfx_coord_t  x,
gfx_coord_t  y,
gfx_color_t  color 
)

Draw a single pixel on the screen.

This function draws a single pixel on screen only setting top limit which makes it more suitable for line drawing. If outside the clipping region, nothing is drawn.

Parameters
xX coordinate of the pixel to be drawn.
yY coordinate of the pixel to be drawn.
colorColor value of the pixel in display native format.

References gfx_max_x, gfx_max_y, gfx_min_x, gfx_min_y, gfx_set_top_left_limit(), and ili9488_write_gram().

void gfx_ili9488_draw_pixel ( gfx_coord_t  x,
gfx_coord_t  y,
gfx_color_t  color 
)

Draw a single pixel on the screen.

Draw a single pixel on screen setting top and bottom limits. If outside the clipping region, nothing is drawn.

Parameters
xX coordinate of the pixel to be drawn.
yY coordinate of the pixel to be drawn.
colorColor value of the pixel in display native format.

References gfx_max_x, gfx_max_y, gfx_min_x, gfx_min_y, gfx_set_limits(), and ili9488_write_gram().

gfx_color_t gfx_ili9488_get_pixel ( gfx_coord_t  x,
gfx_coord_t  y 
)

Get the color of a pixel on the display.

Parameters
xX coordinate of the pixel to be sampled.
yY coordinate of the pixel to be sampled.
Returns
Color value of the pixel at (x, y) in display native format, or GFX_COLOR_INVALID if outside the clipping region.

References gfx_bitmap::color, GFX_COLOR_INVALID, gfx_max_x, gfx_max_y, gfx_min_x, gfx_min_y, gfx_set_limits(), and ili9488_read_gram().

void gfx_ili9488_init ( void  )

Initialize the ili9488 display controller.

This function will be called when calling gfx_init. It will draw a black background to the display and enable the display backlight if available.

References ili9488_opt_t::background_color, COLOR_BLACK, COLOR_WHITE, ili9488_opt_t::foreground_color, GFX_COLOR_BLACK, gfx_draw_filled_rect, gfx_height, gfx_set_clipping(), gfx_width, ili9488_display_on(), ili9488_init(), ILI9488_LCD_HEIGHT, ILI9488_LCD_WIDTH, ili9488_opt_t::ul_height, and ili9488_opt_t::ul_width.

void gfx_ili9488_set_orientation ( uint8_t  flags)