Microchip® Advanced Software Framework

xmega_a1u_xplained_pro.h File Reference

XMEGA-A1U Xplained Pro board definition.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include <conf_board.h>
#include <compiler.h>

Macros

#define BOARD_NAME   "XMEGA_A1U_XPLAINED_PRO"
 Name string macro. More...
 
#define BUTTON_COUNT   1
 Number of on-board buttons. More...
 
#define LED_COUNT   1
 Number of on-board LEDs. More...
 
LED0 definitions
#define LED0_PIN   IOPORT_CREATE_PIN(PORTQ, 3)
 
#define LED0_ACTIVE   false
 
#define LED0_INACTIVE   !LED0_ACTIVE
 
SW0 definitions
#define SW0_PIN   IOPORT_CREATE_PIN(PORTQ, 2)
 
#define SW0_ACTIVE   false
 
#define SW0_INACTIVE   !SW0_ACTIVE
 
external osc definitions
#define BOARD_XOSC_HZ   32768
 
#define BOARD_XOSC_TYPE   XOSC_TYPE_32KHZ
 
#define BOARD_XOSC_STARTUP_US   1000000
 
LED #0 definitions

Wrapper macros for LED0, to ensure common naming across all Xplained Pro boards.

#define LED_0_NAME   "LED0 (yellow)"
 
#define LED_0_PIN   LED0_PIN
 
#define LED_0_ACTIVE   LED0_ACTIVE
 
#define LED_0_INACTIVE   LED0_INACTIVE
 
#define LED0_GPIO   LED0_PIN
 
Button #0 definitions

Wrapper macros for SW0, to ensure common naming across all Xplained Pro boards.

#define BUTTON_0_NAME   "SW0"
 
#define BUTTON_0_PIN   SW0_PIN
 
#define BUTTON_0_ACTIVE   SW0_ACTIVE
 
#define BUTTON_0_INACTIVE   SW0_INACTIVE
 
Extension header #1 pin definitions
#define EXT1_PIN_3   IOPORT_CREATE_PIN(PORTA,0)
 
#define EXT1_PIN_4   IOPORT_CREATE_PIN(PORTA,4)
 
#define EXT1_PIN_5   IOPORT_CREATE_PIN(PORTE,6)
 
#define EXT1_PIN_6   IOPORT_CREATE_PIN(PORTE,7)
 
#define EXT1_PIN_7   IOPORT_CREATE_PIN(PORTE,1)
 
#define EXT1_PIN_8   IOPORT_CREATE_PIN(PORTE,0)
 
#define EXT1_PIN_9   IOPORT_CREATE_PIN(PORTR,0)
 
#define EXT1_PIN_10   IOPORT_CREATE_PIN(PORTR,1)
 
#define EXT1_PIN_11   IOPORT_CREATE_PIN(PORTC,0)
 
#define EXT1_PIN_12   IOPORT_CREATE_PIN(PORTC,1)
 
#define EXT1_PIN_13   IOPORT_CREATE_PIN(PORTC,2)
 
#define EXT1_PIN_14   IOPORT_CREATE_PIN(PORTC,3)
 
#define EXT1_PIN_15   IOPORT_CREATE_PIN(PORTC,4)
 
#define EXT1_PIN_16   IOPORT_CREATE_PIN(PORTC,5)
 
#define EXT1_PIN_17   IOPORT_CREATE_PIN(PORTC,6)
 
#define EXT1_PIN_18   IOPORT_CREATE_PIN(PORTC,7)
 
Extension header #1 pin definitions by function
#define EXT1_PIN_ADC_0   EXT1_PIN_3
 
#define EXT1_PIN_ADC_1   EXT1_PIN_4
 
#define EXT1_PIN_GPIO_0   EXT1_PIN_5
 
#define EXT1_PIN_GPIO_1   EXT1_PIN_6
 
#define EXT1_PIN_PWM_0   EXT1_PIN_7
 
#define EXT1_PIN_PWM_1   EXT1_PIN_8
 
#define EXT1_PIN_IRQ   EXT1_PIN_9
 
#define EXT1_PIN_I2C_SDA   EXT1_PIN_11
 
#define EXT1_PIN_I2C_SCL   EXT1_PIN_12
 
#define EXT1_PIN_UART_RX   EXT1_PIN_13
 
#define EXT1_PIN_UART_TX   EXT1_PIN_14
 
#define EXT1_PIN_SPI_SS_1   EXT1_PIN_10
 
#define EXT1_PIN_SPI_SS_0   EXT1_PIN_15
 
#define EXT1_PIN_SPI_MOSI   EXT1_PIN_16
 
#define EXT1_PIN_SPI_MISO   EXT1_PIN_17
 
#define EXT1_PIN_SPI_SCK   EXT1_PIN_18
 
Extension header #1 ADC definitions
#define EXT1_ADC_MODULE   ADCA
 
#define EXT1_ADC_0_CHANNEL   4
 
#define EXT1_ADC_1_CHANNEL   0
 
Extension header #1 PWM definitions
#define EXT1_PWM_MODULE   TCE0
 
Extension header #1 SPI definitions
#define EXT1_SPI_MODULE   &SPIC
 
Extension header #1 TWI definitions
#define EXT1_TWI_MODULE   TWIC
 
Extension header #1 USART definitions
#define EXT1_USART_MODULE   &USARTC0
 
Extension header #2 pin definitions
#define EXT2_PIN_3   IOPORT_CREATE_PIN(PORTA,1)
 
#define EXT2_PIN_4   IOPORT_CREATE_PIN(PORTA,6)
 
#define EXT2_PIN_5   IOPORT_CREATE_PIN(PORTB,4)
 
#define EXT2_PIN_6   IOPORT_CREATE_PIN(PORTB,5)
 
#define EXT2_PIN_7   IOPORT_CREATE_PIN(PORTE,5)
 
#define EXT2_PIN_8   IOPORT_CREATE_PIN(PORTE,4)
 
#define EXT2_PIN_9   IOPORT_CREATE_PIN(PORTB,6)
 
#define EXT2_PIN_10   IOPORT_CREATE_PIN(PORTB,7)
 
#define EXT2_PIN_11   IOPORT_CREATE_PIN(PORTF,0)
 
#define EXT2_PIN_12   IOPORT_CREATE_PIN(PORTF,1)
 
#define EXT2_PIN_13   IOPORT_CREATE_PIN(PORTF,2)
 
#define EXT2_PIN_14   IOPORT_CREATE_PIN(PORTF,3)
 
#define EXT2_PIN_15   IOPORT_CREATE_PIN(PORTF,4)
 
#define EXT2_PIN_16   IOPORT_CREATE_PIN(PORTC,5)
 
#define EXT2_PIN_17   IOPORT_CREATE_PIN(PORTC,6)
 
#define EXT2_PIN_18   IOPORT_CREATE_PIN(PORTC,7)
 
Extension header #2 pin definitions by function
#define EXT2_PIN_ADC_0   EXT2_PIN_3
 
#define EXT2_PIN_ADC_1   EXT2_PIN_4
 
#define EXT2_PIN_GPIO_0   EXT2_PIN_5
 
#define EXT2_PIN_GPIO_1   EXT2_PIN_6
 
#define EXT2_PIN_PWM_0   EXT2_PIN_7
 
#define EXT2_PIN_PWM_1   EXT2_PIN_8
 
#define EXT2_PIN_IRQ   EXT2_PIN_9
 
#define EXT2_PIN_I2C_SDA   EXT2_PIN_11
 
#define EXT2_PIN_I2C_SCL   EXT2_PIN_12
 
#define EXT2_PIN_UART_RX   EXT2_PIN_13
 
#define EXT2_PIN_UART_TX   EXT2_PIN_14
 
#define EXT2_PIN_SPI_SS_1   EXT2_PIN_10
 
#define EXT2_PIN_SPI_SS_0   EXT2_PIN_15
 
#define EXT2_PIN_SPI_MOSI   EXT2_PIN_16
 
#define EXT2_PIN_SPI_MISO   EXT2_PIN_17
 
#define EXT2_PIN_SPI_SCK   EXT2_PIN_18
 
Extension header #2 ADC definitions
#define EXT2_ADC_MODULE   ADCA
 
#define EXT2_ADC_0_CHANNEL   6
 
#define EXT2_ADC_1_CHANNEL   1
 
Extension header #2 PWM definitions
#define EXT2_PWM_MODULE   TCE1
 
Extension header #2 SPI definitions
#define EXT2_SPI_MODULE   &SPIC
 
Extension header #2 TWI definitions
#define EXT2_TWI_MODULE   TWIF
 
Extension header #2 USART definitions
#define EXT2_USART_MODULE   &USARTF0
 
Extension header #3 pin definitions
#define EXT3_PIN_3   IOPORT_CREATE_PIN(PORTA,3)
 
#define EXT3_PIN_4   IOPORT_CREATE_PIN(PORTA,7)
 
#define EXT3_PIN_5   IOPORT_CREATE_PIN(PORTK,0)
 
#define EXT3_PIN_6   IOPORT_CREATE_PIN(PORTK,1)
 
#define EXT3_PIN_7   IOPORT_CREATE_PIN(PORTD,5)
 
#define EXT3_PIN_8   IOPORT_CREATE_PIN(PORTD,4)
 
#define EXT3_PIN_9   IOPORT_CREATE_PIN(PORTK,2)
 
#define EXT3_PIN_10   IOPORT_CREATE_PIN(PORTK,3)
 
#define EXT3_PIN_11   IOPORT_CREATE_PIN(PORTF,0)
 
#define EXT3_PIN_12   IOPORT_CREATE_PIN(PORTF,1)
 
#define EXT3_PIN_13   IOPORT_CREATE_PIN(PORTF,6)
 
#define EXT3_PIN_14   IOPORT_CREATE_PIN(PORTF,7)
 
#define EXT3_PIN_15   IOPORT_CREATE_PIN(PORTD,0)
 
#define EXT3_PIN_16   IOPORT_CREATE_PIN(PORTC,5)
 
#define EXT3_PIN_17   IOPORT_CREATE_PIN(PORTC,6)
 
#define EXT3_PIN_18   IOPORT_CREATE_PIN(PORTC,7)
 
Extension header #3 pin definitions by function
#define EXT3_PIN_ADC_0   EXT3_PIN_3
 
#define EXT3_PIN_ADC_1   EXT3_PIN_4
 
#define EXT3_PIN_GPIO_0   EXT3_PIN_5
 
#define EXT3_PIN_GPIO_1   EXT3_PIN_6
 
#define EXT3_PIN_PWM_0   EXT3_PIN_7
 
#define EXT3_PIN_PWM_1   EXT3_PIN_8
 
#define EXT3_PIN_IRQ   EXT3_PIN_9
 
#define EXT3_PIN_I2C_SDA   EXT3_PIN_11
 
#define EXT3_PIN_I2C_SCL   EXT3_PIN_12
 
#define EXT3_PIN_UART_RX   EXT3_PIN_13
 
#define EXT3_PIN_UART_TX   EXT3_PIN_14
 
#define EXT3_PIN_SPI_SS_1   EXT3_PIN_10
 
#define EXT3_PIN_SPI_SS_0   EXT3_PIN_15
 
#define EXT3_PIN_SPI_MOSI   EXT3_PIN_16
 
#define EXT3_PIN_SPI_MISO   EXT3_PIN_17
 
#define EXT3_PIN_SPI_SCK   EXT3_PIN_18
 
Extension header #3 ADC definitions
#define EXT3_ADC_MODULE   ADCA
 
#define EXT3_ADC_0_CHANNEL   7
 
#define EXT3_ADC_1_CHANNEL   3
 
Extension header #3 PWM definitions
#define EXT3_PWM_MODULE   TCD1
 
Extension header #3 SPI definitions
#define EXT3_SPI_MODULE   &SPIC
 
Extension header #3 TWI definitions
#define EXT3_TWI_MODULE   TWIF
 
Extension header #3 USART definitions
#define EXT3_USART_MODULE   &USARTF1
 
Embedded debugger GPIO interface definitions
#define EDBG_GPIO0_PIN   IOPORT_CREATE_PIN(PORTK,4)
 
#define EDBG_GPIO1_PIN   IOPORT_CREATE_PIN(PORTK,5)
 
#define EDBG_GPIO2_PIN   IOPORT_CREATE_PIN(PORTK,6)
 
#define EDBG_GPIO3_PIN   IOPORT_CREATE_PIN(PORTK,7)
 
Embedded debugger USART interface definitions
#define EDBG_UART_MODULE   &USARTE0
 
Embedded debugger TWI interface definitions
#define EDBG_TWI_MODULE   TWIC
 
EBI_DATA_ADDR definitions
#define EBI_DATA_ADDR_D7_A7_A15   IOPORT_CREATE_PIN(PORTJ,7)
 
#define EBI_DATA_ADDR_D6_A6_A14   IOPORT_CREATE_PIN(PORTJ,6)
 
#define EBI_DATA_ADDR_D5_A5_A13   IOPORT_CREATE_PIN(PORTJ,5)
 
#define EBI_DATA_ADDR_D4_A4_A12   IOPORT_CREATE_PIN(PORTJ,4)
 
#define EBI_DATA_ADDR_D3_A3_A11   IOPORT_CREATE_PIN(PORTJ,3)
 
#define EBI_DATA_ADDR_D2_A2_A10   IOPORT_CREATE_PIN(PORTJ,2)
 
#define EBI_DATA_ADDR_D1_A1_A9   IOPORT_CREATE_PIN(PORTJ,1)
 
#define EBI_DATA_ADDR_D0_A0_A8   IOPORT_CREATE_PIN(PORTJ,0)
 
EBI_CTRL_ADDR definitions
#define EBI_CTRL_ADDR_ALE1   IOPORT_CREATE_PIN(PORTH,2)
 
#define EBI_CTRL_ADDR_ALE2   IOPORT_CREATE_PIN(PORTH,3)
 
#define EBI_CTRL_ADDR_WE   IOPORT_CREATE_PIN(PORTH,0)
 
#define EBI_CTRL_ADDR_RE   IOPORT_CREATE_PIN(PORTH,1)
 
#define EBI_CTRL_ADDR_CS   IOPORT_CREATE_PIN(PORTH,6)
 
#define EBI_CTRL_ADDR_A18   IOPORT_CREATE_PIN(PORTK,7)
 
#define EBI_CTRL_ADDR_A17   IOPORT_CREATE_PIN(PORTH,5)
 
#define EBI_CTRL_ADDR_A16   IOPORT_CREATE_PIN(PORTH,4)
 
LCD_CTRL definitions
#define LCD_BACKLIGHT_PWM   IOPORT_CREATE_PIN(PORTF,5)
 
#define LCD_DISPLAY_CS   IOPORT_CREATE_PIN(PORTH,7)
 
#define LCD_DISPLAY_ENABLE   IOPORT_CREATE_PIN(PORTK,5)
 
#define LCD_DISPLAY_RESET   IOPORT_CREATE_PIN(PORTA,5)
 
#define LCD_DISPLAY_WE   IOPORT_CREATE_PIN(PORTH,0)
 
#define LCD_DISPLAY_RE   IOPORT_CREATE_PIN(PORTH,1)
 
#define LCD_TWI_SDA   IOPORT_CREATE_PIN(PORTC,0)
 
#define LCD_TWI_SCL   IOPORT_CREATE_PIN(PORTC,1)
 
#define LCD_IRQ1   IOPORT_CREATE_PIN(PORTK,4)
 
#define LCD_IRQ2   IOPORT_CREATE_PIN(PORTK,6)
 
#define LCD_SPI_MOSI   IOPORT_CREATE_PIN(PORTC,5)
 
#define LCD_SPI_MISO   IOPORT_CREATE_PIN(PORTC,6)
 
#define LCD_SPI_SCK   IOPORT_CREATE_PIN(PORTC,7)
 
#define LCD_SPI_CS   IOPORT_CREATE_PIN(PORTB,1)
 
AT86RFX definitions
#define AT86RFX_SPI   EXT1_SPI_MODULE
 
#define AT86RFX_RST_PIN   EXT1_PIN_7
 
#define AT86RFX_MISC_PIN   EXT1_PIN_12
 
#define AT86RFX_IRQ_PIN   EXT1_PIN_9
 
#define AT86RFX_SLP_PIN   EXT1_PIN_10
 
#define AT86RFX_SPI_CS   EXT1_PIN_15
 
#define AT86RFX_SPI_MOSI   EXT1_PIN_16
 
#define AT86RFX_SPI_MISO   EXT1_PIN_17
 
#define AT86RFX_SPI_SCK   EXT1_PIN_18
 
#define AT86RFX_CSD   EXT1_PIN_5
 
#define AT86RFX_CPS   EXT1_PIN_8
 
SPI Connections of external AT45DBX Data Flash Memory

This is mainly used for proper board compilation

#define AT45DBX_SPI   &SPIC
 
#define AT45DBX_CS   EXT1_PIN_GPIO_0
 
#define AT45DBX_MASTER_SCK   EXT1_PIN_SPI_SCK
 
#define AT45DBX_MASTER_SS   EXT1_PIN_SPI_SS_1
 
#define AT45DBX_MASTER_MOSI   EXT1_PIN_SPI_MOSI
 
#define AT45DBX_MASTER_MISO   EXT1_PIN_SPI_MISO
 
#define AT45DBX_SPI_CLK_MASK   SYSCLK_PORT_C
 

Functions

void board_init (void)
 This function initializes the board target resources. More...