This is an example application for the Monochrome graphical display system. It will output some random graphic primitives to a connected LCD screen or framebuffer.
All AVR devices can be used. This example has been tested with the following setup:
Relevant module dependencies for this application are:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.