This service will add the possibility to dump the LCD screen to the USART using the XPM file format.
Before using the screen dump function one should make sure that one has performed initialization of this service by calling gfx_mono_screen_dump_init() to set up which USART to use. One should also make sure that one has initialized the gfx mono driver gfx_mono_init() which will produce the screen buffer that is dumped trough the USART.
This driver depends on the following modules:
Macros | |
#define | _XPM_HEADER(w, h) |
#define | GFX_MONO_LCD_PAGE_COUNT GFX_MONO_LCD_HEIGHT / LCD_PAGE_HEIGHT |
#define | LCD_PAGE_HEIGHT 8 |
TODO: This define should be fetched from the GFX display header file. More... | |
#define | str(s) # s |
#define | XPM_HEADER _XPM_HEADER(GFX_MONO_LCD_WIDTH, GFX_MONO_LCD_HEIGHT) |
Functions | |
static void | gfx_mono_screen_dump (void) |
Function for dumping a LCD framebuffer. More... | |
static void | gfx_mono_screen_dump_init (dump_usart_t *usart, const usart_serial_options_t *options) |
Init the framebuffer dump function. More... | |
Variables | |
dump_usart_t * | dump_usart |
storage for the usart to use when dumping data More... | |
static const uint8_t | xpm_header [] = XPM_HEADER |
#define _XPM_HEADER | ( | w, | |
h | |||
) |
#define GFX_MONO_LCD_PAGE_COUNT GFX_MONO_LCD_HEIGHT / LCD_PAGE_HEIGHT |
Referenced by gfx_mono_screen_dump().
#define LCD_PAGE_HEIGHT 8 |
TODO: This define should be fetched from the GFX display header file.
Referenced by gfx_mono_screen_dump().
#define str | ( | s | ) | # s |
#define XPM_HEADER _XPM_HEADER(GFX_MONO_LCD_WIDTH, GFX_MONO_LCD_HEIGHT) |
|
inlinestatic |
Function for dumping a LCD framebuffer.
This function will dump a framebuffer to a UART in XPM file format.
References gfx_mono_get_page, GFX_MONO_LCD_PAGE_COUNT, GFX_MONO_LCD_WIDTH, LCD_PAGE_HEIGHT, usart_putchar(), usart_serial_getchar(), and usart_serial_write_packet().
Referenced by main().
|
inlinestatic |
Init the framebuffer dump function.
usart | pointer to the USART to use for dumping the image |
options | pointer to the USART options, for documentation see usart_serial_options_t |
References usart_serial_init().
Referenced by main().
dump_usart_t* dump_usart |
storage for the usart to use when dumping data
|
static |