Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
XMEGA compiler driver

Compiler abstraction layer and code utilities for 8-bit AVR.

This module provides various abstraction layers and utilities to make code compatible between different compilers.

Modules

 Assembler Support
 This group provides a good handful of macros intended to smooth out the differences between various assemblers, similar to what compiler.h does for compilers, except that assemblers tend to be much less standardized than compilers.
 
 Macro Repeat
 
 Stringize
 
 Token Paste
 
 Program memory
 
 Status Codes
 

Data Structures

struct  StructCPtr
 Structure of pointers to constant 64-, 32-, 16- and 8-bit unsigned integers. More...
 
struct  StructCVPtr
 Structure of pointers to constant volatile 64-, 32-, 16- and 8-bit unsigned integers. More...
 
struct  StructPtr
 Structure of pointers to 64-, 32-, 16- and 8-bit unsigned integers. More...
 
struct  StructVPtr
 Structure of pointers to volatile 64-, 32-, 16- and 8-bit unsigned integers. More...
 
union  Union16
 16-bit union. More...
 
union  Union32
 32-bit union. More...
 
union  Union64
 64-bit union. More...
 
union  UnionCPtr
 Union of pointers to constant 64-, 32-, 16- and 8-bit unsigned integers. More...
 
union  UnionCVPtr
 Union of pointers to constant volatile 64-, 32-, 16- and 8-bit unsigned integers. More...
 
union  UnionPtr
 Union of pointers to 64-, 32-, 16- and 8-bit unsigned integers. More...
 
union  UnionVPtr
 Union of pointers to volatile 64-, 32-, 16- and 8-bit unsigned integers. More...
 

Macros

#define __always_inline   inline __attribute__((__always_inline__))
 The function should always be inlined. More...
 
#define ADDR_COPY_DST_SRC_16(dst, src)   memcpy((&(dst)), (&(src)), sizeof(uint16_t))
 
#define ADDR_COPY_DST_SRC_64(dst, src)   memcpy((&(dst)), (&(src)), sizeof(uint64_t))
 
#define Assert(expr)   ((void) 0)
 This macro is used to test fatal errors. More...
 
#define barrier()   asm volatile("" ::: "memory")
 Memory barrier. More...
 
#define CCPU_ENDIAN_TO_LE16(x)   (x)
 
#define CCPU_ENDIAN_TO_LE32(x)   (x)
 
#define CCPU_ENDIAN_TO_LE64(x)   (x)
 
#define CLE16_TO_CPU_ENDIAN(x)   (x)
 
#define CLE32_TO_CPU_ENDIAN(x)   (x)
 
#define CLE64_TO_CPU_ENDIAN(x)   (x)
 
#define CMD_ID_OCTET   (0)
 
#define COMPILER_ALIGNED(a)   __attribute__((__aligned__(a)))
 Set aligned boundary. More...
 
#define COMPILER_PACK_RESET(alignment)
 
#define COMPILER_PACK_SET(alignment)
 
#define COMPILER_PRAGMA(arg)   _Pragma(#arg)
 Emit the compiler pragma arg. More...
 
#define COMPILER_WORD_ALIGNED   __attribute__((__aligned__(2)))
 Set word-aligned boundary. More...
 
#define convert_16_bit_to_byte_address(value, data)   ((*(uint16_t *)(data)) = (uint16_t)(value))
 
#define convert_16_bit_to_byte_array(value, data)   ((*(uint16_t *)(data)) = (uint16_t)(value))
 
#define convert_32_bit_to_byte_array(value, data)   ((*(uint32_t *)(data)) = (uint32_t)(value))
 
#define convert_64_bit_to_byte_array(value, data)   memcpy((data), (&(value)), sizeof(uint64_t))
 
#define convert_byte_array_to_16_bit(data)   (*(uint16_t *)(data))
 
#define convert_byte_array_to_32_bit(data)   (*(uint32_t *)(data))
 
#define convert_byte_array_to_64_bit(data)   (*(uint64_t *)(data))
 
#define convert_spec_16_bit_to_byte_array(value, data)   ((*(uint16_t *)(data)) = (uint16_t)(value))
 
#define CPU_ENDIAN_TO_LE16(x)   (x)
 
#define CPU_ENDIAN_TO_LE32(x)   (x)
 
#define CPU_ENDIAN_TO_LE64(x)   (x)
 
#define div_ceil(a, b)   (((a) + (b) - 1) / (b))
 Calculate \( \left\lceil \frac{a}{b} \right\rceil \) using integer arithmetic. More...
 
#define FLASH_DECLARE(x)   const x __attribute__((__progmem__))
 
#define FLASH_EXTERN(x)   extern const x
 
#define FUNC_PTR   void *
 
#define LE16_TO_CPU_ENDIAN(x)   (x)
 
#define LE32_TO_CPU_ENDIAN(x)   (x)
 
#define LE64_TO_CPU_ENDIAN(x)   (x)
 
#define Long_call(addr)   ((*(void (*)(void))(addr))())
 Calls the routine at address addr. More...
 
#define MEMCPY_ENDIAN   memcpy
 
#define nop()   do { __asm__ __volatile__ ("nop"); } while (0)
 
#define PGM_READ_BLOCK(dst, src, len)   memcpy_P((dst), (src), (len))
 
#define PGM_READ_BYTE(x)   pgm_read_byte(x)
 
#define PGM_READ_WORD(x)   pgm_read_word(x)
 
#define SHORTENUM   __attribute__ ((packed))
 
#define UNUSED(v)   (void)(v)
 Marking v as a unused parameter or value. More...
 
#define unused(v)   do { (void)(v); } while(0)
 Marking v as a unused parameter or value. More...
 

Tag functions as deprecated

Tagging a function as deprecated will produce a warning when and only when the function is called.

Usage is to add the DEPRECATED symbol before the function definition. E.g.: DEPRECATED uint8_t some_deprecated_function (void) { ... }

Note
Only supported by GCC 3.1 and above, no IAR support
#define __DEPRECATED__   __attribute__((__deprecated__))
 

Usual Types

typedef unsigned char Bool
 Boolean. More...
 
typedef unsigned char bool
 Boolean. More...
 
typedef int8_t S8
 8-bit signed integer. More...
 
typedef uint8_t U8
 8-bit unsigned integer. More...
 
typedef int16_t S16
 16-bit signed integer. More...
 
typedef uint16_t U16
 16-bit unsigned integer. More...
 
typedef uint16_t le16_t
 
typedef uint16_t be16_t
 
typedef int32_t S32
 32-bit signed integer. More...
 
typedef uint32_t U32
 32-bit unsigned integer. More...
 
typedef uint32_t le32_t
 
typedef uint32_t be32_t
 
typedef int64_t S64
 64-bit signed integer. More...
 
typedef uint64_t U64
 64-bit unsigned integer. More...
 
typedef float F32
 32-bit floating-point number. More...
 
typedef double F64
 64-bit floating-point number. More...
 
typedef uint16_t iram_size_t
 

Status Types

typedef Bool Status_bool_t
 Boolean status. More...
 
typedef U8 Status_t
 8-bit-coded status. More...
 

Usual Constants

#define DISABLE   0
 
#define ENABLE   1
 
#define false   0
 
#define true   1
 
#define PASS   0
 
#define FAIL   1
 
#define LOW   0
 
#define HIGH   1
 

Compile time error handling

#define ERROR_FUNC(name, msg)   extern int name(void)
 Fail compilation if function call isn't eliminated. More...
 

Function call demultiplexing

 ERROR_FUNC (compiler_demux_bad_size,"Invalid parameter size")
 Error function for failed demultiplexing. More...
 
#define compiler_demux_size(size, func,...)
 Demultiplex function call based on size of datatype. More...
 

Optimization Control

#define __always_optimize   __attribute__((optimize(3)))
 The function should always be optimized. More...
 
#define likely(exp)   (exp)
 The expression exp is likely to be true. More...
 
#define unlikely(exp)   (exp)
 The expression exp is unlikely to be true. More...
 
#define is_constant(exp)   __builtin_constant_p(exp)
 Determine if an expression evaluates to a constant value. More...
 

Bit-Field Handling

#define Rd_bits(value, mask)   ((value)&(mask))
 Reads the bits of a value specified by a given bit-mask. More...
 
#define Wr_bits(lvalue, mask, bits)
 Writes the bits of a C lvalue specified by a given bit-mask. More...
 
#define Tst_bits(value, mask)   (Rd_bits(value, mask) != 0)
 Tests the bits of a value specified by a given bit-mask. More...
 
#define Clr_bits(lvalue, mask)   ((lvalue) &= ~(mask))
 Clears the bits of a C lvalue specified by a given bit-mask. More...
 
#define Set_bits(lvalue, mask)   ((lvalue) |= (mask))
 Sets the bits of a C lvalue specified by a given bit-mask. More...
 
#define Tgl_bits(lvalue, mask)   ((lvalue) ^= (mask))
 Toggles the bits of a C lvalue specified by a given bit-mask. More...
 
#define Rd_bitfield(value, mask)   (Rd_bits( value, (uint32_t)mask) >> ctz(mask))
 Reads the bit-field of a value specified by a given bit-mask. More...
 
#define Wr_bitfield(lvalue, mask, bitfield)   (Wr_bits(lvalue, mask, (uint32_t)(bitfield) << ctz(mask)))
 Writes the bit-field of a C lvalue specified by a given bit-mask. More...
 

Bit Reversing

#define bit_reverse8(u8)   ((U8)(bit_reverse32((U8)(u8)) >> 24))
 Reverses the bits of u8. More...
 
#define bit_reverse16(u16)   ((U16)(bit_reverse32((U16)(u16)) >> 16))
 Reverses the bits of u16. More...
 
#define bit_reverse32(u32)
 Reverses the bits of u32. More...
 
#define bit_reverse64(u64)
 Reverses the bits of u64. More...
 

Logarithmic functions

int_fast8_t ilog2_undefined (void)
 
static int_fast8_t ilog2 (uint32_t x)
 Calculate the base-2 logarithm of a number rounded down to the nearest integer. More...
 

Alignment

#define Test_align(val, n)   (!Tst_bits( val, (n) - 1 ) )
 Tests alignment of the number val with the n boundary. More...
 
#define Get_align(val, n)   ( Rd_bits( val, (n) - 1 ) )
 Gets alignment of the number val with respect to the n boundary. More...
 
#define Set_align(lval, n, alg)   ( Wr_bits(lval, (n) - 1, alg) )
 Sets alignment of the lvalue number lval to alg with respect to the n boundary. More...
 
#define Align_up(val, n)   (((val) + ((n) - 1)) & ~((n) - 1))
 Aligns the number val with the upper n boundary. More...
 
#define Align_down(val, n)   ( (val) & ~((n) - 1))
 Aligns the number val with the lower n boundary. More...
 

Mathematics

Compiler optimization for non-constant expressions, only for abs under WinAVR

#define Abs(a)   (((a) < 0 ) ? -(a) : (a))
 Takes the absolute value of a. More...
 
#define abs(a)   Abs(a)
 
#define Min(a, b)   (((a) < (b)) ? (a) : (b))
 Takes the minimal value of a and b. More...
 
#define min(a, b)   Min(a, b)
 
#define Max(a, b)   (((a) > (b)) ? (a) : (b))
 Takes the maximal value of a and b. More...
 
#define max(a, b)   Max(a, b)
 

System Register Access

#define Get_system_register(sysreg)   __builtin_mfsr(sysreg)
 Gets the value of the sysreg system register. More...
 
#define Set_system_register(sysreg, value)   __builtin_mtsr(sysreg, value)
 Sets the value of the sysreg system register to value. More...
 

Debug Register Access

#define Get_debug_register(dbgreg)   __builtin_mfdr(dbgreg)
 Gets the value of the dbgreg debug register. More...
 
#define Set_debug_register(dbgreg, value)   __builtin_mtdr(dbgreg, value)
 Sets the value of the dbgreg debug register to value. More...
 

MCU Endianism Handling

xmega is a MCU little endianism.

#define MSB(u16)   (((uint8_t* )&u16)[1])
 
#define LSB(u16)   (((uint8_t* )&u16)[0])
 
#define MSW(u32)   (((uint16_t*)&u32)[1])
 
#define LSW(u32)   (((uint16_t*)&u32)[0])
 
#define MSB0W(u32)   (((uint8_t*)&(u32))[3])
 Most significant byte of 1st rank of u32. More...
 
#define MSB1W(u32)   (((uint8_t*)&(u32))[2])
 Most significant byte of 2nd rank of u32. More...
 
#define MSB2W(u32)   (((uint8_t*)&(u32))[1])
 Most significant byte of 3rd rank of u32. More...
 
#define MSB3W(u32)   (((uint8_t*)&(u32))[0])
 Most significant byte of 4th rank of u32. More...
 
#define LSB3W(u32)   MSB0W(u32)
 Least significant byte of 4th rank of u32. More...
 
#define LSB2W(u32)   MSB1W(u32)
 Least significant byte of 3rd rank of u32. More...
 
#define LSB1W(u32)   MSB2W(u32)
 Least significant byte of 2nd rank of u32. More...
 
#define LSB0W(u32)   MSB3W(u32)
 Least significant byte of 1st rank of u32. More...
 
#define MSB0(u32)   (((uint8_t*)&u32)[3])
 
#define MSB1(u32)   (((uint8_t*)&u32)[2])
 
#define MSB2(u32)   (((uint8_t*)&u32)[1])
 
#define MSB3(u32)   (((uint8_t*)&u32)[0])
 
#define LSB0(u32)   MSB3(u32)
 
#define LSB1(u32)   MSB2(u32)
 
#define LSB2(u32)   MSB1(u32)
 
#define LSB3(u32)   MSB0(u32)
 
#define LE16(x)   (x)
 
#define le16_to_cpu(x)   (x)
 
#define cpu_to_le16(x)   (x)
 
#define LE16_TO_CPU(x)   (x)
 
#define CPU_TO_LE16(x)   (x)
 
#define BE16(x)   Swap16(x)
 
#define be16_to_cpu(x)   swap16(x)
 
#define cpu_to_be16(x)   swap16(x)
 
#define BE16_TO_CPU(x)   Swap16(x)
 
#define CPU_TO_BE16(x)   Swap16(x)
 
#define LE32(x)   (x)
 
#define le32_to_cpu(x)   (x)
 
#define cpu_to_le32(x)   (x)
 
#define LE32_TO_CPU(x)   (x)
 
#define CPU_TO_LE32(x)   (x)
 
#define BE32(x)   Swap32(x)
 
#define be32_to_cpu(x)   swap32(x)
 
#define cpu_to_be32(x)   swap32(x)
 
#define BE32_TO_CPU(x)   Swap32(x)
 
#define CPU_TO_BE32(x)   Swap32(x)
 

Endianism Conversion

The same considerations as for clz and ctz apply here but AVR32-GCC's __builtin_bswap_16 and __builtin_bswap_32 do not behave like macros when applied to constant expressions, so two sets of macros are defined here:

  • Swap16, Swap32 and Swap64 to apply to constant expressions (values known at compile time);
  • swap16, swap32 and swap64 to apply to non-constant expressions (values unknown at compile time).
#define Swap16(u16)
 Toggles the endianism of u16 (by swapping its bytes). More...
 
#define Swap32(u32)
 Toggles the endianism of u32 (by swapping its bytes). More...
 
#define Swap64(u64)
 Toggles the endianism of u64 (by swapping its bytes). More...
 
#define swap16(u16)   Swap16(u16)
 Toggles the endianism of u16 (by swapping its bytes). More...
 
#define swap32(u32)   Swap32(u32)
 Toggles the endianism of u32 (by swapping its bytes). More...
 
#define swap64(u64)
 Toggles the endianism of u64 (by swapping its bytes). More...
 

Target Abstraction

typedef U8 Byte
 8-bit unsigned integer. More...
 
#define _GLOBEXT_   extern
 extern storage-class specifier. More...
 
#define _CONST_TYPE_   const
 const type qualifier. More...
 
#define _MEM_TYPE_SLOW_
 Slow memory type. More...
 
#define _MEM_TYPE_MEDFAST_
 Fairly fast memory type. More...
 
#define _MEM_TYPE_FAST_
 Fast memory type. More...
 
#define memcmp_ram2ram   memcmp
 Target-specific memcmp of RAM to RAM. More...
 
#define memcmp_code2ram   memcmp
 Target-specific memcmp of RAM to NVRAM. More...
 
#define memcpy_ram2ram   memcpy
 Target-specific memcpy from RAM to RAM. More...
 
#define memcpy_code2ram   memcpy
 Target-specific memcpy from NVRAM to RAM. More...
 

#define __always_inline   inline __attribute__((__always_inline__))

The function should always be inlined.

This annotation instructs the compiler to ignore its inlining heuristics and inline the function no matter how big it thinks it becomes.

#define __always_optimize   __attribute__((optimize(3)))

The function should always be optimized.

This annotation instructs the compiler to ignore global optimization settings and always compile the function with a high level of optimization.

#define __DEPRECATED__   __attribute__((__deprecated__))
#define _CONST_TYPE_   const

const type qualifier.

#define _GLOBEXT_   extern

extern storage-class specifier.

#define _MEM_TYPE_FAST_

Fast memory type.

#define _MEM_TYPE_MEDFAST_

Fairly fast memory type.

#define _MEM_TYPE_SLOW_

Slow memory type.

#define Abs (   a)    (((a) < 0 ) ? -(a) : (a))

Takes the absolute value of a.

Parameters
aInput value.
Returns
Absolute value of a.
Note
More optimized if only used with values known at compile time.
#define abs (   a)    Abs(a)
#define ADDR_COPY_DST_SRC_16 (   dst,
  src 
)    memcpy((&(dst)), (&(src)), sizeof(uint16_t))
#define ADDR_COPY_DST_SRC_64 (   dst,
  src 
)    memcpy((&(dst)), (&(src)), sizeof(uint64_t))
#define Align_down (   val,
 
)    ( (val) & ~((n) - 1))

Aligns the number val with the lower n boundary.

Parameters
valInput value.
nBoundary.
Returns
Value resulting from the number val aligned with the lower n boundary.
#define Align_up (   val,
 
)    (((val) + ((n) - 1)) & ~((n) - 1))

Aligns the number val with the upper n boundary.

Parameters
valInput value.
nBoundary.
Returns
Value resulting from the number val aligned with the upper n boundary.
#define Assert (   expr)    ((void) 0)

This macro is used to test fatal errors.

The macro tests if the expression is false. If it is, a fatal error is detected and the application hangs up. If TEST_SUITE_DEFINE_ASSERT_MACRO is defined, a unit test version of the macro is used, to allow execution of further tests after a false expression.

Parameters
exprExpression to evaluate and supposed to be nonzero.

Referenced by osc_disable(), osc_disable_autocalibration(), osc_enable_autocalibration(), osc_enable_external(), osc_enable_internal(), osc_get_rate(), osc_is_ready(), osc_user_calibration(), pll_config_init(), pll_config_read(), pll_config_write(), pll_disable(), pll_enable(), pll_enable_config_defaults(), pll_enable_source(), pll_get_default_rate_priv(), pll_is_locked(), pll_wait_for_lock(), sysclk_disable_peripheral_clock(), sysclk_enable_peripheral_clock(), sysclk_get_peripheral_bus_hz(), sysclk_init(), and sysclk_rtcsrc_enable().

#define barrier ( )    asm volatile("" ::: "memory")

Memory barrier.

Referenced by cpu_irq_restore().

#define BE16 (   x)    Swap16(x)
#define be16_to_cpu (   x)    swap16(x)
#define BE16_TO_CPU (   x)    Swap16(x)
#define BE32 (   x)    Swap32(x)
#define be32_to_cpu (   x)    swap32(x)
#define BE32_TO_CPU (   x)    Swap32(x)
#define bit_reverse16 (   u16)    ((U16)(bit_reverse32((U16)(u16)) >> 16))

Reverses the bits of u16.

Parameters
u16U16 of which to reverse the bits.
Returns
Value resulting from u16 with reversed bits.
#define bit_reverse32 (   u32)
Value:
(\
{\
unsigned int __value = (U32)(u32);\
__asm__ ("brev\t%0" : "+r" (__value) : : "cc");\
(U32)__value;\
}\
)
uint32_t U32
32-bit unsigned integer.
Definition: compiler.h:170

Reverses the bits of u32.

Parameters
u32U32 of which to reverse the bits.
Returns
Value resulting from u32 with reversed bits.
#define bit_reverse64 (   u64)
Value:
((U64)(((U64)bit_reverse32((U64)(u64) >> 32)) |\
((U64)bit_reverse32((U64)(u64)) << 32)))
#define bit_reverse32(u32)
Reverses the bits of u32.
Definition: compiler.h:606
uint64_t U64
64-bit unsigned integer.
Definition: compiler.h:174

Reverses the bits of u64.

Parameters
u64U64 of which to reverse the bits.
Returns
Value resulting from u64 with reversed bits.
#define bit_reverse8 (   u8)    ((U8)(bit_reverse32((U8)(u8)) >> 24))

Reverses the bits of u8.

Parameters
u8U8 of which to reverse the bits.
Returns
Value resulting from u8 with reversed bits.
#define CCPU_ENDIAN_TO_LE16 (   x)    (x)
#define CCPU_ENDIAN_TO_LE32 (   x)    (x)
#define CCPU_ENDIAN_TO_LE64 (   x)    (x)
#define CLE16_TO_CPU_ENDIAN (   x)    (x)
#define CLE32_TO_CPU_ENDIAN (   x)    (x)
#define CLE64_TO_CPU_ENDIAN (   x)    (x)
#define Clr_bits (   lvalue,
  mask 
)    ((lvalue) &= ~(mask))

Clears the bits of a C lvalue specified by a given bit-mask.

Parameters
lvalueC lvalue of which to clear bits.
maskBit-mask indicating bits to clear.
Returns
Resulting value with cleared bits.
#define CMD_ID_OCTET   (0)
#define COMPILER_ALIGNED (   a)    __attribute__((__aligned__(a)))

Set aligned boundary.

#define compiler_demux_size (   size,
  func,
  ... 
)
Value:
(((size) == 1) ? func##8(__VA_ARGS__) : \
((size) == 2) ? func##16(__VA_ARGS__) : \
((size) == 4) ? func##32(__VA_ARGS__) : \
compiler_demux_bad_size())

Demultiplex function call based on size of datatype.

Evaluates to a function call to a function name with suffix 8, 16 or 32 depending on the size of the datatype. Any number of parameters can be passed to the function.

Usage:

void foo8(uint8_t a, void *b);
void foo16(uint16_t a, void *b);
void foo32(uint32_t a, void *b);
#define foo(x, y) compiler_demux_size(sizeof(x), foo, x, y)
Parameters
sizeSize of the datatype.
funcBase function name.
...List of parameters to pass to the function.
#define COMPILER_PACK_RESET (   alignment)
#define COMPILER_PACK_SET (   alignment)
#define COMPILER_PRAGMA (   arg)    _Pragma(#arg)

Emit the compiler pragma arg.

Parameters
argThe pragma directive as it would appear after #pragma (i.e. not stringified).
#define COMPILER_WORD_ALIGNED   __attribute__((__aligned__(2)))

Set word-aligned boundary.

#define convert_16_bit_to_byte_address (   value,
  data 
)    ((*(uint16_t *)(data)) = (uint16_t)(value))
#define convert_16_bit_to_byte_array (   value,
  data 
)    ((*(uint16_t *)(data)) = (uint16_t)(value))
#define convert_32_bit_to_byte_array (   value,
  data 
)    ((*(uint32_t *)(data)) = (uint32_t)(value))
#define convert_64_bit_to_byte_array (   value,
  data 
)    memcpy((data), (&(value)), sizeof(uint64_t))
#define convert_byte_array_to_16_bit (   data)    (*(uint16_t *)(data))
#define convert_byte_array_to_32_bit (   data)    (*(uint32_t *)(data))
#define convert_byte_array_to_64_bit (   data)    (*(uint64_t *)(data))
#define convert_spec_16_bit_to_byte_array (   value,
  data 
)    ((*(uint16_t *)(data)) = (uint16_t)(value))
#define CPU_ENDIAN_TO_LE16 (   x)    (x)
#define CPU_ENDIAN_TO_LE32 (   x)    (x)
#define CPU_ENDIAN_TO_LE64 (   x)    (x)
#define cpu_to_be16 (   x)    swap16(x)
#define CPU_TO_BE16 (   x)    Swap16(x)
#define cpu_to_be32 (   x)    swap32(x)
#define CPU_TO_BE32 (   x)    Swap32(x)
#define cpu_to_le16 (   x)    (x)
#define CPU_TO_LE16 (   x)    (x)
#define cpu_to_le32 (   x)    (x)
#define CPU_TO_LE32 (   x)    (x)
#define DISABLE   0
#define div_ceil (   a,
 
)    (((a) + (b) - 1) / (b))

Calculate \( \left\lceil \frac{a}{b} \right\rceil \) using integer arithmetic.

Parameters
aAn integer
bAnother integer
Returns
(a / b) rounded up to the nearest integer.
#define ENABLE   1
#define ERROR_FUNC (   name,
  msg 
)    extern int name(void)

Fail compilation if function call isn't eliminated.

If the compiler fails to optimize away all calls to the function name, terminate compilation and display msg to the user.

Note
Not all compilers support this, so this is best-effort only. Sometimes, there may be a linker error instead, and when optimization is disabled, this mechanism will be completely disabled.
#define FAIL   1
#define false   0
#define FLASH_DECLARE (   x)    const x __attribute__((__progmem__))
#define FLASH_EXTERN (   x)    extern const x
#define FUNC_PTR   void *
#define Get_align (   val,
 
)    ( Rd_bits( val, (n) - 1 ) )

Gets alignment of the number val with respect to the n boundary.

Parameters
valInput value.
nBoundary.
Returns
Alignment of the number val with respect to the n boundary.
#define Get_debug_register (   dbgreg)    __builtin_mfdr(dbgreg)

Gets the value of the dbgreg debug register.

Parameters
dbgregAddress of the debug register of which to get the value.
Returns
Value of the dbgreg debug register.
#define Get_system_register (   sysreg)    __builtin_mfsr(sysreg)

Gets the value of the sysreg system register.

Parameters
sysregAddress of the system register of which to get the value.
Returns
Value of the sysreg system register.
#define HIGH   1
#define is_constant (   exp)    __builtin_constant_p(exp)

Determine if an expression evaluates to a constant value.

Parameters
expAny expression
Returns
true if exp is constant, false otherwise.

Referenced by ilog2().

#define LE16 (   x)    (x)
#define le16_to_cpu (   x)    (x)
#define LE16_TO_CPU (   x)    (x)
#define LE16_TO_CPU_ENDIAN (   x)    (x)
#define LE32 (   x)    (x)
#define le32_to_cpu (   x)    (x)
#define LE32_TO_CPU (   x)    (x)
#define LE32_TO_CPU_ENDIAN (   x)    (x)
#define LE64_TO_CPU_ENDIAN (   x)    (x)
#define likely (   exp)    (exp)

The expression exp is likely to be true.

#define Long_call (   addr)    ((*(void (*)(void))(addr))())

Calls the routine at address addr.

It generates a long call opcode.

For example, `Long_call(0x80000000)' generates a software reset on a UC3 if it is invoked from the CPU supervisor mode.

Parameters
addrAddress of the routine to call.
Note
It may be used as a long jump opcode in some special cases.
#define LOW   0
#define LSB (   u16)    (((uint8_t* )&u16)[0])
#define LSB0 (   u32)    MSB3(u32)
#define LSB0W (   u32)    MSB3W(u32)

Least significant byte of 1st rank of u32.

#define LSB1 (   u32)    MSB2(u32)
#define LSB1W (   u32)    MSB2W(u32)

Least significant byte of 2nd rank of u32.

#define LSB2 (   u32)    MSB1(u32)
#define LSB2W (   u32)    MSB1W(u32)

Least significant byte of 3rd rank of u32.

#define LSB3 (   u32)    MSB0(u32)
#define LSB3W (   u32)    MSB0W(u32)

Least significant byte of 4th rank of u32.

#define LSW (   u32)    (((uint16_t*)&u32)[0])
#define Max (   a,
 
)    (((a) > (b)) ? (a) : (b))

Takes the maximal value of a and b.

Parameters
aInput value.
bInput value.
Returns
Maximal value of a and b.
Note
More optimized if only used with values known at compile time.
#define max (   a,
 
)    Max(a, b)
#define memcmp_code2ram   memcmp

Target-specific memcmp of RAM to NVRAM.

#define memcmp_ram2ram   memcmp

Target-specific memcmp of RAM to RAM.

#define memcpy_code2ram   memcpy

Target-specific memcpy from NVRAM to RAM.

#define MEMCPY_ENDIAN   memcpy
#define memcpy_ram2ram   memcpy

Target-specific memcpy from RAM to RAM.

#define Min (   a,
 
)    (((a) < (b)) ? (a) : (b))

Takes the minimal value of a and b.

Parameters
aInput value.
bInput value.
Returns
Minimal value of a and b.
Note
More optimized if only used with values known at compile time.
#define min (   a,
 
)    Min(a, b)
#define MSB (   u16)    (((uint8_t* )&u16)[1])
#define MSB0 (   u32)    (((uint8_t*)&u32)[3])
#define MSB0W (   u32)    (((uint8_t*)&(u32))[3])

Most significant byte of 1st rank of u32.

#define MSB1 (   u32)    (((uint8_t*)&u32)[2])
#define MSB1W (   u32)    (((uint8_t*)&(u32))[2])

Most significant byte of 2nd rank of u32.

#define MSB2 (   u32)    (((uint8_t*)&u32)[1])
#define MSB2W (   u32)    (((uint8_t*)&(u32))[1])

Most significant byte of 3rd rank of u32.

#define MSB3 (   u32)    (((uint8_t*)&u32)[0])
#define MSB3W (   u32)    (((uint8_t*)&(u32))[0])

Most significant byte of 4th rank of u32.

#define MSW (   u32)    (((uint16_t*)&u32)[1])
#define nop ( )    do { __asm__ __volatile__ ("nop"); } while (0)
#define PASS   0
#define PGM_READ_BLOCK (   dst,
  src,
  len 
)    memcpy_P((dst), (src), (len))
#define PGM_READ_BYTE (   x)    pgm_read_byte(x)
#define PGM_READ_WORD (   x)    pgm_read_word(x)
#define Rd_bitfield (   value,
  mask 
)    (Rd_bits( value, (uint32_t)mask) >> ctz(mask))

Reads the bit-field of a value specified by a given bit-mask.

Parameters
valueValue to read a bit-field from.
maskBit-mask indicating the bit-field to read.
Returns
Read bit-field.
#define Rd_bits (   value,
  mask 
)    ((value)&(mask))

Reads the bits of a value specified by a given bit-mask.

Parameters
valueValue to read bits from.
maskBit-mask indicating bits to read.
Returns
Read bits.
#define Set_align (   lval,
  n,
  alg 
)    ( Wr_bits(lval, (n) - 1, alg) )

Sets alignment of the lvalue number lval to alg with respect to the n boundary.

Parameters
lvalInput/output lvalue.
nBoundary.
algAlignment.
Returns
New value of lval resulting from its alignment set to alg with respect to the n boundary.
#define Set_bits (   lvalue,
  mask 
)    ((lvalue) |= (mask))

Sets the bits of a C lvalue specified by a given bit-mask.

Parameters
lvalueC lvalue of which to set bits.
maskBit-mask indicating bits to set.
Returns
Resulting value with set bits.
#define Set_debug_register (   dbgreg,
  value 
)    __builtin_mtdr(dbgreg, value)

Sets the value of the dbgreg debug register to value.

Parameters
dbgregAddress of the debug register of which to set the value.
valueValue to set the dbgreg debug register to.
#define Set_system_register (   sysreg,
  value 
)    __builtin_mtsr(sysreg, value)

Sets the value of the sysreg system register to value.

Parameters
sysregAddress of the system register of which to set the value.
valueValue to set the sysreg system register to.
#define SHORTENUM   __attribute__ ((packed))
#define Swap16 (   u16)
Value:
((U16)(((U16)(u16) >> 8) |\
((U16)(u16) << 8)))
uint16_t U16
16-bit unsigned integer.
Definition: compiler.h:166

Toggles the endianism of u16 (by swapping its bytes).

Parameters
u16U16 of which to toggle the endianism.
Returns
Value resulting from u16 with toggled endianism.
Note
More optimized if only used with values known at compile time.
#define swap16 (   u16)    Swap16(u16)

Toggles the endianism of u16 (by swapping its bytes).

Parameters
u16U16 of which to toggle the endianism.
Returns
Value resulting from u16 with toggled endianism.
Note
More optimized if only used with values unknown at compile time.
#define Swap32 (   u32)
Value:
((U32)(((U32)Swap16((U32)(u32) >> 16)) |\
((U32)Swap16((U32)(u32)) << 16)))
#define Swap16(u16)
Toggles the endianism of u16 (by swapping its bytes).
Definition: compiler.h:935
uint32_t U32
32-bit unsigned integer.
Definition: compiler.h:170

Toggles the endianism of u32 (by swapping its bytes).

Parameters
u32U32 of which to toggle the endianism.
Returns
Value resulting from u32 with toggled endianism.
Note
More optimized if only used with values known at compile time.
#define swap32 (   u32)    Swap32(u32)

Toggles the endianism of u32 (by swapping its bytes).

Parameters
u32U32 of which to toggle the endianism.
Returns
Value resulting from u32 with toggled endianism.
Note
More optimized if only used with values unknown at compile time.
#define Swap64 (   u64)
Value:
((U64)(((U64)Swap32((U64)(u64) >> 32)) |\
((U64)Swap32((U64)(u64)) << 32)))
uint64_t U64
64-bit unsigned integer.
Definition: compiler.h:174
#define Swap32(u32)
Toggles the endianism of u32 (by swapping its bytes).
Definition: compiler.h:946

Toggles the endianism of u64 (by swapping its bytes).

Parameters
u64U64 of which to toggle the endianism.
Returns
Value resulting from u64 with toggled endianism.
Note
More optimized if only used with values known at compile time.
#define swap64 (   u64)
Value:
((U64)(((U64)swap32((U64)(u64) >> 32)) |\
((U64)swap32((U64)(u64)) << 32)))
#define swap32(u32)
Toggles the endianism of u32 (by swapping its bytes).
Definition: compiler.h:978
uint64_t U64
64-bit unsigned integer.
Definition: compiler.h:174

Toggles the endianism of u64 (by swapping its bytes).

Parameters
u64U64 of which to toggle the endianism.
Returns
Value resulting from u64 with toggled endianism.
Note
More optimized if only used with values unknown at compile time.
#define Test_align (   val,
 
)    (!Tst_bits( val, (n) - 1 ) )

Tests alignment of the number val with the n boundary.

Parameters
valInput value.
nBoundary.
Returns
1 if the number val is aligned with the n boundary, else 0.
#define Tgl_bits (   lvalue,
  mask 
)    ((lvalue) ^= (mask))

Toggles the bits of a C lvalue specified by a given bit-mask.

Parameters
lvalueC lvalue of which to toggle bits.
maskBit-mask indicating bits to toggle.
Returns
Resulting value with toggled bits.
#define true   1
#define Tst_bits (   value,
  mask 
)    (Rd_bits(value, mask) != 0)

Tests the bits of a value specified by a given bit-mask.

Parameters
valueValue of which to test bits.
maskBit-mask indicating bits to test.
Returns
1 if at least one of the tested bits is set, else 0.
#define unlikely (   exp)    (exp)

The expression exp is unlikely to be true.

#define UNUSED (   v)    (void)(v)

Marking v as a unused parameter or value.

Referenced by sysclk_init().

#define unused (   v)    do { (void)(v); } while(0)

Marking v as a unused parameter or value.

#define Wr_bitfield (   lvalue,
  mask,
  bitfield 
)    (Wr_bits(lvalue, mask, (uint32_t)(bitfield) << ctz(mask)))

Writes the bit-field of a C lvalue specified by a given bit-mask.

Parameters
lvalueC lvalue to write a bit-field to.
maskBit-mask indicating the bit-field to write.
bitfieldBit-field to write.
Returns
Resulting value with written bit-field.
#define Wr_bits (   lvalue,
  mask,
  bits 
)
Value:
((lvalue) = ((lvalue) & ~(mask)) |\
((bits ) & (mask)))

Writes the bits of a C lvalue specified by a given bit-mask.

Parameters
lvalueC lvalue to write bits to.
maskBit-mask indicating bits to write.
bitsBits to write.
Returns
Resulting value with written bits.

typedef uint16_t be16_t
typedef uint32_t be32_t
typedef unsigned char Bool

Boolean.

typedef unsigned char bool

Boolean.

typedef U8 Byte

8-bit unsigned integer.

typedef float F32

32-bit floating-point number.

typedef double F64

64-bit floating-point number.

typedef uint16_t iram_size_t
typedef uint16_t le16_t
typedef uint32_t le32_t
typedef int16_t S16

16-bit signed integer.

typedef int32_t S32

32-bit signed integer.

typedef int64_t S64

64-bit signed integer.

typedef int8_t S8

8-bit signed integer.

Boolean status.

typedef U8 Status_t

8-bit-coded status.

typedef uint16_t U16

16-bit unsigned integer.

typedef uint32_t U32

32-bit unsigned integer.

typedef uint64_t U64

64-bit unsigned integer.

typedef uint8_t U8

8-bit unsigned integer.

ERROR_FUNC ( compiler_demux_bad_size  ,
"Invalid parameter size"   
)

Error function for failed demultiplexing.

static int_fast8_t ilog2 ( uint32_t  x)
inlinestatic

Calculate the base-2 logarithm of a number rounded down to the nearest integer.

Parameters
xA 32-bit value
Returns
The base-2 logarithm of x, or -1 if x is 0.

References clz, ilog2_undefined(), and is_constant.

int_fast8_t ilog2_undefined ( void  )

Undefined function. Will cause a link failure if ilog2() is called with an invalid constant value.

Referenced by ilog2().