The Qtouch example demonstrates how to use the Qtouch on the SAM EK boards.
This package can be used with SAM EK boards on which there is Qtouch keys or a slider.
This application will configure the silder bar and Qtouch keys on the SAM EK boards.
Whenever touching the keys or the silder, the value will be output the debug terminal.
-# Build the program and download it into the evaluation board. Please refer to the <a href="http://ww1.microchip.com/downloads/en/appnotes/atmel-42438-sam-ba-overview-and-customization-process_applicationnote_at09423.pdf"> SAM-BA User Guide</a>, the <a href="http://ww1.microchip.com/downloads/en/appnotes/doc6310.pdf"> GNU-Based Software Development</a> application note or the <a href="http://www.iar.com/website1/1.0.1.0/78/1/"> IAR EWARM User and reference guides</a>, depending on the solutions that users choose. -# On the computer, open and configure a terminal application (e.g., HyperTerminal on Microsoft Windows) with these settings: - 115200 bauds - 8 bits of data - No parity - 1 stop bit - No flow control -# In the terminal window, the following text should appear (values depend on the board and the chip used):