Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
MEMORY - FLASHC - Flash Controller

FLASHC interfaces a flash block with the 32-bit internal HSB bus.

Macros

#define AVR32_FLASHC_REGIONS
 Number of flash regions defined by the FLASHC. More...
 

FLASHC Status

static unsigned int flashc_error_status = 0
 Sticky error status of the FLASHC. More...
 
static unsigned int flashc_get_error_status (void)
 Gets the error status of the FLASHC. More...
 

Flash Properties

unsigned int flashc_get_flash_size (void)
 Gets the size of the whole flash array. More...
 
unsigned int flashc_get_page_count (void)
 Gets the total number of pages in the flash array. More...
 
unsigned int flashc_get_page_count_per_region (void)
 Gets the number of pages in each flash region. More...
 
unsigned int flashc_get_page_region (int page_number)
 Gets the region number of a page. More...
 
unsigned int flashc_get_region_first_page_number (unsigned int region)
 Gets the number of the first page of a region. More...
 

FLASHC Control

unsigned int flashc_get_wait_state (void)
 Gets the number of wait states of flash read accesses. More...
 
void flashc_set_wait_state (unsigned int wait_state)
 Sets the number of wait states of flash read accesses. More...
 
void flashc_set_bus_freq (unsigned int cpu_f_hz)
 Depending on the CPU frequency, set the wait states of flash read accesses. More...
 
bool flashc_is_ready_int_enabled (void)
 Tells whether the Flash Ready interrupt is enabled. More...
 
void flashc_enable_ready_int (bool enable)
 Enables or disables the Flash Ready interrupt. More...
 
bool flashc_is_lock_error_int_enabled (void)
 Tells whether the Lock Error interrupt is enabled. More...
 
void flashc_enable_lock_error_int (bool enable)
 Enables or disables the Lock Error interrupt. More...
 
bool flashc_is_prog_error_int_enabled (void)
 Tells whether the Programming Error interrupt is enabled. More...
 
void flashc_enable_prog_error_int (bool enable)
 Enables or disables the Programming Error interrupt. More...
 
#define flash_set_bus_freq(cpu_f_hz)   flashc_set_bus_freq(cpu_f_hz)
 Alias on the flashc_set_bus_freq() function. More...
 

FLASHC Status

void(*volatile flashc_wait_until_ready )(void)
 Pointer to the function used by the driver when it needs to wait until the FLASHC is ready to run a new command. More...
 
bool flashc_is_ready (void)
 Tells whether the FLASHC is ready to run a new command. More...
 
void flashc_default_wait_until_ready (void)
 Waits actively until the FLASHC is ready to run a new command. More...
 
bool flashc_is_lock_error (void)
 Tells whether a Lock Error has occurred during the last function called that issued one or more FLASHC commands. More...
 
bool flashc_is_programming_error (void)
 Tells whether a Programming Error has occurred during the last function called that issued one or more FLASHC commands. More...
 

FLASHC Command Control

unsigned int flashc_get_command (void)
 Gets the last issued FLASHC command. More...
 
unsigned int flashc_get_page_number (void)
 Gets the current FLASHC page number. More...
 
void flashc_issue_command (unsigned int command, int page_number)
 Issues a FLASHC command. More...
 

FLASHC Global Commands

void flashc_no_operation (void)
 Issues a No Operation command to the FLASHC. More...
 
void flashc_erase_all (void)
 Issues an Erase All command to the FLASHC. More...
 

FLASHC Protection Mechanisms

bool flashc_is_security_bit_active (void)
 Tells whether the Security bit is active. More...
 
void flashc_activate_security_bit (void)
 Activates the Security bit. More...
 
unsigned int flashc_get_bootloader_protected_size (void)
 Gets the bootloader protected size. More...
 
unsigned int flashc_set_bootloader_protected_size (unsigned int bootprot_size)
 Sets the bootloader protected size. More...
 
bool flashc_is_external_privileged_fetch_locked (void)
 Tells whether external privileged fetch is locked. More...
 
void flashc_lock_external_privileged_fetch (bool lock)
 Locks or unlocks external privileged fetch. More...
 
bool flashc_is_page_region_locked (int page_number)
 Tells whether the region of a page is locked. More...
 
bool flashc_is_region_locked (unsigned int region)
 Tells whether a region is locked. More...
 
void flashc_lock_page_region (int page_number, bool lock)
 Locks or unlocks the region of a page. More...
 
void flashc_lock_region (unsigned int region, bool lock)
 Locks or unlocks a region. More...
 
void flashc_lock_all_regions (bool lock)
 Locks or unlocks all regions. More...
 

Access to General-Purpose Fuses

bool flashc_read_gp_fuse_bit (unsigned int gp_fuse_bit)
 Reads a general-purpose fuse bit. More...
 
uint64_t flashc_read_gp_fuse_bitfield (unsigned int pos, unsigned int width)
 Reads a general-purpose fuse bit-field. More...
 
uint8_t flashc_read_gp_fuse_byte (unsigned int gp_fuse_byte)
 Reads a general-purpose fuse byte. More...
 
uint64_t flashc_read_all_gp_fuses (void)
 Reads all general-purpose fuses. More...
 
bool flashc_erase_gp_fuse_bit (unsigned int gp_fuse_bit, bool check)
 Erases a general-purpose fuse bit. More...
 
bool flashc_erase_gp_fuse_bitfield (unsigned int pos, unsigned int width, bool check)
 Erases a general-purpose fuse bit-field. More...
 
bool flashc_erase_gp_fuse_byte (unsigned int gp_fuse_byte, bool check)
 Erases a general-purpose fuse byte. More...
 
bool flashc_erase_all_gp_fuses (bool check)
 Erases all general-purpose fuses. More...
 
void flashc_write_gp_fuse_bit (unsigned int gp_fuse_bit, bool value)
 Writes a general-purpose fuse bit. More...
 
void flashc_write_gp_fuse_bitfield (unsigned int pos, unsigned int width, uint64_t value)
 Writes a general-purpose fuse bit-field. More...
 
void flashc_write_gp_fuse_byte (unsigned int gp_fuse_byte, uint8_t value)
 Writes a general-purpose fuse byte. More...
 
void flashc_write_all_gp_fuses (uint64_t value)
 Writes all general-purpose fuses. More...
 
void flashc_set_gp_fuse_bit (unsigned int gp_fuse_bit, bool value)
 Sets a general-purpose fuse bit with the appropriate erase and write operations. More...
 
void flashc_set_gp_fuse_bitfield (unsigned int pos, unsigned int width, uint64_t value)
 Sets a general-purpose fuse bit-field with the appropriate erase and write operations. More...
 
void flashc_set_gp_fuse_byte (unsigned int gp_fuse_byte, uint8_t value)
 Sets a general-purpose fuse byte with the appropriate erase and write operations. More...
 
void flashc_set_all_gp_fuses (uint64_t value)
 Sets all general-purpose fuses with the appropriate erase and write operations. More...
 

Access to Flash Pages

void flashc_clear_page_buffer (void)
 Clears the page buffer. More...
 
bool flashc_is_page_erased (void)
 Tells whether the page to which the last Quick Page Read or Quick Page Read User Page command was applied was erased. More...
 
bool flashc_quick_page_read (int page_number)
 Applies the Quick Page Read command to a page. More...
 
bool flashc_erase_page (int page_number, bool check)
 Erases a page. More...
 
bool flashc_erase_all_pages (bool check)
 Erases all pages within the flash array. More...
 
void flashc_write_page (int page_number)
 Writes a page from the page buffer. More...
 
bool flashc_quick_user_page_read (void)
 Issues a Quick Page Read User Page command to the FLASHC. More...
 
bool flashc_erase_user_page (bool check)
 Erases the User page. More...
 
void flashc_write_user_page (void)
 Writes the User page from the page buffer. More...
 
volatile void * flashc_memset8 (volatile void *dst, uint8_t src, size_t nbytes, bool erase)
 Copies nbytes bytes to the flash destination pointed to by dst from the repeated src source byte. More...
 
volatile void * flashc_memset16 (volatile void *dst, uint16_t src, size_t nbytes, bool erase)
 Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source half-word. More...
 
volatile void * flashc_memset32 (volatile void *dst, uint32_t src, size_t nbytes, bool erase)
 Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source word. More...
 
volatile void * flashc_memset64 (volatile void *dst, uint64_t src, size_t nbytes, bool erase)
 Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source double-word. More...
 
volatile void * flashc_memcpy (volatile void *dst, const void *src, size_t nbytes, bool erase)
 Copies nbytes bytes to the flash destination pointed to by dst from the source pointed to by src. More...
 
void flashc_set_flash_waitstate_and_readmode (unsigned long cpu_f_hz)
 Depending to the CPU frequency, set the wait states of flash read accesses and enable or disable the High speed read mode. More...
 
#define flashc_memset(dst, src, src_width, nbytes, erase)   TPASTE2(flashc_memset, src_width)((dst), (src), (nbytes), (erase))
 Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source pattern. More...
 

#define AVR32_FLASHC_REGIONS
Value:
(AVR32_FLASHC_FLASH_SIZE /\
(AVR32_FLASHC_PAGES_PR_REGION * AVR32_FLASHC_PAGE_SIZE))

Number of flash regions defined by the FLASHC.

Referenced by flashc_get_page_count_per_region(), flashc_is_region_locked(), and flashc_lock_all_regions().

#define flash_set_bus_freq (   cpu_f_hz)    flashc_set_bus_freq(cpu_f_hz)

Alias on the flashc_set_bus_freq() function.

Parameters
cpu_f_hzThe CPU frequency

Referenced by sysclk_init().

#define flashc_memset (   dst,
  src,
  src_width,
  nbytes,
  erase 
)    TPASTE2(flashc_memset, src_width)((dst), (src), (nbytes), (erase))

Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source pattern.

All pointer and size alignments are supported.

Parameters
dstPointer to flash destination.
srcSource double-word.
src_widthsrc width in bits: 8, 16, 32 or 64.
nbytesNumber of bytes to set.
eraseWhether to erase before writing: true or false.
Returns
The value of dst.
Warning
This function may be called with erase set to false only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001 then 0xFFFFFFFE are written to a word, the resulting value in flash may be different from 0x00000000.
A Lock Error is issued if the command is applied to pages belonging to a locked region or to the bootloader protected area.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.

void flashc_activate_security_bit ( void  )

Activates the Security bit.

Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.

References flashc_issue_command().

void flashc_clear_page_buffer ( void  )

Clears the page buffer.

This command resets all bits in the page buffer to one. Write accesses to the page buffer can only change page buffer bits from one to zero.

Warning
The page buffer is not automatically reset after a page write.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.

References flashc_issue_command().

Referenced by flashc_memcpy(), and flashc_memset64().

void flashc_default_wait_until_ready ( void  )

Waits actively until the FLASHC is ready to run a new command.

This is the default function assigned to flashc_wait_until_ready.

References flashc_is_ready().

void flashc_enable_lock_error_int ( bool  enable)

Enables or disables the Lock Error interrupt.

Parameters
enableWhether to enable the Lock Error interrupt: true or false.

References u_avr32_flashc_fcr_t::fcr, and u_avr32_flashc_fcr_t::FCR.

void flashc_enable_prog_error_int ( bool  enable)

Enables or disables the Programming Error interrupt.

Parameters
enableWhether to enable the Programming Error interrupt: true or false.

References u_avr32_flashc_fcr_t::fcr, and u_avr32_flashc_fcr_t::FCR.

void flashc_enable_ready_int ( bool  enable)

Enables or disables the Flash Ready interrupt.

Parameters
enableWhether to enable the Flash Ready interrupt: true or false.

References u_avr32_flashc_fcr_t::fcr, and u_avr32_flashc_fcr_t::FCR.

void flashc_erase_all ( void  )

Issues an Erase All command to the FLASHC.

This command erases all bits in the flash array, the general-purpose fuse bits and the Security bit. The User page is not erased.

This command also ensures that all volatile memories, such as register file and RAMs, are erased before the Security bit is erased, i.e. deactivated.

Warning
A Lock Error is issued if at least one region is locked or the bootloader protection is active.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
An erase operation can only set bits.

References flashc_issue_command().

bool flashc_erase_all_gp_fuses ( bool  check)

Erases all general-purpose fuses.

Parameters
checkWhether to check erase: true or false.
Returns
Whether the erase succeeded or always true if erase check was not requested.
Warning
A Lock Error is issued if the Security bit is active.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
An erase operation can only set bits.
The actual number of general-purpose fuse bits implemented by hardware is given by AVR32_FLASHC_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashc_issue_command(), and flashc_read_all_gp_fuses().

Referenced by flashc_erase_gp_fuse_byte(), and flashc_set_all_gp_fuses().

bool flashc_erase_all_pages ( bool  check)

Erases all pages within the flash array.

Parameters
checkWhether to check erase: true or false.
Returns
Whether the erase succeeded or always true if erase check was not requested.
Warning
A Lock Error is issued if at least one region is locked or the bootloader protection is active.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
An erase operation can only set bits.

References flashc_erase_page(), flashc_error_status, and flashc_get_page_count().

bool flashc_erase_gp_fuse_bit ( unsigned int  gp_fuse_bit,
bool  check 
)

Erases a general-purpose fuse bit.

Parameters
gp_fuse_bitThe general-purpose fuse bit: 0 to 63.
checkWhether to check erase: true or false.
Returns
Whether the erase succeeded or always true if erase check was not requested.
Warning
A Lock Error is issued if the Security bit is active and the command is applied to BOOTPROT or EPFL fuses.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
An erase operation can only set bits.
The actual number of general-purpose fuse bits implemented by hardware is given by AVR32_FLASHC_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashc_issue_command(), and flashc_read_gp_fuse_bit().

Referenced by flashc_erase_gp_fuse_bitfield(), and flashc_set_gp_fuse_bit().

bool flashc_erase_gp_fuse_bitfield ( unsigned int  pos,
unsigned int  width,
bool  check 
)

Erases a general-purpose fuse bit-field.

Parameters
posThe bit-position of the general-purpose fuse bit-field: 0 to 63.
widthThe bit-width of the general-purpose fuse bit-field: 0 to 64.
checkWhether to check erase: true or false.
Returns
Whether the erase succeeded or always true if erase check was not requested.
Warning
A Lock Error is issued if the Security bit is active and the command is applied to BOOTPROT or EPFL fuses.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
An erase operation can only set bits.
The actual number of general-purpose fuse bits implemented by hardware is given by AVR32_FLASHC_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashc_erase_gp_fuse_bit(), flashc_error_status, flashc_read_gp_fuse_bitfield(), and min.

bool flashc_erase_gp_fuse_byte ( unsigned int  gp_fuse_byte,
bool  check 
)

Erases a general-purpose fuse byte.

Parameters
gp_fuse_byteThe general-purpose fuse byte: 0 to 7.
checkWhether to check erase: true or false.
Returns
Whether the erase succeeded or always true if erase check was not requested.
Warning
A Lock Error is issued if the Security bit is active.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
An erase operation can only set bits.
The actual number of general-purpose fuse bits implemented by hardware is given by AVR32_FLASHC_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashc_erase_all_gp_fuses(), flashc_error_status, flashc_read_all_gp_fuses(), flashc_read_gp_fuse_byte(), and flashc_write_gp_fuse_byte().

Referenced by flashc_set_gp_fuse_byte().

bool flashc_erase_page ( int  page_number,
bool  check 
)

Erases a page.

Parameters
page_numberThe page number:
checkWhether to check erase: true or false.
Returns
Whether the erase succeeded or always true if erase check was not requested.
Warning
A Lock Error is issued if the command is applied to a page belonging to a locked region or to the bootloader protected area.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
An erase operation can only set bits.

References flashc_error_status, flashc_issue_command(), and flashc_quick_page_read().

Referenced by flashc_erase_all_pages(), flashc_memcpy(), and flashc_memset64().

bool flashc_erase_user_page ( bool  check)

Erases the User page.

Parameters
checkWhether to check erase: true or false.
Returns
Whether the erase succeeded or always true if erase check was not requested.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
An erase operation can only set bits.

References flashc_issue_command(), and flashc_quick_user_page_read().

Referenced by flashc_memcpy(), and flashc_memset64().

unsigned int flashc_get_bootloader_protected_size ( void  )

Gets the bootloader protected size.

Returns
The bootloader protected size in bytes.

References flashc_read_gp_fuse_bitfield().

Referenced by flashc_set_bootloader_protected_size().

unsigned int flashc_get_command ( void  )

Gets the last issued FLASHC command.

Returns
The last issued FLASHC command.
static unsigned int flashc_get_error_status ( void  )
static

Gets the error status of the FLASHC.

Returns
The error status of the FLASHC built up from AVR32_FLASHC_FSR_LOCKE_MASK and AVR32_FLASHC_FSR_PROGE_MASK.
Warning
This hardware error status is cleared by all functions reading the Flash Status Register (FSR). This function is therefore not part of the driver's API which instead presents flashc_is_lock_error and flashc_is_programming_error.

Referenced by flashc_issue_command().

unsigned int flashc_get_flash_size ( void  )

Gets the size of the whole flash array.

Returns
The size of the whole flash array in bytes.

Referenced by flashc_get_page_count(), flashc_memcpy(), and flashc_memset64().

unsigned int flashc_get_page_count ( void  )

Gets the total number of pages in the flash array.

Returns
The total number of pages in the flash array.

References flashc_get_flash_size().

Referenced by flashc_erase_all_pages(), and flashc_get_page_count_per_region().

unsigned int flashc_get_page_count_per_region ( void  )

Gets the number of pages in each flash region.

Returns
The number of pages in each flash region.

References AVR32_FLASHC_REGIONS, and flashc_get_page_count().

Referenced by flashc_get_page_region(), and flashc_get_region_first_page_number().

unsigned int flashc_get_page_number ( void  )

Gets the current FLASHC page number.

Returns
The current FLASHC page number.

Referenced by flashc_get_page_region().

unsigned int flashc_get_page_region ( int  page_number)

Gets the region number of a page.

Parameters
page_numberThe page number:
Returns
The region number of the specified page.

References flashc_get_page_count_per_region(), and flashc_get_page_number().

Referenced by flashc_is_page_region_locked().

unsigned int flashc_get_region_first_page_number ( unsigned int  region)

Gets the number of the first page of a region.

Parameters
regionThe region number: 0 to (AVR32_FLASHC_REGIONS - 1).
Returns
The number of the first page of the specified region.

References flashc_get_page_count_per_region().

Referenced by flashc_lock_region().

unsigned int flashc_get_wait_state ( void  )

Gets the number of wait states of flash read accesses.

Returns
The number of wait states of flash read accesses.
bool flashc_is_external_privileged_fetch_locked ( void  )

Tells whether external privileged fetch is locked.

Returns
Whether external privileged fetch is locked.

References flashc_read_gp_fuse_bit().

bool flashc_is_lock_error ( void  )

Tells whether a Lock Error has occurred during the last function called that issued one or more FLASHC commands.

Returns
Whether a Lock Error has occurred during the last function called that issued one or more FLASHC commands.

References flashc_error_status.

bool flashc_is_lock_error_int_enabled ( void  )

Tells whether the Lock Error interrupt is enabled.

Returns
Whether the Lock Error interrupt is enabled.
bool flashc_is_page_erased ( void  )

Tells whether the page to which the last Quick Page Read or Quick Page Read User Page command was applied was erased.

Returns
Whether the page to which the last Quick Page Read or Quick Page Read User Page command was applied was erased.

Referenced by flashc_quick_page_read(), and flashc_quick_user_page_read().

bool flashc_is_page_region_locked ( int  page_number)

Tells whether the region of a page is locked.

Parameters
page_numberThe page number:
Returns
Whether the region of the specified page is locked.

References flashc_get_page_region(), and flashc_is_region_locked().

bool flashc_is_prog_error_int_enabled ( void  )

Tells whether the Programming Error interrupt is enabled.

Returns
Whether the Programming Error interrupt is enabled.
bool flashc_is_programming_error ( void  )

Tells whether a Programming Error has occurred during the last function called that issued one or more FLASHC commands.

Returns
Whether a Programming Error has occurred during the last function called that issued one or more FLASHC commands.

References flashc_error_status.

bool flashc_is_ready ( void  )

Tells whether the FLASHC is ready to run a new command.

Returns
Whether the FLASHC is ready to run a new command.

Referenced by flashc_default_wait_until_ready().

bool flashc_is_ready_int_enabled ( void  )

Tells whether the Flash Ready interrupt is enabled.

Returns
Whether the Flash Ready interrupt is enabled.
bool flashc_is_region_locked ( unsigned int  region)

Tells whether a region is locked.

Parameters
regionThe region number: 0 to (AVR32_FLASHC_REGIONS - 1).
Returns
Whether the specified region is locked.

References AVR32_FLASHC_REGIONS.

Referenced by flashc_is_page_region_locked().

bool flashc_is_security_bit_active ( void  )

Tells whether the Security bit is active.

Returns
Whether the Security bit is active.
void flashc_issue_command ( unsigned int  command,
int  page_number 
)

Issues a FLASHC command.

Parameters
commandThe command: AVR32_FLASHC_FCMD_CMD_x.
page_numberThe page number to apply the command to:
  • 0 to (flashc_get_page_count() - 1): a page number within the flash array;
  • < 0: use this to apply the command to the current page number or if the command does not apply to any page number;
  • this argument may have other meanings according to the command. See the FLASHC chapter of the MCU datasheet.
Warning
A Lock Error is issued if the command violates the protection mechanism.
A Programming Error is issued if the command is invalid.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.

References u_avr32_flashc_fcmd_t::fcmd, u_avr32_flashc_fcmd_t::FCMD, flashc_error_status, flashc_get_error_status(), and flashc_wait_until_ready.

Referenced by flashc_activate_security_bit(), flashc_clear_page_buffer(), flashc_erase_all(), flashc_erase_all_gp_fuses(), flashc_erase_gp_fuse_bit(), flashc_erase_page(), flashc_erase_user_page(), flashc_lock_page_region(), flashc_no_operation(), flashc_quick_page_read(), flashc_quick_user_page_read(), flashc_write_gp_fuse_bit(), flashc_write_gp_fuse_byte(), flashc_write_page(), flashc_write_user_page(), and pm_configure_clocks().

void flashc_lock_all_regions ( bool  lock)

Locks or unlocks all regions.

Parameters
lockWhether to lock the regions: true or false.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.

References AVR32_FLASHC_REGIONS, flashc_error_status, and flashc_lock_region().

void flashc_lock_external_privileged_fetch ( bool  lock)

Locks or unlocks external privileged fetch.

Parameters
lockWhether to lock external privileged fetch: true or false.
Warning
A Lock Error is issued if the Security bit is active.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.

References flashc_set_gp_fuse_bit().

void flashc_lock_page_region ( int  page_number,
bool  lock 
)

Locks or unlocks the region of a page.

Parameters
page_numberThe page number:
lockWhether to lock the region of the specified page: true or false.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.

References flashc_issue_command().

Referenced by flashc_lock_region().

void flashc_lock_region ( unsigned int  region,
bool  lock 
)

Locks or unlocks a region.

Parameters
regionThe region number: 0 to (AVR32_FLASHC_REGIONS - 1).
lockWhether to lock the specified region: true or false.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.

References flashc_get_region_first_page_number(), and flashc_lock_page_region().

Referenced by flashc_lock_all_regions().

volatile void* flashc_memcpy ( volatile void *  dst,
const void *  src,
size_t  nbytes,
bool  erase 
)

Copies nbytes bytes to the flash destination pointed to by dst from the source pointed to by src.

The destination areas that are not within the flash array or the User page are caught by an Assert() operation.

All pointer and size alignments are supported.

Parameters
dstPointer to flash destination.
srcPointer to source data.
nbytesNumber of bytes to copy.
eraseWhether to erase before writing: true or false.
Returns
The value of dst.
Warning
If copying takes place between areas that overlap, the behavior is undefined.
This function may be called with erase set to false only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001 then 0xFFFFFFFE are written to a word, the resulting value in flash may be different from 0x00000000.
A Lock Error is issued if the command is applied to pages belonging to a locked region or to the bootloader protected area.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.

References Assert, flashc_clear_page_buffer(), flashc_erase_page(), flashc_erase_user_page(), flashc_error_status, flashc_get_flash_size(), flashc_write_page(), flashc_write_user_page(), Union64::u64, and Union64::u8.

volatile void* flashc_memset16 ( volatile void *  dst,
uint16_t  src,
size_t  nbytes,
bool  erase 
)

Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source half-word.

All pointer and size alignments are supported.

Parameters
dstPointer to flash destination.
srcSource half-word.
nbytesNumber of bytes to set.
eraseWhether to erase before writing: true or false.
Returns
The value of dst.
Warning
This function may be called with erase set to false only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001 then 0xFFFFFFFE are written to a word, the resulting value in flash may be different from 0x00000000.
A Lock Error is issued if the command is applied to pages belonging to a locked region or to the bootloader protected area.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.

References flashc_memset32().

Referenced by flashc_memset8().

volatile void* flashc_memset32 ( volatile void *  dst,
uint32_t  src,
size_t  nbytes,
bool  erase 
)

Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source word.

All pointer and size alignments are supported.

Parameters
dstPointer to flash destination.
srcSource word.
nbytesNumber of bytes to set.
eraseWhether to erase before writing: true or false.
Returns
The value of dst.
Warning
This function may be called with erase set to false only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001 then 0xFFFFFFFE are written to a word, the resulting value in flash may be different from 0x00000000.
A Lock Error is issued if the command is applied to pages belonging to a locked region or to the bootloader protected area.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.

References flashc_memset64().

Referenced by flashc_memset16().

volatile void* flashc_memset64 ( volatile void *  dst,
uint64_t  src,
size_t  nbytes,
bool  erase 
)

Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source double-word.

All pointer and size alignments are supported.

Parameters
dstPointer to flash destination.
srcSource double-word.
nbytesNumber of bytes to set.
eraseWhether to erase before writing: true or false.
Returns
The value of dst.
Warning
This function may be called with erase set to false only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001 then 0xFFFFFFFE are written to a word, the resulting value in flash may be different from 0x00000000.
A Lock Error is issued if the command is applied to pages belonging to a locked region or to the bootloader protected area.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.

References Align_down, flashc_clear_page_buffer(), flashc_erase_page(), flashc_erase_user_page(), flashc_error_status, flashc_get_flash_size(), flashc_write_page(), flashc_write_user_page(), Get_align, if(), min, Test_align, StructCVPtr::u16ptr, StructCVPtr::u32ptr, Union64::u64, UnionVPtr::u64ptr, UnionCVPtr::u64ptr, StructCVPtr::u64ptr, Union64::u8, UnionVPtr::u8ptr, UnionCVPtr::u8ptr, and StructCVPtr::u8ptr.

Referenced by flashc_memset32().

volatile void* flashc_memset8 ( volatile void *  dst,
uint8_t  src,
size_t  nbytes,
bool  erase 
)

Copies nbytes bytes to the flash destination pointed to by dst from the repeated src source byte.

All pointer and size alignments are supported.

Parameters
dstPointer to flash destination.
srcSource byte.
nbytesNumber of bytes to set.
eraseWhether to erase before writing: true or false.
Returns
The value of dst.
Warning
This function may be called with erase set to false only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001 then 0xFFFFFFFE are written to a word, the resulting value in flash may be different from 0x00000000.
A Lock Error is issued if the command is applied to pages belonging to a locked region or to the bootloader protected area.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.

References flashc_memset16().

void flashc_no_operation ( void  )

Issues a No Operation command to the FLASHC.

Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.

References flashc_issue_command().

bool flashc_quick_page_read ( int  page_number)

Applies the Quick Page Read command to a page.

Parameters
page_numberThe page number:
Returns
Whether the specified page is erased.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.

References flashc_is_page_erased(), and flashc_issue_command().

Referenced by flashc_erase_page().

bool flashc_quick_user_page_read ( void  )

Issues a Quick Page Read User Page command to the FLASHC.

Returns
Whether the User page is erased.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.

References flashc_is_page_erased(), and flashc_issue_command().

Referenced by flashc_erase_user_page().

uint64_t flashc_read_all_gp_fuses ( void  )

Reads all general-purpose fuses.

Returns
The value of all general-purpose fuses as a word.
Note
The actual number of general-purpose fuse bits implemented by hardware is given by AVR32_FLASHC_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

Referenced by flashc_erase_all_gp_fuses(), flashc_erase_gp_fuse_byte(), flashc_read_gp_fuse_bit(), flashc_read_gp_fuse_bitfield(), and flashc_read_gp_fuse_byte().

bool flashc_read_gp_fuse_bit ( unsigned int  gp_fuse_bit)

Reads a general-purpose fuse bit.

Parameters
gp_fuse_bitThe general-purpose fuse bit: 0 to 63.
Returns
The value of the specified general-purpose fuse bit.
Note
The actual number of general-purpose fuse bits implemented by hardware is given by AVR32_FLASHC_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashc_read_all_gp_fuses().

Referenced by flashc_erase_gp_fuse_bit(), and flashc_is_external_privileged_fetch_locked().

uint64_t flashc_read_gp_fuse_bitfield ( unsigned int  pos,
unsigned int  width 
)

Reads a general-purpose fuse bit-field.

Parameters
posThe bit-position of the general-purpose fuse bit-field: 0 to 63.
widthThe bit-width of the general-purpose fuse bit-field: 0 to 64.
Returns
The value of the specified general-purpose fuse bit-field.
Note
The actual number of general-purpose fuse bits implemented by hardware is given by AVR32_FLASHC_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashc_read_all_gp_fuses(), and min.

Referenced by flashc_erase_gp_fuse_bitfield(), and flashc_get_bootloader_protected_size().

uint8_t flashc_read_gp_fuse_byte ( unsigned int  gp_fuse_byte)

Reads a general-purpose fuse byte.

Parameters
gp_fuse_byteThe general-purpose fuse byte: 0 to 7.
Returns
The value of the specified general-purpose fuse byte.
Note
The actual number of general-purpose fuse bits implemented by hardware is given by AVR32_FLASHC_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashc_read_all_gp_fuses().

Referenced by flashc_erase_gp_fuse_byte().

void flashc_set_all_gp_fuses ( uint64_t  value)

Sets all general-purpose fuses with the appropriate erase and write operations.

Parameters
valueThe value of all general-purpose fuses as a word.
Warning
A Lock Error is issued if the Security bit is active.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
The actual number of general-purpose fuse bits implemented by hardware is given by AVR32_FLASHC_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashc_erase_all_gp_fuses(), flashc_error_status, and flashc_write_all_gp_fuses().

unsigned int flashc_set_bootloader_protected_size ( unsigned int  bootprot_size)

Sets the bootloader protected size.

Parameters
bootprot_sizeThe wanted bootloader protected size in bytes. If this size is not supported, the actual size will be the nearest greater available size or the maximal possible size if the requested size is too large.
Returns
The actual bootloader protected size in bytes.
Warning
A Lock Error is issued if the Security bit is active.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.

References clz, flashc_get_bootloader_protected_size(), flashc_set_gp_fuse_bitfield(), max, and min.

void flashc_set_bus_freq ( unsigned int  cpu_f_hz)

Depending on the CPU frequency, set the wait states of flash read accesses.

Parameters
cpu_f_hzThe CPU frequency

References flashc_set_wait_state().

void flashc_set_flash_waitstate_and_readmode ( unsigned long  cpu_f_hz)

Depending to the CPU frequency, set the wait states of flash read accesses and enable or disable the High speed read mode.

Parameters
cpu_f_hzThe CPU frequency

Referenced by pcl_configure_synchronous_clocks(), and pcl_switch_to_osc().

void flashc_set_gp_fuse_bit ( unsigned int  gp_fuse_bit,
bool  value 
)

Sets a general-purpose fuse bit with the appropriate erase and write operations.

Parameters
gp_fuse_bitThe general-purpose fuse bit: 0 to 63.
valueThe value of the specified general-purpose fuse bit.
Warning
A Lock Error is issued if the Security bit is active and the command is applied to BOOTPROT or EPFL fuses.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
The actual number of general-purpose fuse bits implemented by hardware is given by AVR32_FLASHC_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashc_erase_gp_fuse_bit(), and flashc_write_gp_fuse_bit().

Referenced by flashc_lock_external_privileged_fetch(), and flashc_set_gp_fuse_bitfield().

void flashc_set_gp_fuse_bitfield ( unsigned int  pos,
unsigned int  width,
uint64_t  value 
)

Sets a general-purpose fuse bit-field with the appropriate erase and write operations.

Parameters
posThe bit-position of the general-purpose fuse bit-field: 0 to 63.
widthThe bit-width of the general-purpose fuse bit-field: 0 to 64.
valueThe value of the specified general-purpose fuse bit-field.
Warning
A Lock Error is issued if the Security bit is active and the command is applied to BOOTPROT or EPFL fuses.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
The actual number of general-purpose fuse bits implemented by hardware is given by AVR32_FLASHC_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashc_error_status, flashc_set_gp_fuse_bit(), and min.

Referenced by flashc_set_bootloader_protected_size().

void flashc_set_gp_fuse_byte ( unsigned int  gp_fuse_byte,
uint8_t  value 
)

Sets a general-purpose fuse byte with the appropriate erase and write operations.

Parameters
gp_fuse_byteThe general-purpose fuse byte: 0 to 7.
valueThe value of the specified general-purpose fuse byte.
Warning
A Lock Error is issued if the Security bit is active.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
The actual number of general-purpose fuse bits implemented by hardware is given by AVR32_FLASHC_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashc_erase_gp_fuse_byte(), flashc_error_status, and flashc_write_gp_fuse_byte().

void flashc_set_wait_state ( unsigned int  wait_state)

Sets the number of wait states of flash read accesses.

Parameters
wait_stateThe number of wait states of flash read accesses: 0 to 1.

References u_avr32_flashc_fcr_t::fcr, and u_avr32_flashc_fcr_t::FCR.

Referenced by flashc_set_bus_freq(), and pm_configure_clocks().

void flashc_write_all_gp_fuses ( uint64_t  value)

Writes all general-purpose fuses.

Parameters
valueThe value of all general-purpose fuses as a word.
Warning
A Lock Error is issued if the Security bit is active.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
A write operation can only clear bits; in other words, an erase operation must first be done if some bits need to be set to 1.
The actual number of general-purpose fuse bits implemented by hardware is given by AVR32_FLASHC_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashc_error_status, and flashc_write_gp_fuse_byte().

Referenced by flashc_set_all_gp_fuses().

void flashc_write_gp_fuse_bit ( unsigned int  gp_fuse_bit,
bool  value 
)

Writes a general-purpose fuse bit.

Parameters
gp_fuse_bitThe general-purpose fuse bit: 0 to 63.
valueThe value of the specified general-purpose fuse bit.
Warning
A Lock Error is issued if the Security bit is active and the command is applied to BOOTPROT or EPFL fuses.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
A write operation can only clear bits; in other words, an erase operation must first be done if some bits need to be set to 1.
The actual number of general-purpose fuse bits implemented by hardware is given by AVR32_FLASHC_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashc_issue_command().

Referenced by flashc_set_gp_fuse_bit(), and flashc_write_gp_fuse_bitfield().

void flashc_write_gp_fuse_bitfield ( unsigned int  pos,
unsigned int  width,
uint64_t  value 
)

Writes a general-purpose fuse bit-field.

Parameters
posThe bit-position of the general-purpose fuse bit-field: 0 to 63.
widthThe bit-width of the general-purpose fuse bit-field: 0 to 64.
valueThe value of the specified general-purpose fuse bit-field.
Warning
A Lock Error is issued if the Security bit is active and the command is applied to BOOTPROT or EPFL fuses.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
A write operation can only clear bits; in other words, an erase operation must first be done if some bits need to be set to 1.
The actual number of general-purpose fuse bits implemented by hardware is given by AVR32_FLASHC_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashc_error_status, flashc_write_gp_fuse_bit(), and min.

void flashc_write_gp_fuse_byte ( unsigned int  gp_fuse_byte,
uint8_t  value 
)

Writes a general-purpose fuse byte.

Parameters
gp_fuse_byteThe general-purpose fuse byte: 0 to 7.
valueThe value of the specified general-purpose fuse byte.
Warning
A Lock Error is issued if the Security bit is active.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
A write operation can only clear bits; in other words, an erase operation must first be done if some bits need to be set to 1.
The actual number of general-purpose fuse bits implemented by hardware is given by AVR32_FLASHC_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashc_issue_command().

Referenced by flashc_erase_gp_fuse_byte(), flashc_set_gp_fuse_byte(), and flashc_write_all_gp_fuses().

void flashc_write_page ( int  page_number)

Writes a page from the page buffer.

Parameters
page_numberThe page number:
Warning
A Lock Error is issued if the command is applied to a page belonging to a locked region or to the bootloader protected area.
The page buffer is not automatically reset after a page write.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
A write operation can only clear bits; in other words, an erase operation must first be done if some bits need to be set to 1.

References flashc_issue_command().

Referenced by flashc_memcpy(), and flashc_memset64().

void flashc_write_user_page ( void  )

Writes the User page from the page buffer.

Warning
The page buffer is not automatically reset after a page write.
Note
The FLASHC error status returned by flashc_is_lock_error and flashc_is_programming_error is updated.
A write operation can only clear bits; in other words, an erase operation must first be done if some bits need to be set to 1.

References flashc_issue_command().

Referenced by flashc_memcpy(), and flashc_memset64().

unsigned int flashc_error_status = 0
static
void(*volatile flashc_wait_until_ready)(void)

Pointer to the function used by the driver when it needs to wait until the FLASHC is ready to run a new command.

The default function is flashc_default_wait_until_ready. The user may change this pointer to use another implementation.

Referenced by flashc_issue_command().