Main functions.
Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.
#include "usb_protocol_cdc.h"
Functions | |
void | main_cdc_disable (uint8_t port) |
Closes the communication port This is called by CDC interface when USB Host disable it. More... | |
bool | main_cdc_enable (uint8_t port) |
Opens the communication port This is called by CDC interface when USB Host enable it. More... | |
void | main_cdc_set_dtr (uint8_t port, bool b_enable) |
Save new DTR state to change led behavior. The DTR notify that the terminal have open or close the communication port. More... | |
void | main_resume_action (void) |
Turn on a led to notify active mode Called when the USB line is resumed from the suspend state. More... | |
void | main_sof_action (void) |
Manages the leds behaviors Called when a start of frame is received on USB line each 1ms. More... | |
void | main_suspend_action (void) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More... | |
void main_cdc_disable | ( | uint8_t | port | ) |
Closes the communication port This is called by CDC interface when USB Host disable it.
References main_b_cdc_enable, and uart_close().
bool main_cdc_enable | ( | uint8_t | port | ) |
Opens the communication port This is called by CDC interface when USB Host enable it.
true | if cdc startup is successfully done |
References main_b_cdc_enable, and uart_open().
void main_cdc_set_dtr | ( | uint8_t | port, |
bool | b_enable | ||
) |
Save new DTR state to change led behavior. The DTR notify that the terminal have open or close the communication port.
References ui_com_close(), and ui_com_open().
void main_resume_action | ( | void | ) |
Turn on a led to notify active mode Called when the USB line is resumed from the suspend state.
References ui_wakeup().
void main_sof_action | ( | void | ) |
Manages the leds behaviors Called when a start of frame is received on USB line each 1ms.
References main_b_cdc_enable, udd_get_frame_number(), and ui_process().
void main_suspend_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
References ui_powerdown().