Microchip® Advanced Software Framework

ui.c File Reference

User Interface.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include "compiler.h"
#include "conf_usb.h"
#include "board.h"
#include "led.h"
#include "ui.h"

Functions

void ui_com_close (uint8_t port)
 Called when communication port is closed. More...
 
void ui_com_error (void)
 Called when a communication error occur. More...
 
void ui_com_open (uint8_t port)
 Called when communication port is opened. More...
 
void ui_com_overflow (void)
 Called when a overflow occur. More...
 
void ui_com_rx_start (void)
 Called when a data is received on CDC. More...
 
void ui_com_rx_stop (void)
 Called when all data pending are sent on port com. More...
 
void ui_com_tx_start (void)
 Called when a data is received on port com. More...
 
void ui_com_tx_stop (void)
 Called when all data pending are sent on CDC. More...
 
void ui_init (void)
 Called at firmware startup. More...
 
void ui_powerdown (void)
 Called before enter in powerdown mode. More...
 
void ui_process (uint16_t framenumber)
 This process is called each 1ms It is called only if the USB interface is enabled. More...
 
void ui_wakeup (void)
 Called when CPU exit of powerdown mode. More...
 

void ui_com_close ( uint8_t  port)

Called when communication port is closed.

References LED1_GPIO, LED2_GPIO, and LED_Off().

Referenced by main_cdc_set_dtr().

void ui_com_error ( void  )

Called when a communication error occur.

Referenced by usart_handler().

void ui_com_open ( uint8_t  port)

Called when communication port is opened.

References LED1_GPIO, LED2_GPIO, and LED_On().

Referenced by main_cdc_set_dtr().

void ui_com_overflow ( void  )

Called when a overflow occur.

Referenced by usart_handler().

void ui_com_rx_start ( void  )

Called when a data is received on CDC.

Referenced by usart_handler().

void ui_com_rx_stop ( void  )

Called when all data pending are sent on port com.

Referenced by usart_handler().

void ui_com_tx_start ( void  )

Called when a data is received on port com.

Referenced by usart_handler().

void ui_com_tx_stop ( void  )

Called when all data pending are sent on CDC.

Referenced by usart_handler().

void ui_init ( void  )

Called at firmware startup.

References LED0_GPIO, LED1_GPIO, LED2_GPIO, LED_Off(), and LED_On().

Referenced by main().

void ui_powerdown ( void  )

Called before enter in powerdown mode.

References LED0_GPIO, LED1_GPIO, LED2_GPIO, and LED_Off().

Referenced by main(), and main_suspend_action().

void ui_process ( uint16_t  framenumber)

This process is called each 1ms It is called only if the USB interface is enabled.

Parameters
framenumberCurrent frame number

References LED0_GPIO, LED_Off(), and LED_On().

Referenced by main_sof_action().

void ui_wakeup ( void  )

Called when CPU exit of powerdown mode.

References LED0_GPIO, and LED_On().

Referenced by main_resume_action().