USB Device Driver for UOTGHS.
Compliant with common UDD driver.
Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.
#include "conf_usb.h"
#include "sysclk.h"
#include "udd.h"
#include "uotghs_otg.h"
#include "uotghs_device.h"
#include <string.h>
#include "sleep.h"
#include "sleepmgr.h"
Data Structures | |
struct | udd_ep_job_t |
Structure definition about job registered on an endpoint. More... | |
Macros | |
#define | dbg_print(...) |
#define | UDD_BULK_NB_BANK(ep) 2 |
#define | UDD_BULK_NB_BANK_ERROR |
#define | UDD_EP_BULK_NB_BANK_ERROR(ep) (UDD_EP_USED(ep) && UDD_EP_ISO_NBANK_ERROR(ep)) |
#define | UDD_EP_BULK_NBANK_ERROR(ep) ( (UDD_BULK_NB_BANK(ep) < 1) || (UDD_BULK_NB_BANK(ep) > 2) ) |
#define | UDD_EP_DMA_SUPPORTED |
#define | UDD_EP_INT_NB_BANK_ERROR(ep) (UDD_EP_USED(ep) && UDD_EP_ISO_NBANK_ERROR(ep)) |
#define | UDD_EP_INT_NBANK_ERROR(ep) ( (UDD_INTERRUPT_NB_BANK(ep) < 1) || (UDD_INTERRUPT_NB_BANK(ep) > 2) ) |
#define | UDD_EP_ISO_NB_BANK_ERROR(ep) (UDD_EP_USED(ep) && UDD_EP_ISO_NBANK_ERROR(ep)) |
#define | UDD_EP_ISO_NBANK_ERROR(ep) |
#define | UDD_EP_NB_BANK_ERROR(ep, type) (ATPASTE3(UDD_EP_, type, _NB_BANK_ERROR(ep))) |
#define | UDD_EP_USED(ep) (USB_DEVICE_MAX_EP >= ep) |
#define | UDD_INTERRUPT_NB_BANK(ep) 1 |
#define | UDD_INTERRUPT_NB_BANK_ERROR |
#define | UDD_ISO_NB_BANK_ERROR |
#define | UDD_ISOCHRONOUS_NB_BANK(ep) 2 |
#define | UDD_USB_INT_FUN UOTGHS_Handler |
#define | UDD_USB_INT_LEVEL 5 |
Functions | |
if (udd_ctrl_interrupt()) | |
Function called by UOTGHS interrupt to manage USB Device interrupts. More... | |
if (udd_ep_interrupt()) | |
if (Is_udd_reset()) | |
if (Is_udd_suspend_interrupt_enabled()&&Is_udd_suspend()) | |
if (Is_udd_wake_up_interrupt_enabled()&&Is_udd_wake_up()) | |
if (Is_otg_vbus_transition()) | |
void | udd_attach (void) |
Attach device to the bus when possible. More... | |
void | udd_detach (void) |
Detaches the device from the bus. More... | |
void | udd_disable (void) |
Disables the USB Device mode. More... | |
void | udd_enable (void) |
Enables the USB Device mode. More... | |
void | udd_ep_abort (udd_ep_id_t ep) |
Aborts transfer on going on endpoint. More... | |
bool | udd_ep_alloc (udd_ep_id_t ep, uint8_t bmAttributes, uint16_t MaxEndpointSize) |
Configures and enables an endpoint. More... | |
bool | udd_ep_clear_halt (udd_ep_id_t ep) |
Clear the halted state of the endpoint ep. More... | |
void | udd_ep_free (udd_ep_id_t ep) |
Disables an endpoint. More... | |
bool | udd_ep_is_halted (udd_ep_id_t ep) |
Check if the endpoint ep is halted. More... | |
bool | udd_ep_run (udd_ep_id_t ep, bool b_shortpacket, uint8_t *buf, iram_size_t buf_size, udd_callback_trans_t callback) |
Allows to receive or send data on an endpoint. More... | |
bool | udd_ep_set_halt (udd_ep_id_t ep) |
Set the halted state of the endpoint ep. More... | |
bool | udd_ep_wait_stall_clear (udd_ep_id_t ep, udd_callback_halt_cleared_t callback) |
Registers a callback to call when endpoint halt is cleared. More... | |
uint16_t | udd_get_frame_number (void) |
Returns the current start of frame number. More... | |
uint16_t | udd_get_micro_frame_number (void) |
Returns the current micro start of frame number. More... | |
uint8_t | udd_getaddress (void) |
Returns the USB address of device. More... | |
bool | udd_include_vbus_monitoring (void) |
Authorizes the VBUS event. More... | |
bool | udd_is_high_speed (void) |
Test whether the USB Device Controller is running at high speed or not. More... | |
void | udd_send_remotewakeup (void) |
The USB driver sends a resume signal called Upstream Resume. More... | |
void | udd_set_address (uint8_t address) |
Changes the USB address of device. More... | |
void | udd_set_setup_payload (uint8_t *payload, uint16_t payload_size) |
Load setup payload. More... | |
void | udd_test_mode_j (void) |
void | udd_test_mode_k (void) |
void | udd_test_mode_packet (void) |
void | udd_test_mode_se0_nak (void) |
Variables | |
udd_interrupt_end | __pad0__ |
udd_interrupt_sof_end | __pad1__ |
Power management routine. | |
#define | UOTGHS_SLEEP_MODE_USB_SUSPEND SLEEPMGR_WAIT_FAST |
Definition of sleep levels. More... | |
#define | UOTGHS_SLEEP_MODE_USB_IDLE SLEEPMGR_SLEEP_WFI |
static bool | udd_b_idle |
State of USB line. More... | |
static bool | udd_b_sleep_initialized = false |
State of sleep manager. More... | |
static void | udd_sleep_mode (bool b_idle) |
Authorize or not the CPU powerdown mode. More... | |
Control endpoint low level management routine. | |
This function performs control endpoint mangement. It handle the SETUP/DATA/HANDSHAKE phases of a control transaction. | |
enum | udd_ctrl_ep_state_t { UDD_EPCTRL_SETUP = 0, UDD_EPCTRL_DATA_OUT = 1, UDD_EPCTRL_DATA_IN = 2, UDD_EPCTRL_HANDSHAKE_WAIT_IN_ZLP = 3, UDD_EPCTRL_HANDSHAKE_WAIT_OUT_ZLP = 4, UDD_EPCTRL_STALL_REQ = 5 } |
Bit definitions about endpoint control state machine for udd_ep_control_state. More... | |
COMPILER_WORD_ALIGNED udd_ctrl_request_t | udd_g_ctrlreq |
Global variable to give and record information about setup request management. More... | |
static udd_ctrl_ep_state_t | udd_ep_control_state |
State of the endpoint control management. More... | |
static uint16_t | udd_ctrl_prev_payload_buf_cnt |
Total number of data received/sent during data packet phase with previous payload buffers. More... | |
static uint16_t | udd_ctrl_payload_buf_cnt |
Number of data received/sent to/from udd_g_ctrlreq.payload buffer. More... | |
static void | udd_reset_ep_ctrl (void) |
Reset control endpoint. More... | |
static void | udd_ctrl_init (void) |
Reset control endpoint management. More... | |
static void | udd_ctrl_setup_received (void) |
Managed reception of SETUP packet on control endpoint. More... | |
static void | udd_ctrl_in_sent (void) |
Managed reception of IN packet on control endpoint. More... | |
static void | udd_ctrl_out_received (void) |
Managed reception of OUT packet on control endpoint. More... | |
static void | udd_ctrl_underflow (void) |
Managed underflow event of IN packet on control endpoint. More... | |
static void | udd_ctrl_overflow (void) |
Managed overflow event of OUT packet on control endpoint. More... | |
static void | udd_ctrl_stall_data (void) |
Managed stall event of IN/OUT packet on control endpoint. More... | |
static void | udd_ctrl_send_zlp_in (void) |
Send a ZLP IN on control endpoint. More... | |
static void | udd_ctrl_send_zlp_out (void) |
Send a ZLP OUT on control endpoint. More... | |
static void | udd_ctrl_endofrequest (void) |
Call callback associated to setup request. More... | |
static bool | udd_ctrl_interrupt (void) |
Main interrupt routine for control endpoint. More... | |
Management of bulk/interrupt/isochronous endpoints | |
The UDD manages the data transfer on endpoints:
| |
static udd_ep_job_t | udd_ep_job [USB_DEVICE_MAX_EP] |
Array to register a job on bulk/interrupt/isochronous endpoint. More... | |
static void | udd_ep_job_table_reset (void) |
Reset all job table. More... | |
static void | udd_ep_job_table_kill (void) |
Abort all endpoint jobs on going. More... | |
static void | udd_ep_abort_job (udd_ep_id_t ep) |
Abort endpoint job on going. More... | |
static void | udd_ep_finish_job (udd_ep_job_t *ptr_job, bool b_abort, uint8_t ep_num) |
Call the callback associated to the job which is finished. More... | |
static void | udd_ep_trans_done (udd_ep_id_t ep) |
Start the next transfer if necessary or complet the job associated. More... | |
static bool | udd_ep_interrupt (void) |
Main interrupt routine for bulk/interrupt/isochronous endpoints. More... | |
#define dbg_print | ( | ... | ) |
Referenced by if(), udd_ctrl_interrupt(), udd_ep_alloc(), udd_ep_finish_job(), udd_ep_interrupt(), udd_ep_run(), udd_ep_trans_done(), and udd_sleep_mode().
#define UDD_EP_DMA_SUPPORTED |
#define UDD_EP_USED | ( | ep | ) | (USB_DEVICE_MAX_EP >= ep) |
#define UDD_USB_INT_FUN UOTGHS_Handler |
#define UDD_USB_INT_LEVEL 5 |
Referenced by udd_enable().