Microchip® Advanced Software Framework

unit_tests.c File Reference

Main functions for CDC unit test.

Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.

#include <stdio.h>
#include <asf.h>
#include <unit_test/suite.h>
#include <stdio_serial.h>
#include <conf_test.h>

Functions

int main (void)
 Run usb device cdc unit tests. More...
 
void main_cdc_config (void)
 Called by UDI interface Callback running when USB Host send a port configuration. More...
 
void main_cdc_disable (void)
 Called by UDI interface Callback running when USB Host disable CDC interface. More...
 
bool main_cdc_enable (void)
 Called by UDI interface Callback running when USB Host enable CDC interface. More...
 
void main_remotewakeup_disable (void)
 Called by UDC when USB Host request to disable remote wakeup. More...
 
void main_remotewakeup_enable (void)
 Called by UDC when USB Host request to enable remote wakeup. More...
 
void main_resume_action (void)
 Called by UDD when the USB line exit of suspend state. More...
 
void main_sof_action (void)
 Called when a start of frame is received on USB line. More...
 
void main_suspend_action (void)
 Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More...
 
void main_vbus_action (bool b_high)
 Called when Vbus line state change. More...
 
static void run_usb_cdc_config_test (const struct test_case *test)
 
static void run_usb_cdc_test (const struct test_case *test)
 
static void run_usb_resume_test (const struct test_case *test)
 
static void run_usb_sof_test (const struct test_case *test)
 
static void run_usb_suspend_test (const struct test_case *test)
 
static void run_usb_vbus_test (const struct test_case *test)
 

Variables

static bool main_b_cdc_configurated = false
 
static bool main_b_cdc_enumerated = false
 
static bool main_b_resume_event = false
 
static bool main_b_sof_event = false
 
static bool main_b_suspend_event = false
 
static bool main_b_vbus_event = false
 

void main_cdc_config ( void  )

Called by UDI interface Callback running when USB Host send a port configuration.

References main_b_cdc_configurated.

void main_cdc_disable ( void  )

Called by UDI interface Callback running when USB Host disable CDC interface.

References main_b_cdc_enumerated.

bool main_cdc_enable ( void  )

Called by UDI interface Callback running when USB Host enable CDC interface.

Return values
trueif CDC startup is ok

References main_b_cdc_enumerated.

void main_remotewakeup_disable ( void  )

Called by UDC when USB Host request to disable remote wakeup.

void main_remotewakeup_enable ( void  )

Called by UDC when USB Host request to enable remote wakeup.

void main_resume_action ( void  )

Called by UDD when the USB line exit of suspend state.

References main_b_suspend_event.

void main_sof_action ( void  )

Called when a start of frame is received on USB line.

References main_b_sof_event.

void main_suspend_action ( void  )

Enters the application in low power mode Callback called when USB host sets USB line in suspend state.

References main_b_resume_event.

void main_vbus_action ( bool  b_high)

Called when Vbus line state change.

References main_b_vbus_event.

Referenced by run_usb_cdc_test().

static void run_usb_cdc_config_test ( const struct test_case test)
static

References main_b_cdc_configurated, and test_assert_true.

Referenced by main().

static void run_usb_cdc_test ( const struct test_case test)
static
static void run_usb_resume_test ( const struct test_case test)
static

References main_b_resume_event, and test_assert_true.

Referenced by main().

static void run_usb_sof_test ( const struct test_case test)
static

References main_b_sof_event, and test_assert_true.

Referenced by main().

static void run_usb_suspend_test ( const struct test_case test)
static

References main_b_suspend_event, and test_assert_true.

Referenced by main().

static void run_usb_vbus_test ( const struct test_case test)
static

References main_b_vbus_event, and test_assert_true.

Referenced by main().

bool main_b_cdc_configurated = false
static
bool main_b_cdc_enumerated = false
static
bool main_b_resume_event = false
static
bool main_b_sof_event = false
static
bool main_b_suspend_event = false
static
bool main_b_vbus_event = false
static