Microchip® Advanced Software Framework

•All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
PLL Management

This group contains functions and definitions related to configuring and enabling/disabling on-chip PLLs.

A PLL will take an input signal (the source), optionally divide the frequency by a configurable divider, and then multiply the frequency by a configurable multiplier.

Some devices don't support input dividers; specifying any other divisor than 1 on these devices will result in an assertion failure. Other devices may have various restrictions to the frequency range of the input and output signals.

Example: Setting up PLL0 with default parameters

The following example shows how to configure and enable PLL0 using the default parameters specified using the configuration symbols listed above.

To configure, enable PLL0 using the default parameters and to disable a specific feature like Wide Bandwidth Mode (a UC3A3-specific PLL option.), you can use this initialization process.

struct pll_config pllcfg;
if (pll_is_locked(pll_id)) {
return; // Pll already running
}
pll_enable_source(CONFIG_PLL0_SOURCE);
pll_config_defaults(&pllcfg, 0);
pll_enable(&pllcfg, 0);

When the last function call returns, PLL0 is ready to be used as the main system clock source.

Configuration Symbols

Each PLL has a set of default parameters determined by the following configuration symbols in the application's configuration file:

These configuration symbols determine the result of calling pll_config_defaults() and pll_get_default_rate().

Data Structures

struct  pll_config
 Hardware-specific representation of PLL configuration. More...
 

Macros

#define PLL_TIMEOUT_MS   div_ceil(1000 * (PLL_MAX_STARTUP_CYCLES * 2), OSC_SLOW_MIN_HZ)
 Number of milliseconds to wait for PLL lock. More...
 

Enumerations

enum  pll_source {
  PLL_SRC_OSC0 = 0,
  PLL_SRC_OSC1 = 1,
  PLL_NR_SOURCES
}
 PLL clock source. More...
 

Chip-specific PLL characteristics

#define PLL_MAX_STARTUP_CYCLES   ((1 << AVR32_PM_PLL0_PLLCOUNT_SIZE) - 1)
 Maximum PLL startup time in number of slow clock cycles. More...
 
#define NR_PLLS   2
 Number of on-chip PLLs. More...
 
#define PLL_MIN_HZ   40000000
 Minimum frequency that the PLL can generate. More...
 
#define PLL_MAX_HZ   240000000
 Maximum frequency that the PLL can generate. More...
 

PLL configuration

static void pll_config_set_option (struct pll_config *cfg, unsigned int option)
 Set the PLL option bit option in the configuration cfg. More...
 
static void pll_config_clear_option (struct pll_config *cfg, unsigned int option)
 Clear the PLL option bit option in the configuration cfg. More...
 
static void pll_config_init (struct pll_config *cfg, enum pll_source src, unsigned int div, unsigned int mul)
 The PLL options PLL_OPT_VCO_RANGE_LOW and PLL_OPT_OUTPUT_DIV will be set automatically based on the calculated target frequency. More...
 
static void pll_config_read (struct pll_config *cfg, unsigned int pll_id)
 Read the currently active configuration of pll_id. More...
 
static void pll_config_write (const struct pll_config *cfg, unsigned int pll_id)
 Activate the configuration cfg on pll_id. More...
 
#define pll_config_defaults(cfg, pll_id)
 Initialize PLL configuration using default parameters. More...
 
#define pll_get_default_rate(pll_id)
 Get the default rate in Hz of pll_id. More...
 

Interaction with the PLL hardware

static int pll_wait_for_lock (unsigned int pll_id)
 Wait for PLL pll_id to become locked. More...
 
static void pll_enable (const struct pll_config *cfg, unsigned int pll_id)
 Activate the configuration cfg and enable PLL pll_id. More...
 
static void pll_disable (unsigned int pll_id)
 Disable the PLL identified by pll_id. More...
 
static bool pll_is_locked (unsigned int pll_id)
 Determine whether the PLL is locked or not. More...
 
static void pll_enable_source (enum pll_source src)
 Enable the source of the pll. More...
 
static void pll_enable_config_defaults (unsigned int pll_id)
 Enable the pll with the default configuration. More...
 

Chip-specific PLL options

#define PLL_NR_OPTIONS   AVR32_PM_PLL0_PLLOPT_SIZE
 Number of PLL option bits. More...
 
#define PLL_OPT_VCO_RANGE_LOW   0
 VCO frequency range is 80-180 MHz (160-240 MHz if unset). More...
 
#define PLL_OPT_OUTPUT_DIV   1
 Divide output frequency by two. More...
 
#define PLL_OPT_WBM_DISABLE   2
 Disable wide-bandwidth mode. More...
 
#define PLL_VCO_LOW_THRESHOLD
 The threshold under which to set the PLL_OPT_VCO_RANGE_LOW option. More...
 

#define NR_PLLS   2
#define pll_config_defaults (   cfg,
  pll_id 
)
Value:
CONFIG_PLL##pll_id##_SOURCE, \
CONFIG_PLL##pll_id##_DIV, \
CONFIG_PLL##pll_id##_MUL)
static void pll_config_init(struct pll_config *cfg, enum pll_source src, unsigned int div, unsigned int mul)
The PLL options PLL_OPT_VCO_RANGE_LOW and PLL_OPT_OUTPUT_DIV will be set automatically based on the c...
Definition: uc3a0_a1/pll.h:123

Initialize PLL configuration using default parameters.

After this function returns, cfg will contain a configuration which will make the PLL run at (CONFIG_PLLx_MUL / CONFIG_PLLx_DIV) times the frequency of CONFIG_PLLx_SOURCE.

Parameters
cfgThe PLL configuration to be initialized.
pll_idUse defaults for this PLL.
#define pll_get_default_rate (   pll_id)
Value:
((osc_get_rate(CONFIG_PLL##pll_id##_SOURCE) \
* CONFIG_PLL##pll_id##_MUL) \
/ CONFIG_PLL##pll_id##_DIV)
static uint32_t osc_get_rate(uint8_t id)
Return the frequency of oscillator id in Hz.
Definition: uc3a0_a1/osc.h:498

Get the default rate in Hz of pll_id.

Referenced by sysclk_get_main_hz().

#define PLL_MAX_HZ   240000000

Maximum frequency that the PLL can generate.

Referenced by pll_config_init().

#define PLL_MAX_STARTUP_CYCLES   ((1 << AVR32_PM_PLL0_PLLCOUNT_SIZE) - 1)

Maximum PLL startup time in number of slow clock cycles.

Referenced by pll_config_init().

#define PLL_MIN_HZ   40000000

Minimum frequency that the PLL can generate.

Note
The PLL must run at twice this frequency internally, but the output frequency may be divided by two by setting the PLLOPT[1] bit.

Referenced by pll_config_init().

#define PLL_NR_OPTIONS   AVR32_PM_PLL0_PLLOPT_SIZE

Number of PLL option bits.

Number of PLL options.

Referenced by pll_config_clear_option(), and pll_config_set_option().

#define PLL_OPT_OUTPUT_DIV   1

Divide output frequency by two.

Referenced by pll_config_init().

#define PLL_OPT_VCO_RANGE_LOW   0

VCO frequency range is 80-180 MHz (160-240 MHz if unset).

Referenced by pll_config_init().

#define PLL_OPT_WBM_DISABLE   2

Disable wide-bandwidth mode.

#define PLL_TIMEOUT_MS   div_ceil(1000 * (PLL_MAX_STARTUP_CYCLES * 2), OSC_SLOW_MIN_HZ)

Number of milliseconds to wait for PLL lock.

#define PLL_VCO_LOW_THRESHOLD
Value:
((AVR32_PM_PLL_VCO_RANGE0_MIN_FREQ \
+ AVR32_PM_PLL_VCO_RANGE1_MAX_FREQ) / 2)

The threshold under which to set the PLL_OPT_VCO_RANGE_LOW option.

Referenced by pll_config_init().

enum pll_source

PLL clock source.

Enumerator
PLL_SRC_OSC0 

Oscillator 0.

PLL_SRC_OSC1 

Oscillator 1.

PLL_NR_SOURCES 

Number of PLL sources.

void pll_config_clear_option ( struct pll_config cfg,
unsigned int  option 
)
inlinestatic

Clear the PLL option bit option in the configuration cfg.

Parameters
cfgThe PLL configuration to be changed.
optionThe PLL option bit to be cleared.

References Assert, pll_config::ctrl, and PLL_NR_OPTIONS.

void pll_config_init ( struct pll_config cfg,
enum pll_source  src,
unsigned int  div,
unsigned int  mul 
)
inlinestatic

The PLL options PLL_OPT_VCO_RANGE_LOW and PLL_OPT_OUTPUT_DIV will be set automatically based on the calculated target frequency.

Initialize PLL configuration from standard parameters.

Note
This function may be defined inline because it is assumed to be called very few times, and usually with constant parameters. Inlining it will in such cases reduce the code size significantly.
Parameters
cfgThe PLL configuration to be initialized.
srcThe oscillator to be used as input to the PLL.
divPLL input divider.
mulPLL loop divider (i.e. multiplier).
Returns
A configuration which will make the PLL run at (mul / div) times the frequency of src

References Assert, pll_config::ctrl, osc_get_rate(), pll_config_set_option(), PLL_MAX_HZ, PLL_MAX_STARTUP_CYCLES, PLL_MIN_HZ, PLL_NR_SOURCES, PLL_OPT_OUTPUT_DIV, PLL_OPT_VCO_RANGE_LOW, and PLL_VCO_LOW_THRESHOLD.

Referenced by pll_enable_config_defaults().

void pll_config_read ( struct pll_config cfg,
unsigned int  pll_id 
)
inlinestatic

Read the currently active configuration of pll_id.

Parameters
cfgThe configuration object into which to store the currently active configuration.
pll_idThe ID of the PLL to be accessed.

References Assert, pll_config::ctrl, and NR_PLLS.

void pll_config_set_option ( struct pll_config cfg,
unsigned int  option 
)
inlinestatic

Set the PLL option bit option in the configuration cfg.

Parameters
cfgThe PLL configuration to be changed.
optionThe PLL option bit to be set.

References Assert, pll_config::ctrl, and PLL_NR_OPTIONS.

Referenced by pll_config_init().

void pll_config_write ( const struct pll_config cfg,
unsigned int  pll_id 
)
inlinestatic

Activate the configuration cfg on pll_id.

Parameters
cfgThe configuration object representing the PLL configuration to be activated.
pll_idThe ID of the PLL to be updated.

References Assert, pll_config::ctrl, and NR_PLLS.

void pll_disable ( unsigned int  pll_id)
inlinestatic

Disable the PLL identified by pll_id.

After this function is called, the PLL identified by pll_id will be disabled. The PLL configuration stored in hardware may be affected by this, so if the caller needs to restore the same configuration later, it should either do a pll_config_read() before disabling the PLL, or remember the last configuration written to the PLL.

Parameters
pll_idThe ID of the PLL to be disabled.

References Assert, and NR_PLLS.

void pll_enable ( const struct pll_config cfg,
unsigned int  pll_id 
)
inlinestatic

Activate the configuration cfg and enable PLL pll_id.

Parameters
cfgThe PLL configuration to be activated.
pll_idThe ID of the PLL to be enabled.

References Assert, pll_config::ctrl, and NR_PLLS.

Referenced by pll_enable_config_defaults().

void pll_enable_config_defaults ( unsigned int  pll_id)
inlinestatic

Enable the pll with the default configuration.

PLL is enabled, if the PLL is not already locked.

Parameters
pll_idThe ID of the PLL to enable.

References Assert, CONFIG_PLL1_DIV, CONFIG_PLL1_MUL, CONFIG_PLL1_SOURCE, pll_config_init(), pll_enable(), pll_enable_source(), and pll_is_locked().

Referenced by genclk_enable_source(), and sysclk_init().

void pll_enable_source ( enum pll_source  src)
inlinestatic

Enable the source of the pll.

The source is enabled, if the source is not already running.

Parameters
srcThe ID of the PLL source to enable.

References Assert, osc_enable(), OSC_ID_OSC0, OSC_ID_OSC1, osc_is_ready(), osc_wait_ready(), PLL_SRC_OSC0, and PLL_SRC_OSC1.

Referenced by pll_enable_config_defaults().

bool pll_is_locked ( unsigned int  pll_id)
inlinestatic

Determine whether the PLL is locked or not.

Parameters
pll_idThe ID of the PLL to check.
Return values
trueThe PLL is locked and ready to use as a clock source
falseThe PLL is not yet locked, or has not been enabled.

References Assert, and NR_PLLS.

Referenced by pll_enable_config_defaults(), and pll_wait_for_lock().

static int pll_wait_for_lock ( unsigned int  pll_id)
inlinestatic

Wait for PLL pll_id to become locked.

Todo:
Use a timeout to avoid waiting forever and hanging the system
Parameters
pll_idThe ID of the PLL to wait for.
Return values
STATUS_OKThe PLL is now locked.
ERR_TIMEOUTTimed out waiting for PLL to become locked.

References Assert, NR_PLLS, and pll_is_locked().