License | Subject to your compliance with these terms, you may use Microchip software and any derivatives exclusively with Microchip products |
Quick Start Guide for the SPI Master Driver | This is the quick start guide for the SPI Driver, with step-by-step instructions on how to configure and use the driver for a specific use case |
 Basic setup for SPI master on XMEGA devices | |
Quick start guide for SPI master on UC3 devices | |
Quick start guide for SPI driver on AVR32 devices | This is the quick start guide for the SPI - Serial Peripheral Interface, with step-by-step instructions on how to configure and use the driver for a specific use case |
Quick Start Guide for the System Clock Management service (UC3B0/UC3B1) | This is the quick start guide for the System Clock Management service, with step-by-step instructions on how to configure and use the service for specific use cases |
Advanced use case - Peripheral Bus Clock Management (UC3B0/UC3B1) | |
Quick start guide for USB device keyboard module (UDI keyboard) | This is the quick start guide for the USB device keyboard module (UDI keyboard) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 HID keyboard in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
conf_clock.h examples with USB support | Content of XMEGA conf_clock.h: |
Quick start guide for USB device Mass Storage module (UDI MSC) | This is the quick start guide for the USB device interface MSC module (UDI MSC) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 MSC in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
Todo List | |