Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Related Pages
Here is a list of all related documentation pages:
[detail level 12]
oLicenseSubject to your compliance with these terms, you may use Microchip software and any derivatives exclusively with Microchip products
oQuick Start Guide for the System Clock ManagementService (SAM4E)
oAdvanced use case - Peripheral Bus ClockManagement (SAM4E)
oQuick start guide for the SAM PMC moduleThis is the quick start guide for the PMC module, with step-by-step instructions on how to configure and use the driver in a selection of use cases
oQuick start guide for USB device keyboard module (UDI keyboard)This is the quick start guide for the USB device keyboard module (UDI keyboard) with step-by-step instructions on how to configure and use the modules in a selection of use cases
|oHID keyboard in a composite deviceA USB Composite Device is a USB Device which uses more than one USB class
|oChange USB speedIn this use case, the USB device is used with different USB speeds
|oUse USB stringsIn this use case, the usual USB strings is added in the USB device
|oUse USB remote wakeup featureIn this use case, the USB remote wakeup feature is enabled
|oBus power application recommendationsIn this use case, the USB device BUS power feature is enabled
|\USB dynamic serial numberIn this use case, the USB serial strings is dynamic
oconf_clock.h examples with USB supportContent of XMEGA conf_clock.h:
oQuick start guide for the common IOPORT serviceThis is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases
|\Advanced use case doing port accessIn this case we will read out the pins from one whole port and write the read value to another port
oQuick Start Guide for the SAM PIO driverThis is the quick start guide for the PIO Driver, with step-by-step instructions on how to configure and use the driver for specific use cases
oAdvanced use case - Interrupt driven edge detection
oQuick start guide for USB device Mass Storage module (UDI MSC)This is the quick start guide for the USB device interface MSC module (UDI MSC) with step-by-step instructions on how to configure and use the modules in a selection of use cases
|oMSC in a composite deviceA USB Composite Device is a USB Device which uses more than one USB class
|oChange USB speedIn this use case, the USB device is used with different USB speeds
|oUse USB stringsIn this use case, the usual USB strings is added in the USB device
|oUse USB remote wakeup featureIn this use case, the USB remote wakeup feature is enabled
|oBus power application recommendationsIn this use case, the USB device BUS power feature is enabled
|\USB dynamic serial numberIn this use case, the USB serial strings is dynamic
o"SAM4E-EK - Operating frequencies"This page lists several definition related to the board operating frequency
o"SAM4E-EK - Board informations"This page lists several definition related to the board description
o"SAM4E-EK - USB device"
o"SAM4E-EK - External components"This page lists the definitions related to external on-board components located in the board.h file for the SAM4E-EK
o"SAM4E-EK - Memories"This page lists definitions related to internal & external on-board memories
o"SAM4E-EK - CAN"This page lists definitions related to CAN0 and CAN1
\Todo List