Microchip® Advanced Software Framework

ui.c File Reference

User Interface.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include <asf.h>
#include "ui.h"

Macros

#define SEQUENCE_PERIOD   150
 Sequence process running each SEQUENCE_PERIOD ms. More...
 
#define UI_WAKEUP_BPM_SRC   BPM_BKUPWEN_EIC
 
#define UI_WAKEUP_EIC_LINE   GPIO_PUSH_BUTTON_EIC_LINE
 
#define UI_WAKEUP_HANDLER   button_handler
 
#define UI_WAKEUP_IRQ_LEVEL   5
 
#define UI_WAKEUP_IRQN   EIC_5_IRQn
 

Functions

void ui_init (void)
 Initializes the user interface. More...
 
void ui_kbd_led (uint8_t value)
 Turn on or off the keyboard LEDs. More...
 
void ui_powerdown (void)
 Enters the user interface in power down mode. More...
 
void ui_process (uint16_t framenumber)
 This process is called each 1ms It is called only if the USB interface is enabled. More...
 
void ui_start_read (void)
 
void ui_start_write (void)
 
void ui_stop_read (void)
 
void ui_stop_write (void)
 
void ui_wakeup (void)
 Exits the user interface of power down mode. More...
 
void ui_wakeup_disable (void)
 Disables the asynchronous interrupts of the user interface. More...
 
void ui_wakeup_enable (void)
 Enables the asynchronous interrupts of the user interface. More...
 
Internal routines to manage asynchronous interrupt pin change

This interrupt is connected to a switch and allows to wakeup CPU in low sleep mode. This wakeup the USB devices connected via a downstream resume.

static void ui_enable_asynchronous_interrupt (void)
 Initializes and enables interrupt pin change. More...
 
static void ui_disable_asynchronous_interrupt (void)
 Disables interrupt pin change. More...
 
static void UI_WAKEUP_HANDLER (void)
 

Variables

static bool btn_wakeup = false
 Wakeup, ignore button change until button is back to default state. More...
 
struct {
   bool   b_down
 
   bool   b_modifier
 
   uint8_t   u8_value
 
ui_sequence []
 

#define SEQUENCE_PERIOD   150

Sequence process running each SEQUENCE_PERIOD ms.

Referenced by ui_process().

#define UI_WAKEUP_BPM_SRC   BPM_BKUPWEN_EIC
#define UI_WAKEUP_HANDLER   button_handler
#define UI_WAKEUP_IRQ_LEVEL   5
#define UI_WAKEUP_IRQN   EIC_5_IRQn

static void ui_disable_asynchronous_interrupt ( void  )
static
void ui_init ( void  )

Initializes the user interface.

References LED0, and LED_On.

Referenced by main().

void ui_kbd_led ( uint8_t  value)

Turn on or off the keyboard LEDs.

References UNUSED.

void ui_powerdown ( void  )

Enters the user interface in power down mode.

References LED0, and LED_Off.

Referenced by main(), and main_suspend_action().

void ui_process ( uint16_t  framenumber)

This process is called each 1ms It is called only if the USB interface is enabled.

Parameters
framenumberCurrent frame number

References b_down, b_modifier, btn_wakeup, GPIO_PUSH_BUTTON_0, ioport_get_pin_level(), LED0, LED_Off, LED_On, SEQUENCE_PERIOD, u8_value, udi_hid_kbd_down(), udi_hid_kbd_modifier_down(), udi_hid_kbd_modifier_up(), udi_hid_kbd_up(), and ui_sequence.

Referenced by main_sof_action().

void ui_start_read ( void  )
void ui_start_write ( void  )
void ui_stop_read ( void  )
void ui_stop_write ( void  )
void ui_wakeup ( void  )

Exits the user interface of power down mode.

References LED0, and LED_On.

Referenced by main_resume_action().

void ui_wakeup_disable ( void  )

Disables the asynchronous interrupts of the user interface.

References ui_disable_asynchronous_interrupt().

Referenced by main_remotewakeup_disable().

void ui_wakeup_enable ( void  )

Enables the asynchronous interrupts of the user interface.

References ui_enable_asynchronous_interrupt().

Referenced by main_remotewakeup_enable().

bool b_down

Referenced by ui_process().

bool b_modifier

Referenced by ui_process().

bool btn_wakeup = false
static

Wakeup, ignore button change until button is back to default state.

Referenced by ui_process(), and UI_WAKEUP_HANDLER().

uint8_t u8_value

Referenced by ui_process().

struct { ... } ui_sequence[]

Referenced by ui_process().