User Interface | Human interface on SAME70-Xplained: |
Virtual Memory in RAM | The component manages a disk on a volatile memory (internal RAM) |
Power Management Controller (PMC) | |
Peripheral Parallel Input/Output (PIO) Controller | |
Descriptors for a USB Device | Composite |
MPU - Memory Protect Unit | |
MMU Initialization | |
Memory Control Access | Common abstraction layer for memory interfaces |
Clock Management | |
Generic Clock Management | Generic clocks are configurable clocks which run outside the system clock domain |
Oscillator Management | This group contains functions and definitions related to configuring and enabling/disabling on-chip oscillators |
PLL Management | This group contains functions and definitions related to configuring and enabling/disabling on-chip PLLs |
System Clock Management | See Quick Start Guide for the System Clock Management |
Power Manager (PM) | This is a stub on the SAM Power Manager Control (PMC) for the sleepmgr service |
Compiler abstraction layer and code utilities | Compiler abstraction layer and code utilities for AT91SAM |
Preprocessor - Macro Repeat | |
Preprocessor - Stringize | |
Preprocessor - Token Paste | |
Global interrupt management | This is a driver for global enabling and disabling of interrupts |
Deprecated interrupt definitions | |
Atmel part identification macros | This collection of macros identify which series and families that the various Atmel parts belong to |
AVR UC3 parts | |
AVR XMEGA parts | |
megaAVR parts | |
SAM parts | |
Sleep manager | The sleep manager is a service for ensuring that the device is not put to sleep in deeper sleep modes than the system (e.g., peripheral drivers, services or the application) allows at any given time |
Common IOPORT API | See Quick start guide for the common IOPORT service |
USB Stack | This stack includes the USB Device Stack, USB Host Stack and common definitions |
USB Stack Device | This module includes USB Stack Device implementation |
USB Device Controller (UDC) | The UDC provides a high-level abstraction of the usb device |
Implementation of UDC | Internal implementation |
USB Device Controller (UDC) - Prerequisites | Common prerequisites for all USB devices |
USB Device Controller (UDC) - Example code | Common example code for all USB devices |
USB Device Controller (UDC) - Workflow | Common workflow for all USB devices |
USB Device Descriptor | |
USB Device Driver (UDD) | The UDD driver provides a low-level abstraction of the device controller hardware |
USB High-Speed Port for device mode (USBHS) | USBHS low-level driver for USB device mode |
USB Device Interface (UDI) | The UDI provides a common API for all classes, and this is used by UDC for the main control of USB Device interface |
USB Device Interface (UDI) for Human Interface Device (HID) | Common library for all Human Interface Device (HID) implementation |
Implementation of HID common library | |
USB Device Interface (UDI) for Human Interface Device (HID) Keyboard Class | Common APIs used by high level application to use this USB class |
Interface with USB Device Core (UDC) | Structures and functions required by UDC |
Implementation of UDI HID keyboard | Class internal implementation |
USB interface descriptors | The following structures provide predefined USB interface descriptors |
USB interface descriptors | The following structures provide predefined USB interface descriptors |
Interface with USB Device Core (UDC) | Structures and functions required by UDC |
Implementation of UDI MSC | Class internal implementation |
USBHS OTG Driver | USBHS low-level driver for OTG features |
Atmel USB Identifiers | This module defines Atmel PID and VIDs constants |
USB Protocol Definitions | This module defines constants and data structures provided by the USB 2.0 specification |
USB Human Interface Device (HID) | Protocol definitions |
USB Mass Storage Class (MSC) protocol definitions | |
SCSI Block Commands protocol definitions | |
SCSI Primary Commands protocol definitions | |
Generic board support | The generic board support module includes board-specific definitions and function prototypes, such as the board initialization function |
General Purpose Input/Output | This is the common API for GPIO |