Microchip® Advanced Software Framework

ui.c File Reference

User Interface.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include "compiler.h"
#include "conf_usb.h"
#include "udi_msc.h"
#include "udc.h"
#include "udi_hid_mouse.h"
#include "board.h"
#include "led.h"
#include "ui.h"
#include "pio.h"
#include "pio_handler.h"
#include "pmc.h"

Macros

#define MOUSE_MOVE_RANGE   3
 
#define WAKEUP_PIN   (GPIO_PUSH_BUTTON_2)
 
#define WAKEUP_PIO   (PIN_PUSHBUTTON_2_PIO)
 
#define WAKEUP_PIO_ATTR   (PIN_PUSHBUTTON_2_ATTR)
 
#define WAKEUP_PIO_ID   (PIN_PUSHBUTTON_2_ID)
 
#define WAKEUP_PIO_MASK   (PIN_PUSHBUTTON_2_MASK)
 
#define WAKEUP_PMC_FSTT   (PMC_FSMR_FSTT14)
 

Functions

void ui_init (void)
 Initializes the user interface. More...
 
void ui_powerdown (void)
 Sets the user interface in power down mode. More...
 
void ui_process (uint16_t framenumber)
 This process is called each 1ms It is called only if the USB interface is enabled. More...
 
void ui_start_read (void)
 
void ui_start_write (void)
 
void ui_stop_read (void)
 
void ui_stop_write (void)
 
void ui_wakeup (void)
 Exits the user interface of power down mode. More...
 
void ui_wakeup_disable (void)
 Disables the asynchronous interrupts of the user interface. More...
 
void ui_wakeup_enable (void)
 Enables the asynchronous interrupts of the user interface. More...
 
static void ui_wakeup_handler (uint32_t id, uint32_t mask)
 

#define MOUSE_MOVE_RANGE   3

Referenced by ui_process().

#define WAKEUP_PIN   (GPIO_PUSH_BUTTON_2)
#define WAKEUP_PIO   (PIN_PUSHBUTTON_2_PIO)

Referenced by ui_init().

#define WAKEUP_PIO_ATTR   (PIN_PUSHBUTTON_2_ATTR)

Referenced by ui_init(), and ui_wakeup_enable().

#define WAKEUP_PIO_ID   (PIN_PUSHBUTTON_2_ID)

Referenced by ui_init(), and ui_wakeup_handler().

#define WAKEUP_PIO_MASK   (PIN_PUSHBUTTON_2_MASK)

Referenced by ui_init(), and ui_wakeup_handler().

#define WAKEUP_PMC_FSTT   (PMC_FSMR_FSTT14)

void ui_init ( void  )
void ui_powerdown ( void  )

Sets the user interface in power down mode.

References LED0_GPIO, LED1_GPIO, LED2_GPIO, and LED_Off().

Referenced by main(), and main_suspend_action().

void ui_process ( uint16_t  framenumber)

This process is called each 1ms It is called only if the USB interface is enabled.

Parameters
framenumberCurrent frame number

References gpio_pin_is_high, GPIO_PUSH_BUTTON_1, GPIO_PUSH_BUTTON_2, LED0_GPIO, LED_Off(), LED_On(), MOUSE_MOVE_RANGE, and udi_hid_mouse_moveX().

Referenced by main_sof_action().

void ui_start_read ( void  )

References LED1_GPIO, and LED_On().

void ui_start_write ( void  )

References LED2_GPIO, and LED_On().

void ui_stop_read ( void  )

References LED1_GPIO, and LED_Off().

void ui_stop_write ( void  )

References LED2_GPIO, and LED_Off().

void ui_wakeup ( void  )

Exits the user interface of power down mode.

References LED0_GPIO, and LED_On().

Referenced by main_resume_action().

void ui_wakeup_disable ( void  )

Disables the asynchronous interrupts of the user interface.

References pio_disable_pin_interrupt(), pmc_clr_fast_startup_input(), WAKEUP_PIN, and WAKEUP_PMC_FSTT.

Referenced by main_remotewakeup_disable().

void ui_wakeup_enable ( void  )

Enables the asynchronous interrupts of the user interface.

References pio_configure_pin(), pio_enable_pin_interrupt(), pmc_set_fast_startup_input(), WAKEUP_PIN, WAKEUP_PIO_ATTR, and WAKEUP_PMC_FSTT.

Referenced by main_remotewakeup_enable().

static void ui_wakeup_handler ( uint32_t  id,
uint32_t  mask 
)
static

References udc_remotewakeup(), WAKEUP_PIO_ID, and WAKEUP_PIO_MASK.

Referenced by ui_init().