SCSI Mode Parameter Header used by MODE SELECT(6) and MODE SENSE(6)
#include <spc_protocol.h>
Data Fields | |
uint8_t | block_descriptor_length |
Length of block descriptors. More... | |
uint8_t | device_specific_parameter |
Defined by command set. More... | |
uint8_t | medium_type |
Medium Type. More... | |
uint8_t | mode_data_length |
Number of bytes after this. More... | |
uint8_t scsi_mode_param_header6::block_descriptor_length |
Length of block descriptors.
uint8_t scsi_mode_param_header6::device_specific_parameter |
Defined by command set.
uint8_t scsi_mode_param_header6::medium_type |
Medium Type.
uint8_t scsi_mode_param_header6::mode_data_length |
Number of bytes after this.