Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Modules
Here is a list of all modules:
[detail level 123456]
oUser InterfaceHuman interface on SAM4E-EK:
oVirtual Memory in RAMThe component manages a disk on a volatile memory (internal RAM)
oUniversal Synchronous AsynchronousReceiver Transmitter (USART)
oPower Management Controller (PMC)
oDescriptors for a USB DeviceComposite
oMatrix (MATRIX)
oPeripheral Parallel Input/Output (PIO) Controller
oMemory Control AccessCommon abstraction layer for memory interfaces
oUniversal Synchronous Asynchronous ReceiverTransmitter (USART)
oClock Management
|oGeneric Clock ManagementGeneric clocks are configurable clocks which run outside the system clock domain
|oOscillator ManagementThis group contains functions and definitions related to configuring and enabling/disabling on-chip oscillators
|oPLL ManagementThis group contains functions and definitions related to configuring and enabling/disabling on-chip PLLs
|\System Clock ManagementSee Quick Start Guide for the System Clock Management
oPower Manager (PM)This is a stub on the SAM Power Manager Control (PMC) for the sleepmgr service
oCompiler abstraction layer and code utilitiesCompiler abstraction layer and code utilities for AT91SAM
|oPreprocessor - Macro Repeat
|oPreprocessor - Stringize
|\Preprocessor - Token Paste
oGlobal interrupt managementThis is a driver for global enabling and disabling of interrupts
|\Deprecated interrupt definitions
oAtmel part identification macrosThis collection of macros identify which series and families that the various Atmel parts belong to
|oAVR UC3 parts
|oAVR XMEGA parts
|omegaAVR parts
|\SAM parts
oSleep managerThe sleep manager is a service for ensuring that the device is not put to sleep in deeper sleep modes than the system (e.g., peripheral drivers, services or the application) allows at any given time
oCommon IOPORT APISee Quick start guide for the common IOPORT service
oUSB StackThis stack includes the USB Device Stack, USB Host Stack and common definitions
|oUSB Stack DeviceThis module includes USB Stack Device implementation
||oUSB Device Controller (UDC)The UDC provides a high-level abstraction of the usb device
|||oImplementation of UDCInternal implementation
|||oUSB Device Controller (UDC) - PrerequisitesCommon prerequisites for all USB devices
|||oUSB Device Controller (UDC) - Example codeCommon example code for all USB devices
|||oUSB Device Controller (UDC) - WorkflowCommon workflow for all USB devices
|||\USB Device Descriptor
||oUSB Device Driver (UDD)The UDD driver provides a low-level abstraction of the device controller hardware
|||\USB Device Port DriverUDP low-level driver for USB device mode
||\USB Device Interface (UDI)The UDI provides a common API for all classes, and this is used by UDC for the main control of USB Device interface
|| oUSB Device Interface (UDI) for Communication Class Device (CDC)Common APIs used by high level application to use this USB class
|| |oInterface with USB Device Core (UDC)Structures and functions required by UDC
|| |oImplementation of UDI CDCClass internal implementation
|| |\USB interface descriptorsThe following structures provide predefined USB interface descriptors
|| oUSB Device Interface (UDI) for Human Interface Device (HID)Common library for all Human Interface Device (HID) implementation
|| |oImplementation of HID common library
|| |oUSB Device Interface (UDI) for Human Interface Device (HID) Keyboard ClassCommon APIs used by high level application to use this USB class
|| ||oInterface with USB Device Core (UDC)Structures and functions required by UDC
|| ||oImplementation of UDI HID keyboardClass internal implementation
|| ||\USB interface descriptorsThe following structures provide predefined USB interface descriptors
|| |\USB Device Interface (UDI) for Human Interface Device (HID) Mouse ClassCommon APIs used by high level application to use this USB class
|| | oInterface with USB Device Core (UDC)Structures and functions required by UDC
|| | oImplementation of UDI HID MouseClass internal implementation
|| | \USB interface descriptorsThe following structures provide predefined USB interface descriptors
|| \USB interface descriptorsThe following structures provide predefined USB interface descriptors
||  oInterface with USB Device Core (UDC)Structures and functions required by UDC
||  \Implementation of UDI MSCClass internal implementation
|oAtmel USB IdentifiersThis module defines Atmel PID and VIDs constants
|\USB Protocol DefinitionsThis module defines constants and data structures provided by the USB 2.0 specification
| oCommunication Device Class Definitions
| oUSB Human Interface Device (HID)Protocol definitions
| \USB Mass Storage Class (MSC) protocol definitions
|  oSCSI Block Commands protocol definitions
|  \SCSI Primary Commands protocol definitions
\Generic board supportThe generic board support module includes board-specific definitions and function prototypes, such as the board initialization function