Microchip® Advanced Software Framework

ui.c File Reference

User Interface.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include <asf.h>
#include "ui.h"

Macros

#define MOUSE_MOVE_COUNT   50
 
#define MOUSE_MOVE_RANGE   3
 
#define MOVE_DOWN   2
 
#define MOVE_LEFT   3
 
#define MOVE_RIGHT   1
 
#define MOVE_UP   0
 
#define SEQUENCE_PERIOD   150
 
#define WAKEUP_PIN   (GPIO_PUSH_BUTTON_1)
 
#define WAKEUP_PIO   (PIN_PUSHBUTTON_1_PIO)
 
#define WAKEUP_PIO_ATTR   (PIO_INPUT | PIO_PULLUP | PIO_DEBOUNCE | PIO_IT_LOW_LEVEL)
 
#define WAKEUP_PIO_ID   (PIN_PUSHBUTTON_1_ID)
 
#define WAKEUP_PIO_MASK   (PIN_PUSHBUTTON_1_MASK)
 

Functions

void ui_com_close (uint8_t port)
 Called when communication port is closed. More...
 
void ui_com_error (void)
 Called when a communication error occur. More...
 
void ui_com_open (uint8_t port)
 Called when communication port is opened. More...
 
void ui_com_overflow (void)
 Called when a overflow occur. More...
 
void ui_com_rx_start (void)
 Called when a data is received on CDC. More...
 
void ui_com_rx_stop (void)
 Called when all data pending are sent on port com. More...
 
void ui_com_tx_start (void)
 Called when a data is received on port com. More...
 
void ui_com_tx_stop (void)
 Called when all data pending are sent on CDC. More...
 
void ui_init (void)
 Initializes the user interface. More...
 
void ui_kbd_led (uint8_t value)
 Turn on or off the keyboard LEDs. More...
 
void ui_powerdown (void)
 Enters the user interface in power down mode. More...
 
void ui_process (uint16_t framenumber)
 This process is called each 1ms It is called only if the USB interface is enabled. More...
 
void ui_start_read (void)
 
void ui_start_write (void)
 
void ui_stop_read (void)
 
void ui_stop_write (void)
 
void ui_wakeup (void)
 Exits the user interface of power down mode. More...
 
void ui_wakeup_disable (void)
 Disables the asynchronous interrupts of the user interface. More...
 
void ui_wakeup_enable (void)
 Enables the asynchronous interrupts of the user interface. More...
 
static void ui_wakeup_handler (uint32_t id, uint32_t mask)
 

Variables

static int32_t move_count = MOUSE_MOVE_COUNT
 
static uint8_t move_dir = MOVE_UP
 
struct {
   bool   b_down
 
   bool   b_modifier
 
   uint8_t   u8_value
 
ui_sequence []
 

#define MOUSE_MOVE_COUNT   50

Referenced by ui_process().

#define MOUSE_MOVE_RANGE   3

Referenced by ui_process().

#define MOVE_DOWN   2

Referenced by ui_process().

#define MOVE_LEFT   3

Referenced by ui_process().

#define MOVE_RIGHT   1

Referenced by ui_process().

#define MOVE_UP   0

Referenced by ui_process().

#define SEQUENCE_PERIOD   150

Sequence process running each SEQUENCE_PERIOD ms

Referenced by ui_process().

#define WAKEUP_PIN   (GPIO_PUSH_BUTTON_1)
#define WAKEUP_PIO   (PIN_PUSHBUTTON_1_PIO)

Referenced by ui_init().

#define WAKEUP_PIO_ATTR   (PIO_INPUT | PIO_PULLUP | PIO_DEBOUNCE | PIO_IT_LOW_LEVEL)

Referenced by ui_init(), and ui_wakeup_enable().

#define WAKEUP_PIO_ID   (PIN_PUSHBUTTON_1_ID)

Referenced by ui_init(), and ui_wakeup_handler().

#define WAKEUP_PIO_MASK   (PIN_PUSHBUTTON_1_MASK)

Referenced by ui_init(), and ui_wakeup_handler().

void ui_com_close ( uint8_t  port)

Called when communication port is closed.

References UNUSED.

Referenced by main_cdc_set_dtr().

void ui_com_error ( void  )

Called when a communication error occur.

Referenced by ISR().

void ui_com_open ( uint8_t  port)

Called when communication port is opened.

References UNUSED.

Referenced by main_cdc_set_dtr().

void ui_com_overflow ( void  )

Called when a overflow occur.

Referenced by ISR().

void ui_com_rx_start ( void  )

Called when a data is received on CDC.

Referenced by ISR().

void ui_com_rx_stop ( void  )

Called when all data pending are sent on port com.

Referenced by ISR().

void ui_com_tx_start ( void  )

Called when a data is received on port com.

Referenced by ISR().

void ui_com_tx_stop ( void  )

Called when all data pending are sent on CDC.

Referenced by ISR().

void ui_init ( void  )
void ui_kbd_led ( uint8_t  value)

Turn on or off the keyboard LEDs.

References UNUSED.

void ui_powerdown ( void  )

Enters the user interface in power down mode.

References LED_Off.

Referenced by main(), and main_suspend_action().

void ui_process ( uint16_t  framenumber)
void ui_start_read ( void  )
void ui_start_write ( void  )
void ui_stop_read ( void  )
void ui_stop_write ( void  )
void ui_wakeup ( void  )

Exits the user interface of power down mode.

References LED_On.

Referenced by main_resume_action().

void ui_wakeup_disable ( void  )

Disables the asynchronous interrupts of the user interface.

References pio_disable_pin_interrupt(), and WAKEUP_PIN.

Referenced by main_remotewakeup_disable().

void ui_wakeup_enable ( void  )

Enables the asynchronous interrupts of the user interface.

References pio_configure_pin(), pio_enable_pin_interrupt(), WAKEUP_PIN, and WAKEUP_PIO_ATTR.

Referenced by main_remotewakeup_enable().

static void ui_wakeup_handler ( uint32_t  id,
uint32_t  mask 
)
static

References udc_remotewakeup(), WAKEUP_PIO_ID, and WAKEUP_PIO_MASK.

Referenced by ui_init().

bool b_down

Referenced by ui_process().

bool b_modifier

Referenced by ui_process().

int32_t move_count = MOUSE_MOVE_COUNT
static

Referenced by ui_process().

uint8_t move_dir = MOVE_UP
static

Referenced by ui_process().

uint8_t u8_value

Referenced by ui_process().

struct { ... } ui_sequence[]

Referenced by ui_process().