Microchip® Advanced Software Framework

uotghs_otg.h File Reference

USB OTG Driver for UOTGHS.

Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.

#include "compiler.h"

Macros

UOTGHS OTG ID pin management

The ID pin come from the USB OTG connector (A and B receptable) and allows to select the USB mode host or device.

The UOTGHS hardware can manage it automatically. This feature is optional. When USB_ID_GPIO is defined (in board.h), this feature is enabled.

#define otg_enable_id_pin()   (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_UIDE))
 Enable external OTG_ID pin (listened to by USB) More...
 
#define otg_disable_id_pin()   (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_UIDE))
 Disable external OTG_ID pin (ignored by USB) More...
 
#define Is_otg_id_pin_enabled()   (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_UIDE))
 Test if external OTG_ID pin enabled (listened to by USB) More...
 
#define otg_force_device_mode()   (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_UIMOD), otg_disable_id_pin())
 Disable external OTG_ID pin and force device mode. More...
 
#define Is_otg_device_mode_forced()   (!Is_otg_id_pin_enabled() && Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_UIMOD))
 Test if device mode is forced. More...
 
#define otg_force_host_mode()   (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_UIMOD), otg_disable_id_pin())
 Disable external OTG_ID pin and force host mode. More...
 
#define Is_otg_host_mode_forced()   (!Is_otg_id_pin_enabled() && !Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_UIMOD))
 Test if host mode is forced. More...
 
UOTGHS OTG ID pin interrupt management

These macros manage the ID pin interrupt

#define otg_enable_id_interrupt()   (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_IDTE))
 
#define otg_disable_id_interrupt()   (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_IDTE))
 
#define Is_otg_id_interrupt_enabled()   (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_IDTE))
 
#define Is_otg_id_device()   (Tst_bits(UOTGHS->UOTGHS_SR, UOTGHS_SR_ID))
 
#define Is_otg_id_host()   (!Is_otg_id_device())
 
#define otg_ack_id_transition()   (UOTGHS->UOTGHS_SCR = UOTGHS_SCR_IDTIC)
 
#define otg_raise_id_transition()   (UOTGHS->UOTGHS_SFR = UOTGHS_SFR_IDTIS)
 
#define Is_otg_id_transition()   (Tst_bits(UOTGHS->UOTGHS_SR, UOTGHS_SR_IDTI))
 
OTG Vbus management
#define otg_enable_vbus_interrupt()   (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_VBUSTE))
 
#define otg_disable_vbus_interrupt()   (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_VBUSTE))
 
#define Is_otg_vbus_interrupt_enabled()   (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_VBUSTE))
 
#define Is_otg_vbus_high()   (Tst_bits(UOTGHS->UOTGHS_SR, UOTGHS_SR_VBUS))
 
#define Is_otg_vbus_low()   (!Is_otg_vbus_high())
 
#define otg_ack_vbus_transition()   (UOTGHS->UOTGHS_SCR = UOTGHS_SCR_VBUSTIC)
 
#define otg_raise_vbus_transition()   (UOTGHS->UOTGHS_SFR = UOTGHS_SFR_VBUSTIS)
 
#define Is_otg_vbus_transition()   (Tst_bits(UOTGHS->UOTGHS_SR, UOTGHS_SR_VBUSTI))
 
UOTGHS OTG main management

These macros allows to enable/disable pad and UOTGHS hardware

#define otg_reset()
 Reset USB macro. More...
 
#define otg_enable()   (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_USBE))
 Enable USB macro. More...
 
#define otg_disable()   (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_USBE))
 Disable USB macro. More...
 
#define Is_otg_enabled()   (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_USBE))
 
#define otg_enable_pad()   (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_OTGPADE))
 Enable OTG pad. More...
 
#define otg_disable_pad()   (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_OTGPADE))
 Disable OTG pad. More...
 
#define Is_otg_pad_enabled()   (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_OTGPADE))
 
#define Is_otg_clock_usable()   (Tst_bits(UOTGHS->UOTGHS_SR, UOTGHS_SR_CLKUSABLE))
 Check Clock Usable For parts with HS feature, this one corresponding at UTMI clock. More...
 
#define otg_freeze_clock()   (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_FRZCLK))
 Stop (freeze) internal USB clock. More...
 
#define otg_unfreeze_clock()   (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_FRZCLK))
 
#define Is_otg_clock_frozen()   (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_FRZCLK))
 
#define otg_configure_timeout(timer, timeout)
 Configure time-out of specified OTG timer. More...
 
#define otg_get_timeout(timer)
 Get configured time-out of specified OTG timer. More...
 
#define otg_get_fsm_drd_state()   (Rd_bitfield(UOTGHS->UOTGHS_FSM, UOTGHS_FSM_DRDSTATE_Msk))
 Get the dual-role device state of the internal USB finite state machine of the UOTGHS controller. More...
 
#define Is_otg_a_suspend()   (4==otg_get_fsm_drd_state())
 
#define Is_otg_a_wait_vrise()   (1==otg_get_fsm_drd_state())
 
UOTGHS OTG hardware protocol

These macros manages the hardware OTG protocol

#define otg_device_initiate_hnp()   (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_HNPREQ))
 Initiates a Host negotiation Protocol. More...
 
#define otg_host_accept_hnp()   (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_HNPREQ))
 Accepts a Host negotiation Protocol. More...
 
#define otg_host_reject_hnp()   (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_HNPREQ))
 Rejects a Host negotiation Protocol. More...
 
#define otg_device_initiate_srp()   (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_SRPREQ))
 initiates a Session Request Protocol More...
 
#define otg_select_vbus_srp_method()   (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_SRPSEL))
 Selects VBus as SRP method. More...
 
#define Is_otg_vbus_srp_method_selected()   (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_SRPSEL))
 
#define otg_select_data_srp_method()   (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_SRPSEL))
 Selects data line as SRP method. More...
 
#define Is_otg_data_srp_method_selected()   (!Is_otg_vbus_srp_method_selected())
 
#define Is_otg_hnp()   (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_HNPREQ))
 Tests if a HNP occurs. More...
 
#define Is_otg_device_srp()   (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_SRPREQ))
 Tests if a SRP from device occurs. More...
 
#define otg_enable_hnp_error_interrupt()   (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_HNPERRE))
 Enables HNP error interrupt. More...
 
#define otg_disable_hnp_error_interrupt()   (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_HNPERRE))
 Disables HNP error interrupt. More...
 
#define Is_otg_hnp_error_interrupt_enabled()   (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_HNPERRE))
 
#define otg_ack_hnp_error_interrupt()   (UOTGHS->UOTGHS_SCR = UOTGHS_SCR_HNPERRIC)
 ACKs HNP error interrupt. More...
 
#define otg_raise_hnp_error_interrupt()   (UOTGHS->UOTGHS_SFR = UOTGHS_SFR_HNPERRIS)
 Raises HNP error interrupt. More...
 
#define Is_otg_hnp_error_interrupt()   (Tst_bits(UOTGHS->UOTGHS_SR, UOTGHS_SR_HNPERRI))
 Tests if a HNP error occurs. More...
 
#define otg_enable_role_exchange_interrupt()   (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_ROLEEXE))
 Enables role exchange interrupt. More...
 
#define otg_disable_role_exchange_interrupt()   (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_ROLEEXE))
 Disables role exchange interrupt. More...
 
#define Is_otg_role_exchange_interrupt_enabled()   (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_ROLEEXE))
 
#define otg_ack_role_exchange_interrupt()   (UOTGHS->UOTGHS_SCR = UOTGHS_SCR_ROLEEXIC)
 ACKs role exchange interrupt. More...
 
#define otg_raise_role_exchange_interrupt()   (UOTGHS->UOTGHS_SFR = UOTGHS_SFR_ROLEEXIS)
 Raises role exchange interrupt. More...
 
#define Is_otg_role_exchange_interrupt()   (Tst_bits(UOTGHS->UOTGHS_SR, UOTGHS_SR_ROLEEXI))
 Tests if a role exchange occurs. More...
 
#define otg_enable_srp_interrupt()   (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_SRPE))
 Enables SRP interrupt. More...
 
#define otg_disable_srp_interrupt()   (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_SRPE))
 Disables SRP interrupt. More...
 
#define Is_otg_srp_interrupt_enabled()   (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_SRPE))
 
#define otg_ack_srp_interrupt()   (UOTGHS->UOTGHS_SCR = UOTGHS_SCR_SRPIC)
 ACKs SRP interrupt. More...
 
#define otg_raise_srp_interrupt()   (UOTGHS->UOTGHS_SFR = UOTGHS_SFR_SRPIS)
 Raises SRP interrupt. More...
 
#define Is_otg_srp_interrupt()   (Tst_bits(UOTGHS->UOTGHS_SR, UOTGHS_SR_SRPI))
 Tests if a SRP occurs. More...
 

Functions

void otg_dual_disable (void)
 Uninitialize the dual role This function is implemented in uotghs_host.c file. More...
 
bool otg_dual_enable (void)
 Initialize the dual role This function is implemented in uotghs_host.c file. More...
 

#define Is_otg_a_suspend ( )    (4==otg_get_fsm_drd_state())

Referenced by ISR().

#define Is_otg_a_wait_vrise ( )    (1==otg_get_fsm_drd_state())
#define Is_otg_clock_frozen ( )    (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_FRZCLK))
#define Is_otg_clock_usable ( )    (Tst_bits(UOTGHS->UOTGHS_SR, UOTGHS_SR_CLKUSABLE))

Check Clock Usable For parts with HS feature, this one corresponding at UTMI clock.

Referenced by ISR(), uhd_disable(), uhd_enable(), uhd_interrupt(), and uhd_resume().

#define Is_otg_data_srp_method_selected ( )    (!Is_otg_vbus_srp_method_selected())
#define Is_otg_device_srp ( )    (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_SRPREQ))

Tests if a SRP from device occurs.

#define Is_otg_enabled ( )    (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_USBE))
#define Is_otg_hnp ( )    (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_HNPREQ))

Tests if a HNP occurs.

#define Is_otg_hnp_error_interrupt ( )    (Tst_bits(UOTGHS->UOTGHS_SR, UOTGHS_SR_HNPERRI))

Tests if a HNP error occurs.

#define Is_otg_hnp_error_interrupt_enabled ( )    (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_HNPERRE))
#define Is_otg_pad_enabled ( )    (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_OTGPADE))
#define Is_otg_role_exchange_interrupt ( )    (Tst_bits(UOTGHS->UOTGHS_SR, UOTGHS_SR_ROLEEXI))

Tests if a role exchange occurs.

#define Is_otg_role_exchange_interrupt_enabled ( )    (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_ROLEEXE))
#define Is_otg_srp_interrupt ( )    (Tst_bits(UOTGHS->UOTGHS_SR, UOTGHS_SR_SRPI))

Tests if a SRP occurs.

#define Is_otg_srp_interrupt_enabled ( )    (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_SRPE))
#define Is_otg_vbus_high ( )    (Tst_bits(UOTGHS->UOTGHS_SR, UOTGHS_SR_VBUS))

Referenced by uhd_enable(), and uhd_interrupt().

#define Is_otg_vbus_interrupt_enabled ( )    (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_VBUSTE))
#define Is_otg_vbus_low ( )    (!Is_otg_vbus_high())
#define Is_otg_vbus_srp_method_selected ( )    (Tst_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_SRPSEL))
#define Is_otg_vbus_transition ( )    (Tst_bits(UOTGHS->UOTGHS_SR, UOTGHS_SR_VBUSTI))

Referenced by uhd_interrupt().

#define otg_ack_hnp_error_interrupt ( )    (UOTGHS->UOTGHS_SCR = UOTGHS_SCR_HNPERRIC)

ACKs HNP error interrupt.

#define otg_ack_role_exchange_interrupt ( )    (UOTGHS->UOTGHS_SCR = UOTGHS_SCR_ROLEEXIC)

ACKs role exchange interrupt.

#define otg_ack_srp_interrupt ( )    (UOTGHS->UOTGHS_SCR = UOTGHS_SCR_SRPIC)

ACKs SRP interrupt.

#define otg_ack_vbus_transition ( )    (UOTGHS->UOTGHS_SCR = UOTGHS_SCR_VBUSTIC)

Referenced by uhd_enable(), and uhd_interrupt().

#define otg_configure_timeout (   timer,
  timeout 
)
Value:
(Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_UNLOCK),\
Wr_bitfield(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_TIMPAGE_Msk, timer),\
Wr_bitfield(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_TIMVALUE_Msk, timeout),\
Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_UNLOCK))
#define Clr_bits(lvalue, mask)
Clears the bits of a C lvalue specified by a given bit-mask.
Definition: compiler.h:512
#define Wr_bitfield(lvalue, mask, bitfield)
Writes the bit-field of a C lvalue specified by a given bit-mask.
Definition: compiler.h:549
#define Set_bits(lvalue, mask)
Sets the bits of a C lvalue specified by a given bit-mask.
Definition: compiler.h:521

Configure time-out of specified OTG timer.

#define otg_device_initiate_hnp ( )    (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_HNPREQ))

Initiates a Host negotiation Protocol.

#define otg_device_initiate_srp ( )    (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_SRPREQ))

initiates a Session Request Protocol

#define otg_disable ( )    (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_USBE))

Disable USB macro.

Referenced by otg_dual_disable(), and uhd_disable().

#define otg_disable_hnp_error_interrupt ( )    (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_HNPERRE))

Disables HNP error interrupt.

#define otg_disable_pad ( )    (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_OTGPADE))

Disable OTG pad.

Referenced by otg_dual_disable().

#define otg_disable_role_exchange_interrupt ( )    (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_ROLEEXE))

Disables role exchange interrupt.

#define otg_disable_srp_interrupt ( )    (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_SRPE))

Disables SRP interrupt.

#define otg_disable_vbus_interrupt ( )    (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_VBUSTE))
#define otg_enable ( )    (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_USBE))

Enable USB macro.

Referenced by otg_dual_enable(), and uhd_enable().

#define otg_enable_hnp_error_interrupt ( )    (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_HNPERRE))

Enables HNP error interrupt.

#define otg_enable_pad ( )    (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_OTGPADE))

Enable OTG pad.

Referenced by uhd_enable().

#define otg_enable_role_exchange_interrupt ( )    (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_ROLEEXE))

Enables role exchange interrupt.

#define otg_enable_srp_interrupt ( )    (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_SRPE))

Enables SRP interrupt.

#define otg_enable_vbus_interrupt ( )    (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_VBUSTE))
#define otg_freeze_clock ( )    (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_FRZCLK))
#define otg_get_fsm_drd_state ( )    (Rd_bitfield(UOTGHS->UOTGHS_FSM, UOTGHS_FSM_DRDSTATE_Msk))

Get the dual-role device state of the internal USB finite state machine of the UOTGHS controller.

#define otg_get_timeout (   timer)
Value:
(Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_UNLOCK),\
Wr_bitfield(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_TIMPAGE_Msk, timer),\
Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_UNLOCK),\
Rd_bitfield(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_TIMVALUE_Msk))
#define Clr_bits(lvalue, mask)
Clears the bits of a C lvalue specified by a given bit-mask.
Definition: compiler.h:512
#define Rd_bitfield(value, mask)
Reads the bit-field of a value specified by a given bit-mask.
Definition: compiler.h:539
#define Wr_bitfield(lvalue, mask, bitfield)
Writes the bit-field of a C lvalue specified by a given bit-mask.
Definition: compiler.h:549
#define Set_bits(lvalue, mask)
Sets the bits of a C lvalue specified by a given bit-mask.
Definition: compiler.h:521

Get configured time-out of specified OTG timer.

#define otg_host_accept_hnp ( )    (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_HNPREQ))

Accepts a Host negotiation Protocol.

#define otg_host_reject_hnp ( )    (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_HNPREQ))

Rejects a Host negotiation Protocol.

#define otg_raise_hnp_error_interrupt ( )    (UOTGHS->UOTGHS_SFR = UOTGHS_SFR_HNPERRIS)

Raises HNP error interrupt.

#define otg_raise_role_exchange_interrupt ( )    (UOTGHS->UOTGHS_SFR = UOTGHS_SFR_ROLEEXIS)

Raises role exchange interrupt.

#define otg_raise_srp_interrupt ( )    (UOTGHS->UOTGHS_SFR = UOTGHS_SFR_SRPIS)

Raises SRP interrupt.

#define otg_raise_vbus_transition ( )    (UOTGHS->UOTGHS_SFR = UOTGHS_SFR_VBUSTIS)

Referenced by uhd_enable().

#define otg_reset ( )
Value:
do { \
UOTGHS->UOTGHS_CTRL = 0; \
while( UOTGHS->UOTGHS_SR & 0x3FFF) {\
UOTGHS->UOTGHS_SCR = 0xFFFFFFFF;\
} \
} while (0)

Reset USB macro.

#define otg_select_data_srp_method ( )    (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_SRPSEL))

Selects data line as SRP method.

#define otg_select_vbus_srp_method ( )    (Set_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_SRPSEL))

Selects VBus as SRP method.

#define otg_unfreeze_clock ( )    (Clr_bits(UOTGHS->UOTGHS_CTRL, UOTGHS_CTRL_FRZCLK))