License | Subject to your compliance with these terms, you may use Microchip software and any derivatives exclusively with Microchip products |
Extra Information for Asynchronous Timer Driver | |
Examples for Asynchronous Timer Driver | This is a list of the available Quick Start Guides (QSGs) and example applications for SAM4L Asynchronous Timer (AST) Driver |
 Quick Start Guide for the AST driver | This is the quick start guide for the SAM4L Asynchronous Timer (AST) Driver, with step-by-step instructions on how to configure and use the driver for a specific use case.The code examples can be copied into the main application loop or any other function that will need to control the AST module |
 Asynchronous Timer (AST) - Example 1 Calendar Mode | |
 Asynchronous Timer (AST) - Example 2 Alarm Wakeup | |
Document Revision History | |
Quick Start Guide for the System Clock Management service (SAM4L) | This is the quick start guide for the System Clock Management service, with step-by-step instructions on how to configure and use the service for specific use cases |
Quickstart guide for SAM FLASHCALW driver | This is the quickstart guide for the SAM FLASHCALW driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick start guide for the SAM BPM module | This is the quick start guide for the BPM Module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Advanced use case - Switch Power Scaling Modes | In this use case, the BPM module can switch the power scaling modes of the system |
Quick start guide for USB host mouse module (UHI mouse) | This is the quick start guide for the USB host mouse module (UHI mouse) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 Enable USB high speed support | In this use case, the USB host is used to support USB high speed |
 Multiple classes support | In this use case, the USB host is used to support several USB classes |
 Dual roles support | In this use case, the USB host and USB device are enabled, it is the dual role |
conf_clock.h examples with USB support | Content of conf_clock.h for AT32UC3A0, AT32UC3A1, AT32UC3B devices (USBB): |
Quick start guide for the common IOPORT service | This is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases |
 Advanced use case doing port access | In this case we will read out the pins from one whole port and write the read value to another port |
Extra Information for GPIO | |
Examples for GPIO | This is a list of the available Quick Start guides (QSGs) and example applications for SAM4L General-Purpose Input/Output (GPIO) Driver |
Document Revision History | |
Quick Start Guide for the GPIO driver | This is the quick start guide for the group_sam_drivers_gpio, with step-by-step instructions on how to configure and use the driver for a specific use case |
Example | |
Extra Information for EIC | |
Quickstart guide for SAM EIC driver | This is the quickstart guide for the SAM4L External Interrupt Controller (EIC) Driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Document Revision History | |
Quick start guide for USB host mass-storage module (UHI MSC) | This is the quick start guide for the USB host mass-storage module (UHI MSC) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 Enable USB high speed support | In this use case, the USB host is used to support USB high speed |
 Multiple classes support | In this use case, the USB host is used to support several USB classes |
 Dual roles support | In this use case, the USB host and USB device are enabled, it is the dual role |
Quickstart guide for SAM4L watchdog driver | This is the quickstart guide for the SAM4L watchdog driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Todo List | |