Modules | |
In System Programming UC3 implementation | |
This implementation links the UC3 NVM functions to the common isp API. | |
Boot Process definition for UC3 parts | |
The behavior of the UC3 boot process for bootloader is defined by the fuses values and two Words in the user page. | |
Data Structures | |
struct | isp_mem_bootloader_t |
Memory bootloader structure. More... | |
struct | isp_mem_t |
Memory API definition. More... | |
union | isp_mems_t |
Memories list structure. More... | |
Typedefs | |
typedef uint32_t | isp_addr_t |
Data type for holding flash memory addresses. More... | |
Functions | |
COMPILER_PACK_SET (1) typedef union | |
Memory signature structure to store JTAG ID. More... | |
Variables | |
isp_mem_signature_t | |
const isp_mems_t | isp_memories |
Memories list declaration. More... | |
Main In System Programming functions | |
void | isp_init (void) |
Initializes the ISP interface. More... | |
bool | isp_is_security (void) |
Gives the security state of the chip. More... | |
void | isp_force_boot_isp (bool force) |
Change the boot process configuration to enable/disable the ISP mode for the next startup. More... | |
bool | isp_erase_chip (void) |
Erase the application flash area and eventually the eeprom. More... | |
bool | isp_erase_chip_split (void) |
Erase a part of the application flash area This function must be called again as long as it returns 0. More... | |
void | isp_start_appli (void) |
Resets the device to start the user application. More... | |
Memory units index values | |
Used to access at a memory through isp_memories list. | |
#define | ISP_MEM_FLASH 0x00 |
#define | ISP_MEM_EEPROM 0x01 |
#define | ISP_MEM_SECURITY 0x02 |
#define | ISP_MEM_CONFIGURATION 0x03 |
#define | ISP_MEM_BOOTLOADER 0x04 |
#define | ISP_MEM_SIGNATURE 0x05 |
#define | ISP_MEM_USER 0x06 |
#define | ISP_MEM_INT_RAM 0x07 |
#define | ISP_MEM_EXT_MEM_CS0 0x08 |
#define | ISP_MEM_EXT_MEM_CS1 0x09 |
#define | ISP_MEM_EXT_MEM_CS2 0x0A |
#define | ISP_MEM_EXT_MEM_CS3 0x0B |
#define | ISP_MEM_EXT_MEM_CS4 0x0C |
#define | ISP_MEM_EXT_MEM_CS5 0x0D |
#define | ISP_MEM_EXT_MEM_CS6 0x0E |
#define | ISP_MEM_EXT_MEM_CS7 0x0F |
#define | ISP_MEM_EXT_MEM_DF 0x10 |
#define | ISP_MEM_COUNT 0x11 |
#define ISP_MEM_BOOTLOADER 0x04 |
Referenced by udi_dfu_atmel_sel_mem().
#define ISP_MEM_CONFIGURATION 0x03 |
Referenced by udi_dfu_atmel_sel_mem().
#define ISP_MEM_COUNT 0x11 |
Referenced by udi_dfu_atmel_select_memory().
#define ISP_MEM_EEPROM 0x01 |
#define ISP_MEM_EXT_MEM_CS0 0x08 |
#define ISP_MEM_EXT_MEM_CS1 0x09 |
#define ISP_MEM_EXT_MEM_CS2 0x0A |
#define ISP_MEM_EXT_MEM_CS3 0x0B |
#define ISP_MEM_EXT_MEM_CS4 0x0C |
#define ISP_MEM_EXT_MEM_CS5 0x0D |
#define ISP_MEM_EXT_MEM_CS6 0x0E |
#define ISP_MEM_EXT_MEM_CS7 0x0F |
#define ISP_MEM_EXT_MEM_DF 0x10 |
#define ISP_MEM_FLASH 0x00 |
#define ISP_MEM_INT_RAM 0x07 |
#define ISP_MEM_SECURITY 0x02 |
Referenced by udi_dfu_atmel_sel_mem().
#define ISP_MEM_SIGNATURE 0x05 |
Referenced by udi_dfu_atmel_sel_mem().
#define ISP_MEM_USER 0x06 |
typedef uint32_t isp_addr_t |
Data type for holding flash memory addresses.
COMPILER_PACK_SET | ( | 1 | ) |
Memory signature structure to store JTAG ID.
bool isp_erase_chip | ( | void | ) |
Erase the application flash area and eventually the eeprom.
1
if function was successfully done, otherwise 0
. Referenced by udi_dfu_atmel_erase_chip().
bool isp_erase_chip_split | ( | void | ) |
Erase a part of the application flash area This function must be called again as long as it returns 0.
1
if the whole application flash area is erased, otherwise it is not finished.This function has been created to split a long erase so that the ISP application is able to answer external pending requests.
Referenced by udi_dfu_atmel_erase_chip().
void isp_force_boot_isp | ( | bool | force | ) |
Change the boot process configuration to enable/disable the ISP mode for the next startup.
force | Enable the ISP mode for the next startup if true |
References BOOT_CFG1, BOOT_CFG1_ADDRESS, BOOT_CFG1_CRC8_MASK, BOOT_CFG1_CRC8_OFFSET, BOOT_CFG1_FORCE_MASK, BOOT_CFG1_FORCE_OFFSET, and isp_crc8().
Referenced by udi_dfu_atmel_setup(), and udi_dfu_flip_msg_decode().
void isp_init | ( | void | ) |
Initializes the ISP interface.
Example, load the JTAG ID in signature memory
References Get_debug_register, mem_signature, and Rd_bitfield.
Referenced by udi_dfu_atmel_enable().
bool isp_is_security | ( | void | ) |
Gives the security state of the chip.
1
if chip is secured, otherwise 0
. References isp_mem_t::fnct_read.
Referenced by udi_dfu_atmel_enable().
void isp_start_appli | ( | void | ) |
Resets the device to start the user application.
The ISP mode must be disabled before (See isp_force_boot_isp(false)) to allow the boot process to jump to the user application.
References cpu_irq_disable, UC3C, UC3D, and UC3L3_L4.
Referenced by udi_dfu_atmel_setup().
isp_mem_signature_t |
const isp_mems_t isp_memories |
Memories list declaration.
Referenced by udi_dfu_atmel_sel_mem().