Microchip® Advanced Software Framework

ui.c File Reference

User Interface.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include "compiler.h"
#include "conf_usb.h"
#include "udc.h"
#include "udi_hid_generic.h"
#include "board.h"
#include "led.h"
#include "ui.h"
#include "conf_board.h"
#include "pio.h"
#include "sysclk.h"

Functions

void ui_init (void)
 Initializes the user interface. More...
 
void ui_led_change (uint8_t *report)
 This function is called when a HID report is received. More...
 
void ui_powerdown (void)
 Enters the user interface in power down mode. More...
 
void ui_process (uint16_t framenumber)
 This process is called each 1ms It is called only if the USB interface is enabled. More...
 
void ui_wakeup (void)
 Exits the user interface of power down mode. More...
 
void ui_wakeup_disable (void)
 Disables the asynchronous interrupts of the user interface. More...
 
void ui_wakeup_enable (void)
 Enables the asynchronous interrupts of the user interface. More...
 

Variables

static uint8_t ui_hid_report [UDI_HID_REPORT_OUT_SIZE]
 

void ui_init ( void  )

Initializes the user interface.

References LED0_GPIO, LED1_GPIO, LED2_GPIO, LED_Off(), LED_On(), and pmc_enable_periph_clk().

Referenced by main().

void ui_led_change ( uint8_t *  report)

This function is called when a HID report is received.

References LED1_GPIO, LED2_GPIO, LED_Off(), and LED_On().

void ui_powerdown ( void  )

Enters the user interface in power down mode.

References LED0_GPIO, LED1_GPIO, LED2_GPIO, and LED_Off().

Referenced by main(), main_hid_set_feature(), and main_suspend_action().

void ui_process ( uint16_t  framenumber)

This process is called each 1ms It is called only if the USB interface is enabled.

Parameters
framenumberCurrent frame number

References gpio_pin_is_high, GPIO_PUSH_BUTTON_1, GPIO_PUSH_BUTTON_2, LED0_GPIO, LED_Off(), LED_On(), udi_hid_generic_send_report_in(), and ui_hid_report.

Referenced by main(), and main_sof_action().

void ui_wakeup ( void  )

Exits the user interface of power down mode.

References LED0_GPIO, and LED_On().

Referenced by main_resume_action().

void ui_wakeup_disable ( void  )

Disables the asynchronous interrupts of the user interface.

Referenced by main_remotewakeup_disable().

void ui_wakeup_enable ( void  )

Enables the asynchronous interrupts of the user interface.

Referenced by main_remotewakeup_enable().

uint8_t ui_hid_report[UDI_HID_REPORT_OUT_SIZE]
static

Referenced by ui_process().