User Interface.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | ui_init (void) |
Initializes the user interface. More... | |
void | ui_led_change (uint8_t *report) |
This function is called when a HID report is received. More... | |
void | ui_powerdown (void) |
Enters the user interface in power down mode. More... | |
void | ui_process (uint16_t framenumber) |
This process is called each 1ms It is called only if the USB interface is enabled. More... | |
void | ui_wakeup (void) |
Exits the user interface of power down mode. More... | |
void | ui_wakeup_disable (void) |
Disables the asynchronous interrupts of the user interface. More... | |
void | ui_wakeup_enable (void) |
Enables the asynchronous interrupts of the user interface. More... | |
Variables | |
static uint8_t | ui_hid_report [UDI_HID_REPORT_OUT_SIZE] |
HID report buffer. More... | |
void ui_led_change | ( | uint8_t * | report | ) |
void ui_powerdown | ( | void | ) |
Enters the user interface in power down mode.
References LED_Off.
Referenced by main(), main_hid_set_feature(), and main_suspend_action().
void ui_process | ( | uint16_t | framenumber | ) |
This process is called each 1ms It is called only if the USB interface is enabled.
framenumber | Current frame number |
References GPIO_PUSH_BUTTON_1, GPIO_PUSH_BUTTON_2, ioport_get_pin_level(), LED_Off, LED_On, udi_hid_generic_send_report_in(), and ui_hid_report.
Referenced by main(), and main_sof_action().
void ui_wakeup | ( | void | ) |
void ui_wakeup_disable | ( | void | ) |
Disables the asynchronous interrupts of the user interface.
Referenced by main_remotewakeup_disable().
void ui_wakeup_enable | ( | void | ) |
Enables the asynchronous interrupts of the user interface.
Referenced by main_remotewakeup_enable().
|
static |
HID report buffer.
Referenced by ui_process().