Microchip® Advanced Software Framework

ui.c File Reference

User Interface.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include <asf.h>
#include "ui.h"

Functions

void ui_init (void)
 Initializes the user interface. More...
 
void ui_led_change (uint8_t *report)
 This function is called when a HID report is received. More...
 
void ui_powerdown (void)
 Enters the user interface in power down mode. More...
 
void ui_process (uint16_t framenumber)
 This process is called each 1ms It is called only if the USB interface is enabled. More...
 
void ui_wakeup (void)
 Exits the user interface of power down mode. More...
 
void ui_wakeup_disable (void)
 Disables the asynchronous interrupts of the user interface. More...
 
void ui_wakeup_enable (void)
 Enables the asynchronous interrupts of the user interface. More...
 

Variables

static bool ui_b_led_blink = true
 
static uint8_t ui_hid_report [UDI_HID_REPORT_OUT_SIZE]
 

void ui_init ( void  )

Initializes the user interface.

References LED_Off.

Referenced by main().

void ui_led_change ( uint8_t *  report)

This function is called when a HID report is received.

References LED_On, and ui_b_led_blink.

void ui_powerdown ( void  )

Enters the user interface in power down mode.

References LED_Off.

Referenced by main(), main_hid_set_feature(), and main_suspend_action().

void ui_process ( uint16_t  framenumber)

This process is called each 1ms It is called only if the USB interface is enabled.

Parameters
framenumberCurrent frame number

References GPIO_PUSH_BUTTON_1, ioport_get_pin_level(), LED_Off, LED_On, udi_hid_generic_send_report_in(), ui_b_led_blink, and ui_hid_report.

Referenced by main(), and main_sof_action().

void ui_wakeup ( void  )

Exits the user interface of power down mode.

References LED_On.

Referenced by main_resume_action().

void ui_wakeup_disable ( void  )

Disables the asynchronous interrupts of the user interface.

Referenced by main_remotewakeup_disable().

void ui_wakeup_enable ( void  )

Enables the asynchronous interrupts of the user interface.

Referenced by main_remotewakeup_enable().

bool ui_b_led_blink = true
static

Referenced by ui_led_change(), and ui_process().

uint8_t ui_hid_report[UDI_HID_REPORT_OUT_SIZE]
static

Referenced by ui_process().