Common User Interface for HID Mouse application.
Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | ui_init (void) |
Initializes the user interface. More... | |
void | ui_led_change (uint8_t *report) |
This function is called when a HID report is received. More... | |
void | ui_powerdown (void) |
Enters the user interface in power down mode. More... | |
void | ui_process (uint16_t framenumber) |
This process is called each 1ms It is called only if the USB interface is enabled. More... | |
void | ui_wakeup (void) |
Exits the user interface of power down mode. More... | |
void | ui_wakeup_disable (void) |
Disables the asynchronous interrupts of the user interface. More... | |
void | ui_wakeup_enable (void) |
Enables the asynchronous interrupts of the user interface. More... | |
void ui_init | ( | void | ) |
Initializes the user interface.
References cpu_irq_restore(), cpu_irq_save(), GPIO_PUSH_BUTTON_1, irq_register_handler, LED0, LED1, LED2, LED3, LED_Off(), and LED_On().
Referenced by main().
void ui_led_change | ( | uint8_t * | report | ) |
void ui_powerdown | ( | void | ) |
Enters the user interface in power down mode.
References LED0, LED1, LED2, LED3, and LED_Off().
Referenced by main(), main_hid_set_feature(), and main_suspend_action().
void ui_process | ( | uint16_t | framenumber | ) |
This process is called each 1ms It is called only if the USB interface is enabled.
framenumber | Current frame number |
References gpio_get_pin_value(), GPIO_PUSH_BUTTON_0, GPIO_PUSH_BUTTON_1, LED1, LED_Off(), LED_On(), udi_hid_generic_send_report_in(), and ui_hid_report.
Referenced by main(), and main_sof_action().
void ui_wakeup | ( | void | ) |
Exits the user interface of power down mode.
References LED0, and LED_On().
Referenced by main_resume_action().
void ui_wakeup_disable | ( | void | ) |
Disables the asynchronous interrupts of the user interface.
References eic_disable_line(), EXT_NMI, gpio_disable_pin_interrupt(), and GPIO_PUSH_BUTTON_1.
Referenced by main_remotewakeup_disable().
void ui_wakeup_enable | ( | void | ) |
Enables the asynchronous interrupts of the user interface.
References eic_enable_line(), eic_init(), EXT_NMI, gpio_enable_module_pin(), gpio_enable_pin_interrupt(), gpio_enable_pin_pull_up(), GPIO_PIN_CHANGE, and GPIO_PUSH_BUTTON_1.
Referenced by main_remotewakeup_enable().