User Interface.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | SEQUENCE_PERIOD 150 |
Sequence process running each SEQUENCE_PERIOD ms. More... | |
#define | WAKEUP_PIN (GPIO_PUSH_BUTTON_2) |
#define | WAKEUP_PIO (PIN_PUSHBUTTON_2_PIO) |
#define | WAKEUP_PIO_ATTR (PIO_INPUT | PIO_PULLUP | PIO_DEBOUNCE | PIO_IT_LOW_LEVEL) |
#define | WAKEUP_PIO_ID (PIN_PUSHBUTTON_2_ID) |
#define | WAKEUP_PIO_MASK (PIN_PUSHBUTTON_2_MASK) |
#define | WAKEUP_PMC_FSTT (PUSHBUTTON_2_WKUP_FSTT) |
Functions | |
void | ui_init (void) |
Initializes the user interface. More... | |
void | ui_kbd_led (uint8_t value) |
Turn on or off the keyboard LEDs. More... | |
void | ui_powerdown (void) |
Enters the user interface in power down mode. More... | |
void | ui_process (uint16_t framenumber) |
This process is called each 1ms It is called only if the USB interface is enabled. More... | |
void | ui_wakeup (void) |
Exits the user interface of power down mode. More... | |
void | ui_wakeup_disable (void) |
Disables the asynchronous interrupts of the user interface. More... | |
void | ui_wakeup_enable (void) |
Enables the asynchronous interrupts of the user interface. More... | |
static void | ui_wakeup_handler (uint32_t id, uint32_t mask) |
Variables | |
static bool | btn_wakeup = false |
Wakeup, ignore button change until button is back to default state. More... | |
struct { | |
bool b_down | |
bool b_modifier | |
uint8_t value | |
} | ui_sequence [] |
#define SEQUENCE_PERIOD 150 |
Sequence process running each SEQUENCE_PERIOD
ms.
Referenced by ui_process().
#define WAKEUP_PIN (GPIO_PUSH_BUTTON_2) |
Referenced by ui_wakeup_disable(), and ui_wakeup_enable().
#define WAKEUP_PIO (PIN_PUSHBUTTON_2_PIO) |
Referenced by ui_init().
#define WAKEUP_PIO_ATTR (PIO_INPUT | PIO_PULLUP | PIO_DEBOUNCE | PIO_IT_LOW_LEVEL) |
Referenced by ui_init(), and ui_wakeup_enable().
#define WAKEUP_PIO_ID (PIN_PUSHBUTTON_2_ID) |
Referenced by ui_init(), and ui_wakeup_handler().
#define WAKEUP_PIO_MASK (PIN_PUSHBUTTON_2_MASK) |
Referenced by ui_init(), and ui_wakeup_handler().
#define WAKEUP_PMC_FSTT (PUSHBUTTON_2_WKUP_FSTT) |
Referenced by ui_wakeup_disable(), and ui_wakeup_enable().
void ui_init | ( | void | ) |
Initializes the user interface.
References LED_Off, pio_handler_set(), ui_wakeup_handler(), WAKEUP_PIO, WAKEUP_PIO_ATTR, WAKEUP_PIO_ID, and WAKEUP_PIO_MASK.
Referenced by main().
void ui_kbd_led | ( | uint8_t | value | ) |
Turn on or off the keyboard LEDs.
References HID_LED_CAPS_LOCK, LED_Off, and LED_On.
void ui_powerdown | ( | void | ) |
Enters the user interface in power down mode.
References LED_Off.
Referenced by main(), and main_suspend_action().
void ui_process | ( | uint16_t | framenumber | ) |
This process is called each 1ms It is called only if the USB interface is enabled.
framenumber | Current frame number |
References b_down, b_modifier, btn_wakeup, GPIO_PUSH_BUTTON_2, ioport_get_pin_level(), LED_Off, LED_On, SEQUENCE_PERIOD, udi_hid_kbd_down(), udi_hid_kbd_modifier_down(), udi_hid_kbd_modifier_up(), udi_hid_kbd_up(), ui_sequence, and value.
Referenced by main(), and main_sof_action().
void ui_wakeup | ( | void | ) |
void ui_wakeup_disable | ( | void | ) |
Disables the asynchronous interrupts of the user interface.
References pio_disable_pin_interrupt(), pmc_clr_fast_startup_input(), WAKEUP_PIN, and WAKEUP_PMC_FSTT.
Referenced by main_remotewakeup_disable().
void ui_wakeup_enable | ( | void | ) |
Enables the asynchronous interrupts of the user interface.
References pio_configure_pin(), pio_enable_pin_interrupt(), pmc_set_fast_startup_input(), WAKEUP_PIN, WAKEUP_PIO_ATTR, and WAKEUP_PMC_FSTT.
Referenced by main_remotewakeup_enable().
|
static |
References btn_wakeup, LED_On, udc_remotewakeup(), WAKEUP_PIO_ID, and WAKEUP_PIO_MASK.
Referenced by ui_init().
bool b_down |
Referenced by ui_process().
bool b_modifier |
Referenced by ui_process().
Wakeup, ignore button change until button is back to default state.
Referenced by ui_process(), and ui_wakeup_handler().
struct { ... } ui_sequence[] |
Referenced by ui_process().
uint8_t value |
Referenced by ui_process().