See Quickstart guide for SAM FLASHCALW driver.
FLASHCALW interfaces a flash block with the 32-bit internal HSB bus.
Flash Properties | |
uint32_t | flashcalw_get_flash_size (void) |
Gets the size of the whole flash array. More... | |
uint32_t | flashcalw_get_page_count (void) |
Gets the total number of pages in the flash array. More... | |
uint32_t | flashcalw_get_page_count_per_region (void) |
Gets the number of pages in each flash region. More... | |
uint32_t | flashcalw_get_page_region (int32_t page_number) |
Gets the region number of a page. More... | |
uint32_t | flashcalw_get_region_first_page_number (uint32_t region) |
Gets the number of the first page of a region. More... | |
FLASHC Control | |
uint32_t | flashcalw_get_wait_state (void) |
Gets the number of wait states of flash read accesses. More... | |
void | flashcalw_set_wait_state (uint32_t wait_state) |
Sets the number of wait states of flash read accesses. More... | |
void | flashcalw_set_flash_waitstate_and_readmode (uint32_t cpu_f_hz, uint32_t ps_value, bool is_fwu_enabled) |
Depending on the CPU frequency, on the Power Scaling mode and on the Fast Wakeup mode, set the wait states of flash read accesses and enable or disable the High speed read mode. More... | |
bool | flashcalw_is_ready_int_enabled (void) |
Tells whether the Flash Ready interrupt is enabled. More... | |
void | flashcalw_enable_ready_int (bool enable) |
Enables or disables the Flash Ready interrupt. More... | |
bool | flashcalw_is_lock_error_int_enabled (void) |
Tells whether the Lock Error interrupt is enabled. More... | |
void | flashcalw_enable_lock_error_int (bool enable) |
Enables or disables the Lock Error interrupt. More... | |
bool | flashcalw_is_prog_error_int_enabled (void) |
Tells whether the Programming Error interrupt is enabled. More... | |
void | flashcalw_enable_prog_error_int (bool enable) |
Enables or disables the Programming Error interrupt. More... | |
#define | FLASH_FWS_0_MAX_FREQ CHIP_FREQ_FWS_0 |
#define | FLASH_FWS_1_MAX_FREQ CHIP_FREQ_FWS_1 |
#define | FLASH_HSEN_FWS_0_MAX_FREQ CHIP_FREQ_FLASH_HSEN_FWS_0 |
#define | FLASH_HSEN_FWS_1_MAX_FREQ CHIP_FREQ_FLASH_HSEN_FWS_1 |
FLASHCALW Status | |
void(*volatile | flashcalw_wait_until_ready )(void) = flashcalw_default_wait_until_ready |
Pointer to the function used by the driver when it needs to wait until the FLASHCALW is ready to run a new command. More... | |
static uint32_t | flashcalw_error_status = 0 |
Sticky error status of the FLASHCALW. More... | |
bool | flashcalw_is_ready (void) |
Tells whether the FLASHCALW is ready to run a new command. More... | |
void | flashcalw_default_wait_until_ready (void) |
Waits actively until the FLASHCALW is ready to run a new command. More... | |
static uint32_t | flashcalw_get_error_status (void) |
Gets the error status of the FLASHCALW. More... | |
bool | flashcalw_is_lock_error (void) |
Tells whether a Lock Error has occurred during the last function called that issued one or more FLASHCALW commands. More... | |
bool | flashcalw_is_programming_error (void) |
Tells whether a Programming Error has occurred during the last function called that issued one or more FLASHCALW commands. More... | |
FLASHCALW Command Control | |
uint32_t | flashcalw_get_command (void) |
Gets the last issued FLASHCALW command. More... | |
uint32_t | flashcalw_get_page_number (void) |
Gets the current FLASHCALW page number. More... | |
void | flashcalw_issue_command (uint32_t command, int page_number) |
Issues a FLASHCALW command. More... | |
FLASHCALW Global Commands | |
void | flashcalw_no_operation (void) |
Issues a No Operation command to the FLASHCALW. More... | |
void | flashcalw_erase_all (void) |
Issues an Erase All command to the FLASHCALW. More... | |
FLASHCALW Protection Mechanisms | |
bool | flashcalw_is_security_bit_active (void) |
Tells whether the Security bit is active. More... | |
void | flashcalw_set_security_bit (void) |
Activates the Security bit. More... | |
bool | flashcalw_is_page_region_locked (uint32_t page_number) |
Tells whether the region of a page is locked. More... | |
bool | flashcalw_is_region_locked (uint32_t region) |
Tells whether a region is locked. More... | |
void | flashcalw_lock_page_region (int page_number, bool lock) |
Locks or unlocks the region of a page. More... | |
void | flashcalw_lock_region (uint32_t region, bool lock) |
Locks or unlocks a region. More... | |
void | flashcalw_lock_all_regions (bool lock) |
Locks or unlocks all regions. More... | |
Access to General-Purpose Fuses | |
bool | flashcalw_read_gp_fuse_bit (uint32_t gp_fuse_bit) |
Reads a general-purpose fuse bit. More... | |
uint64_t | flashcalw_read_gp_fuse_bitfield (uint32_t pos, uint32_t width) |
Reads a general-purpose fuse bit-field. More... | |
uint8_t | flashcalw_read_gp_fuse_byte (uint32_t gp_fuse_byte) |
Reads a general-purpose fuse byte. More... | |
uint64_t | flashcalw_read_all_gp_fuses (void) |
Reads all general-purpose fuses. More... | |
bool | flashcalw_erase_gp_fuse_bit (uint32_t gp_fuse_bit, bool check) |
Erases a general-purpose fuse bit. More... | |
bool | flashcalw_erase_gp_fuse_bitfield (uint32_t pos, uint32_t width, bool check) |
Erases a general-purpose fuse bit-field. More... | |
bool | flashcalw_erase_gp_fuse_byte (uint32_t gp_fuse_byte, bool check) |
Erases a general-purpose fuse byte. More... | |
bool | flashcalw_erase_all_gp_fuses (bool check) |
Erases all general-purpose fuses. More... | |
void | flashcalw_write_gp_fuse_bit (uint32_t gp_fuse_bit, bool value) |
Writes a general-purpose fuse bit. More... | |
void | flashcalw_write_gp_fuse_bitfield (uint32_t pos, uint32_t width, uint64_t value) |
Writes a general-purpose fuse bit-field. More... | |
void | flashcalw_write_gp_fuse_byte (uint32_t gp_fuse_byte, uint8_t value) |
Writes a general-purpose fuse byte. More... | |
void | flashcalw_write_all_gp_fuses (uint64_t value) |
Writes all general-purpose fuses. More... | |
void | flashcalw_set_gp_fuse_bit (uint32_t gp_fuse_bit, bool value) |
Sets a general-purpose fuse bit with the appropriate erase and write operations. More... | |
void | flashcalw_set_gp_fuse_bitfield (uint32_t pos, uint32_t width, uint64_t value) |
Sets a general-purpose fuse bit-field with the appropriate erase and write operations. More... | |
void | flashcalw_set_gp_fuse_byte (uint32_t gp_fuse_byte, uint8_t value) |
Sets a general-purpose fuse byte with the appropriate erase and write operations. More... | |
void | flashcalw_set_all_gp_fuses (uint64_t value) |
Sets all general-purpose fuses with the appropriate erase and write operations. More... | |
Access to Flash Pages | |
void | flashcalw_clear_page_buffer (void) |
Clears the page buffer. More... | |
bool | flashcalw_is_page_erased (void) |
Tells whether the page to which the last Quick Page Read or Quick Page Read User Page command was applied was erased. More... | |
bool | flashcalw_quick_page_read (int page_number) |
Applies the Quick Page Read command to a page. More... | |
bool | flashcalw_erase_page (int page_number, bool check) |
Erases a page. More... | |
bool | flashcalw_erase_all_pages (bool check) |
Erases all pages within the flash array. More... | |
void | flashcalw_write_page (int page_number) |
Writes a page from the page buffer. More... | |
bool | flashcalw_quick_user_page_read (void) |
Issues a Quick Page Read User Page command to the FLASHCALW. More... | |
bool | flashcalw_erase_user_page (bool check) |
Erases the User page. More... | |
void | flashcalw_write_user_page (void) |
Writes the User page from the page buffer. More... | |
volatile void * | flashcalw_memset8 (volatile void *dst, uint8_t src, size_t nbytes, bool erase) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src source byte. More... | |
volatile void * | flashcalw_memset16 (volatile void *dst, uint16_t src, size_t nbytes, bool erase) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source half-word. More... | |
volatile void * | flashcalw_memset32 (volatile void *dst, uint32_t src, size_t nbytes, bool erase) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source word. More... | |
volatile void * | flashcalw_memset64 (volatile void *dst, uint64_t src, size_t nbytes, bool erase) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source double-word. More... | |
volatile void * | flashcalw_memcpy (volatile void *dst, const void *src, size_t nbytes, bool erase) |
Copies nbytes bytes to the flash destination pointed to by dst from the source pointed to by src. More... | |
PicoCache interfaces | |
void | flashcalw_picocache_enable (void) |
Enable PicoCache. More... | |
void | flashcalw_picocache_disable (void) |
Disable PicoCache. More... | |
uint32_t | flashcalw_picocache_get_status (void) |
Get PicoCache status. More... | |
void | flashcalw_picocache_invalid_all (void) |
Invalid all PicoCache lines. More... | |
void | flashcalw_picocache_invalid_line (uint32_t index) |
Invalid specific cache line. More... | |
void | flashcalw_picocache_set_monitor_mode (uint32_t mode) |
Set PicoCache monitor mode. More... | |
void | flashcalw_picocache_enable_monitor (void) |
Enable PicoCache monitor. More... | |
void | flashcalw_picocache_disable_monitor (void) |
Disable PicoCache monitor. More... | |
void | flashcalw_picocache_reset_monitor (void) |
Reset PicoCache monitor. More... | |
uint32_t | flashcalw_picocache_get_monitor_cnt (void) |
Get PicoCache monitor count number. More... | |
uint32_t | flashcalw_picocache_get_version (void) |
Get PicoCache version. More... | |
#define FLASH_FWS_0_MAX_FREQ CHIP_FREQ_FWS_0 |
#define FLASH_FWS_1_MAX_FREQ CHIP_FREQ_FWS_1 |
#define FLASH_HSEN_FWS_0_MAX_FREQ CHIP_FREQ_FLASH_HSEN_FWS_0 |
#define FLASH_HSEN_FWS_1_MAX_FREQ CHIP_FREQ_FLASH_HSEN_FWS_1 |
void flashcalw_clear_page_buffer | ( | void | ) |
Clears the page buffer.
This command resets all bits in the page buffer to one. Write accesses to the page buffer can only change page buffer bits from one to zero.
References flashcalw_issue_command().
Referenced by flashcalw_memcpy(), and flashcalw_memset64().
void flashcalw_default_wait_until_ready | ( | void | ) |
Waits actively until the FLASHCALW is ready to run a new command.
This is the default function assigned to flashcalw_wait_until_ready.
References flashcalw_is_ready().
void flashcalw_enable_lock_error_int | ( | bool | enable | ) |
Enables or disables the Lock Error interrupt.
enable | Whether to enable the Lock Error interrupt: true or false . |
void flashcalw_enable_prog_error_int | ( | bool | enable | ) |
Enables or disables the Programming Error interrupt.
enable | Whether to enable the Programming Error interrupt: true or false . |
void flashcalw_enable_ready_int | ( | bool | enable | ) |
Enables or disables the Flash Ready interrupt.
enable | Whether to enable the Flash Ready interrupt: true or false . |
void flashcalw_erase_all | ( | void | ) |
Issues an Erase All command to the FLASHCALW.
This command erases all bits in the flash array, the general-purpose fuse bits and the Security bit. The User page is not erased.
This command also ensures that all volatile memories, such as register file and RAMs, are erased before the Security bit is erased, i.e. deactivated.
References flashcalw_issue_command().
Erases all general-purpose fuses.
check | Whether to check erase: true or false . |
true
if erase check was not requested.FLASH_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. use (uint64_t)-1 instead of 0xFFFFFFFFFFFFFFFFULL to avoid compilation warning
References flashcalw_issue_command(), and flashcalw_read_all_gp_fuses().
Referenced by flashcalw_erase_gp_fuse_byte(), and flashcalw_set_all_gp_fuses().
Erases all pages within the flash array.
check | Whether to check erase: true or false . |
true
if erase check was not requested.References flashcalw_erase_page(), flashcalw_error_status, and flashcalw_get_page_count().
Erases a general-purpose fuse bit.
gp_fuse_bit | The general-purpose fuse bit: 0 to 63 . |
check | Whether to check erase: true or false . |
true
if erase check was not requested.FLASH_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcalw_issue_command(), and flashcalw_read_gp_fuse_bit().
Referenced by flashcalw_erase_gp_fuse_bitfield(), and flashcalw_set_gp_fuse_bit().
Erases a general-purpose fuse bit-field.
pos | The bit-position of the general-purpose fuse bit-field: 0 to 63 . |
width | The bit-width of the general-purpose fuse bit-field: 0 to 64 . |
check | Whether to check erase: true or false . |
true
if erase check was not requested.FLASH_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcalw_erase_gp_fuse_bit(), flashcalw_error_status, flashcalw_read_gp_fuse_bitfield(), and Min.
Erases a general-purpose fuse byte.
gp_fuse_byte | The general-purpose fuse byte: 0 to 7 . |
check | Whether to check erase: true or false . |
true
if erase check was not requested.FLASH_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcalw_erase_all_gp_fuses(), flashcalw_error_status, flashcalw_read_all_gp_fuses(), flashcalw_read_gp_fuse_byte(), flashcalw_write_gp_fuse_byte(), and value.
Referenced by flashcalw_set_gp_fuse_byte().
Erases a page.
page_number | The page number:
|
check | Whether to check erase: true or false . |
true
if erase check was not requested.References flashcalw_error_status, flashcalw_issue_command(), and flashcalw_quick_page_read().
Referenced by flashcalw_erase_all_pages(), flashcalw_memcpy(), and flashcalw_memset64().
Erases the User page.
check | Whether to check erase: true or false . |
true
if erase check was not requested.References flashcalw_issue_command(), and flashcalw_quick_user_page_read().
Referenced by flashcalw_memcpy(), and flashcalw_memset64().
uint32_t flashcalw_get_command | ( | void | ) |
Gets the last issued FLASHCALW command.
|
static |
Gets the error status of the FLASHCALW.
FLASHCALW_FSR_LOCKE
and FLASHCALW_FSR_PROGE
.Referenced by flashcalw_issue_command().
uint32_t flashcalw_get_flash_size | ( | void | ) |
Gets the size of the whole flash array.
Referenced by flashcalw_get_page_count(), flashcalw_memcpy(), and flashcalw_memset64().
uint32_t flashcalw_get_page_count | ( | void | ) |
Gets the total number of pages in the flash array.
References FLASH_PAGE_SIZE, and flashcalw_get_flash_size().
Referenced by flashcalw_erase_all_pages(), and flashcalw_get_page_count_per_region().
uint32_t flashcalw_get_page_count_per_region | ( | void | ) |
Gets the number of pages in each flash region.
References FLASH_NB_OF_REGIONS, and flashcalw_get_page_count().
Referenced by flashcalw_get_page_region(), and flashcalw_get_region_first_page_number().
uint32_t flashcalw_get_page_number | ( | void | ) |
Gets the current FLASHCALW page number.
Referenced by flashcalw_get_page_region().
uint32_t flashcalw_get_page_region | ( | int32_t | page_number | ) |
Gets the region number of a page.
page_number | The page number:
|
References flashcalw_get_page_count_per_region(), and flashcalw_get_page_number().
Referenced by flashcalw_is_page_region_locked().
uint32_t flashcalw_get_region_first_page_number | ( | uint32_t | region | ) |
Gets the number of the first page of a region.
region | The region number: 0 to (FLASHCALW_REGIONS - 1) . |
References flashcalw_get_page_count_per_region().
Referenced by flashcalw_lock_region().
uint32_t flashcalw_get_wait_state | ( | void | ) |
Gets the number of wait states of flash read accesses.
bool flashcalw_is_lock_error | ( | void | ) |
Tells whether a Lock Error has occurred during the last function called that issued one or more FLASHCALW commands.
bool flashcalw_is_lock_error_int_enabled | ( | void | ) |
Tells whether the Lock Error interrupt is enabled.
bool flashcalw_is_page_erased | ( | void | ) |
Tells whether the page to which the last Quick Page Read or Quick Page Read User Page command was applied was erased.
Referenced by flashcalw_quick_page_read(), and flashcalw_quick_user_page_read().
bool flashcalw_is_page_region_locked | ( | uint32_t | page_number | ) |
Tells whether the region of a page is locked.
page_number | The page number:
|
References flashcalw_get_page_region(), and flashcalw_is_region_locked().
bool flashcalw_is_prog_error_int_enabled | ( | void | ) |
Tells whether the Programming Error interrupt is enabled.
bool flashcalw_is_programming_error | ( | void | ) |
Tells whether a Programming Error has occurred during the last function called that issued one or more FLASHCALW commands.
bool flashcalw_is_ready | ( | void | ) |
Tells whether the FLASHCALW is ready to run a new command.
Referenced by flashcalw_default_wait_until_ready().
bool flashcalw_is_ready_int_enabled | ( | void | ) |
Tells whether the Flash Ready interrupt is enabled.
bool flashcalw_is_region_locked | ( | uint32_t | region | ) |
Tells whether a region is locked.
region | The region number: 0 to (FLASHCALW_REGIONS - 1) . |
References FLASHCALW_REGIONS.
Referenced by flashcalw_is_page_region_locked().
bool flashcalw_is_security_bit_active | ( | void | ) |
Tells whether the Security bit is active.
void flashcalw_issue_command | ( | uint32_t | command, |
int | page_number | ||
) |
Issues a FLASHCALW command.
command | The command: FLASHCALW_FCMD_CMD_x . |
page_number | The page number to apply the command to:
|
References flashcalw_get_error_status(), and flashcalw_wait_until_ready.
Referenced by flashcalw_clear_page_buffer(), flashcalw_erase_all(), flashcalw_erase_all_gp_fuses(), flashcalw_erase_gp_fuse_bit(), flashcalw_erase_page(), flashcalw_erase_user_page(), flashcalw_lock_page_region(), flashcalw_no_operation(), flashcalw_quick_page_read(), flashcalw_quick_user_page_read(), flashcalw_set_flash_waitstate_and_readmode(), flashcalw_set_security_bit(), flashcalw_write_gp_fuse_bit(), flashcalw_write_gp_fuse_byte(), flashcalw_write_page(), and flashcalw_write_user_page().
void flashcalw_lock_all_regions | ( | bool | lock | ) |
Locks or unlocks all regions.
lock | Whether to lock the regions: true or false . |
References flashcalw_error_status, flashcalw_lock_region(), and FLASHCALW_REGIONS.
void flashcalw_lock_page_region | ( | int | page_number, |
bool | lock | ||
) |
Locks or unlocks the region of a page.
page_number | The page number:
|
lock | Whether to lock the region of the specified page: true or false . |
References flashcalw_issue_command().
Referenced by flashcalw_lock_region().
void flashcalw_lock_region | ( | uint32_t | region, |
bool | lock | ||
) |
Locks or unlocks a region.
region | The region number: 0 to (FLASHCALW_REGIONS - 1) . |
lock | Whether to lock the specified region: true or false . |
References flashcalw_get_region_first_page_number(), and flashcalw_lock_page_region().
Referenced by flashcalw_lock_all_regions().
volatile void* flashcalw_memcpy | ( | volatile void * | dst, |
const void * | src, | ||
size_t | nbytes, | ||
bool | erase | ||
) |
Copies nbytes bytes to the flash destination pointed to by dst from the source pointed to by src.
The destination areas that are not within the flash array or the User page are caught by an Assert() operation.
All pointer and size alignments are supported.
dst | Pointer to flash destination. |
src | Pointer to source data. |
nbytes | Number of bytes to copy. |
erase | Whether to erase before writing: true or false . |
false
only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001
then 0xFFFFFFFE
are written to a word, the resulting value in flash may be different from 0x00000000
.References Assert, FLASH_PAGE_SIZE, flashcalw_clear_page_buffer(), flashcalw_erase_page(), flashcalw_erase_user_page(), flashcalw_error_status, flashcalw_get_flash_size(), flashcalw_write_page(), flashcalw_write_user_page(), Union64::u64, and Union64::u8.
volatile void* flashcalw_memset16 | ( | volatile void * | dst, |
uint16_t | src, | ||
size_t | nbytes, | ||
bool | erase | ||
) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source half-word.
All pointer and size alignments are supported.
dst | Pointer to flash destination. |
src | Source half-word. |
nbytes | Number of bytes to set. |
erase | Whether to erase before writing: true or false . |
false
only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001
then 0xFFFFFFFE
are written to a word, the resulting value in flash may be different from 0x00000000
.References flashcalw_memset32().
Referenced by flashcalw_memset8().
volatile void* flashcalw_memset32 | ( | volatile void * | dst, |
uint32_t | src, | ||
size_t | nbytes, | ||
bool | erase | ||
) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source word.
All pointer and size alignments are supported.
dst | Pointer to flash destination. |
src | Source word. |
nbytes | Number of bytes to set. |
erase | Whether to erase before writing: true or false . |
false
only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001
then 0xFFFFFFFE
are written to a word, the resulting value in flash may be different from 0x00000000
.References flashcalw_memset64().
Referenced by flashcalw_memset16().
volatile void* flashcalw_memset64 | ( | volatile void * | dst, |
uint64_t | src, | ||
size_t | nbytes, | ||
bool | erase | ||
) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source double-word.
All pointer and size alignments are supported.
dst | Pointer to flash destination. |
src | Source double-word. |
nbytes | Number of bytes to set. |
erase | Whether to erase before writing: true or false . |
false
only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001
then 0xFFFFFFFE
are written to a word, the resulting value in flash may be different from 0x00000000
.References Align_down, FLASH_PAGE_SIZE, flashcalw_clear_page_buffer(), flashcalw_erase_page(), flashcalw_erase_user_page(), flashcalw_error_status, flashcalw_get_flash_size(), flashcalw_write_page(), flashcalw_write_user_page(), Get_align, Min, Test_align, StructCVPtr::u16ptr, UnionVPtr::u32ptr, StructCVPtr::u32ptr, Union64::u64, UnionVPtr::u64ptr, UnionCVPtr::u64ptr, StructCVPtr::u64ptr, Union64::u8, UnionVPtr::u8ptr, UnionCVPtr::u8ptr, and StructCVPtr::u8ptr.
Referenced by flashcalw_memset32().
volatile void* flashcalw_memset8 | ( | volatile void * | dst, |
uint8_t | src, | ||
size_t | nbytes, | ||
bool | erase | ||
) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src source byte.
All pointer and size alignments are supported.
dst | Pointer to flash destination. |
src | Source byte. |
nbytes | Number of bytes to set. |
erase | Whether to erase before writing: true or false . |
false
only if the destination consists only of erased words, i.e. this function cannot be used to write only one bit of a previously written word. E.g., if 0x00000001
then 0xFFFFFFFE
are written to a word, the resulting value in flash may be different from 0x00000000
.References flashcalw_memset16().
void flashcalw_no_operation | ( | void | ) |
Issues a No Operation command to the FLASHCALW.
References flashcalw_issue_command().
void flashcalw_picocache_disable | ( | void | ) |
Disable PicoCache.
References flashcalw_picocache_get_status(), and sysclk_disable_peripheral_clock().
void flashcalw_picocache_disable_monitor | ( | void | ) |
Disable PicoCache monitor.
void flashcalw_picocache_enable | ( | void | ) |
Enable PicoCache.
References flashcalw_picocache_get_status(), and sysclk_enable_peripheral_clock().
void flashcalw_picocache_enable_monitor | ( | void | ) |
Enable PicoCache monitor.
uint32_t flashcalw_picocache_get_monitor_cnt | ( | void | ) |
Get PicoCache monitor count number.
uint32_t flashcalw_picocache_get_status | ( | void | ) |
Get PicoCache status.
Referenced by flashcalw_picocache_disable(), flashcalw_picocache_enable(), and flashcalw_picocache_invalid_line().
uint32_t flashcalw_picocache_get_version | ( | void | ) |
Get PicoCache version.
void flashcalw_picocache_invalid_all | ( | void | ) |
Invalid all PicoCache lines.
void flashcalw_picocache_invalid_line | ( | uint32_t | index | ) |
Invalid specific cache line.
index | Lines to be invalid. |
References flashcalw_picocache_get_status().
void flashcalw_picocache_reset_monitor | ( | void | ) |
Reset PicoCache monitor.
void flashcalw_picocache_set_monitor_mode | ( | uint32_t | mode | ) |
Set PicoCache monitor mode.
mode | PicoCache mode, 0 for cycle, 1 for instruction hit and 2 for data hit. |
bool flashcalw_quick_page_read | ( | int | page_number | ) |
Applies the Quick Page Read command to a page.
page_number | The page number:
|
References flashcalw_is_page_erased(), and flashcalw_issue_command().
Referenced by flashcalw_erase_page().
bool flashcalw_quick_user_page_read | ( | void | ) |
Issues a Quick Page Read User Page command to the FLASHCALW.
References flashcalw_is_page_erased(), and flashcalw_issue_command().
Referenced by flashcalw_erase_user_page().
uint64_t flashcalw_read_all_gp_fuses | ( | void | ) |
Reads all general-purpose fuses.
FLASH_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. Referenced by flashcalw_erase_all_gp_fuses(), flashcalw_erase_gp_fuse_byte(), flashcalw_read_gp_fuse_bit(), flashcalw_read_gp_fuse_bitfield(), and flashcalw_read_gp_fuse_byte().
bool flashcalw_read_gp_fuse_bit | ( | uint32_t | gp_fuse_bit | ) |
Reads a general-purpose fuse bit.
gp_fuse_bit | The general-purpose fuse bit: 0 to 63 . |
FLASH_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcalw_read_all_gp_fuses().
Referenced by flashcalw_erase_gp_fuse_bit().
uint64_t flashcalw_read_gp_fuse_bitfield | ( | uint32_t | pos, |
uint32_t | width | ||
) |
Reads a general-purpose fuse bit-field.
pos | The bit-position of the general-purpose fuse bit-field: 0 to 63 . |
width | The bit-width of the general-purpose fuse bit-field: 0 to 64 . |
FLASH_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcalw_read_all_gp_fuses(), and Min.
Referenced by flashcalw_erase_gp_fuse_bitfield().
uint8_t flashcalw_read_gp_fuse_byte | ( | uint32_t | gp_fuse_byte | ) |
Reads a general-purpose fuse byte.
gp_fuse_byte | The general-purpose fuse byte: 0 to 7 . |
FLASH_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcalw_read_all_gp_fuses().
Referenced by flashcalw_erase_gp_fuse_byte().
void flashcalw_set_all_gp_fuses | ( | uint64_t | value | ) |
Sets all general-purpose fuses with the appropriate erase and write operations.
value | The value of all general-purpose fuses as a word. |
FLASH_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. use (uint64_t)-1 instead of 0xFFFFFFFFFFFFFFFFULL to avoid compilation warning
References flashcalw_erase_all_gp_fuses(), flashcalw_error_status, and flashcalw_write_all_gp_fuses().
void flashcalw_set_flash_waitstate_and_readmode | ( | uint32_t | cpu_f_hz, |
uint32_t | ps_value, | ||
bool | is_fwu_enabled | ||
) |
Depending on the CPU frequency, on the Power Scaling mode and on the Fast Wakeup mode, set the wait states of flash read accesses and enable or disable the High speed read mode.
cpu_f_hz | The CPU frequency |
ps_value | Power Scaling mode value (0, 1) |
is_fwu_enabled | (boolean), Is fast wakeup mode enabled or not |
References FLASH_FREQ_PS0_FWS_0_MAX_FREQ, FLASH_FREQ_PS0_FWS_1_MAX_FREQ, FLASH_FREQ_PS1_FWS_0_MAX_FREQ, FLASH_FREQ_PS1_FWS_1_FWU_MAX_FREQ, FLASH_FREQ_PS2_FWS_0_MAX_FREQ, flashcalw_issue_command(), flashcalw_set_wait_state(), and UNUSED.
void flashcalw_set_gp_fuse_bit | ( | uint32_t | gp_fuse_bit, |
bool | value | ||
) |
Sets a general-purpose fuse bit with the appropriate erase and write operations.
gp_fuse_bit | The general-purpose fuse bit: 0 to 63 . |
value | The value of the specified general-purpose fuse bit. |
FLASH_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcalw_erase_gp_fuse_bit(), and flashcalw_write_gp_fuse_bit().
Referenced by flashcalw_set_gp_fuse_bitfield().
void flashcalw_set_gp_fuse_bitfield | ( | uint32_t | pos, |
uint32_t | width, | ||
uint64_t | value | ||
) |
Sets a general-purpose fuse bit-field with the appropriate erase and write operations.
pos | The bit-position of the general-purpose fuse bit-field: 0 to 63 . |
width | The bit-width of the general-purpose fuse bit-field: 0 to 64 . |
value | The value of the specified general-purpose fuse bit-field. |
FLASH_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcalw_error_status, flashcalw_set_gp_fuse_bit(), and Min.
void flashcalw_set_gp_fuse_byte | ( | uint32_t | gp_fuse_byte, |
uint8_t | value | ||
) |
Sets a general-purpose fuse byte with the appropriate erase and write operations.
gp_fuse_byte | The general-purpose fuse byte: 0 to 7 . |
value | The value of the specified general-purpose fuse byte. |
FLASH_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcalw_erase_gp_fuse_byte(), flashcalw_error_status, and flashcalw_write_gp_fuse_byte().
void flashcalw_set_security_bit | ( | void | ) |
Activates the Security bit.
References flashcalw_issue_command().
void flashcalw_set_wait_state | ( | uint32_t | wait_state | ) |
Sets the number of wait states of flash read accesses.
wait_state | The number of wait states of flash read accesses: 0 to 1 . |
Referenced by flashcalw_set_flash_waitstate_and_readmode().
void flashcalw_write_all_gp_fuses | ( | uint64_t | value | ) |
Writes all general-purpose fuses.
value | The value of all general-purpose fuses as a word. |
FLASH_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcalw_error_status, and flashcalw_write_gp_fuse_byte().
Referenced by flashcalw_set_all_gp_fuses().
void flashcalw_write_gp_fuse_bit | ( | uint32_t | gp_fuse_bit, |
bool | value | ||
) |
Writes a general-purpose fuse bit.
gp_fuse_bit | The general-purpose fuse bit: 0 to 63 . |
value | The value of the specified general-purpose fuse bit. |
FLASH_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcalw_issue_command().
Referenced by flashcalw_set_gp_fuse_bit(), and flashcalw_write_gp_fuse_bitfield().
void flashcalw_write_gp_fuse_bitfield | ( | uint32_t | pos, |
uint32_t | width, | ||
uint64_t | value | ||
) |
Writes a general-purpose fuse bit-field.
pos | The bit-position of the general-purpose fuse bit-field: 0 to 63 . |
width | The bit-width of the general-purpose fuse bit-field: 0 to 64 . |
value | The value of the specified general-purpose fuse bit-field. |
FLASH_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcalw_error_status, flashcalw_write_gp_fuse_bit(), and Min.
void flashcalw_write_gp_fuse_byte | ( | uint32_t | gp_fuse_byte, |
uint8_t | value | ||
) |
Writes a general-purpose fuse byte.
gp_fuse_byte | The general-purpose fuse byte: 0 to 7 . |
value | The value of the specified general-purpose fuse byte. |
FLASH_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcalw_issue_command().
Referenced by flashcalw_erase_gp_fuse_byte(), flashcalw_set_gp_fuse_byte(), and flashcalw_write_all_gp_fuses().
void flashcalw_write_page | ( | int | page_number | ) |
Writes a page from the page buffer.
page_number | The page number:
|
References flashcalw_issue_command().
Referenced by flashcalw_memcpy(), and flashcalw_memset64().
void flashcalw_write_user_page | ( | void | ) |
Writes the User page from the page buffer.
References flashcalw_issue_command().
Referenced by flashcalw_memcpy(), and flashcalw_memset64().
|
static |
Sticky error status of the FLASHCALW.
This variable is updated by functions that issue FLASHCALW commands. It contains the cumulated FLASHCALW error status of all the FLASHCALW commands issued by a function.
Referenced by flashcalw_erase_all_pages(), flashcalw_erase_gp_fuse_bitfield(), flashcalw_erase_gp_fuse_byte(), flashcalw_erase_page(), flashcalw_lock_all_regions(), flashcalw_memcpy(), flashcalw_memset64(), flashcalw_set_all_gp_fuses(), flashcalw_set_gp_fuse_bitfield(), flashcalw_set_gp_fuse_byte(), flashcalw_write_all_gp_fuses(), and flashcalw_write_gp_fuse_bitfield().
void(*volatile flashcalw_wait_until_ready)(void) = flashcalw_default_wait_until_ready |
Pointer to the function used by the driver when it needs to wait until the FLASHCALW is ready to run a new command.
The default function is flashcalw_default_wait_until_ready. The user may change this pointer to use another implementation.
Referenced by flashcalw_issue_command().