![]() | Subject to your compliance with these terms, you may use Microchip software and any derivatives exclusively with Microchip products |
![]() | Service (SAMV71) |
![]() | Management (SAMV71) |
![]() | This is the quick start guide for the PMC module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
![]() | This is the quick start guide for the USB device keyboard module (UDI keyboard) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
![]() ![]() | A USB Composite Device is a USB Device which uses more than one USB class |
![]() ![]() | In this use case, the USB device is used with different USB speeds |
![]() ![]() | In this use case, the usual USB strings is added in the USB device |
![]() ![]() | In this use case, the USB remote wakeup feature is enabled |
![]() ![]() | In this use case, the USB device BUS power feature is enabled |
![]() ![]() | In this use case, the USB serial strings is dynamic |
![]() | Content of XMEGA conf_clock.h: |
![]() | This is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases |
![]() ![]() | In this case we will read out the pins from one whole port and write the read value to another port |
![]() | This is the quick start guide for the PIO Driver, with step-by-step instructions on how to configure and use the driver for specific use cases |
![]() | |
![]() | This page lists several definition related to the board operating frequency |
![]() | This page lists several definition related to the board description |
![]() | This page lists definitions related to CAN0 and CAN1 |
![]() |