User Interface.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | SEQUENCE_PERIOD 150 |
Sequence process running each SEQUENCE_PERIOD ms. More... | |
Functions | |
ISR (PORTF_INT0_vect) | |
Interrupt on "pin change" from switch to do wakeup on USB Callback running when USB Host enable mouse interface. More... | |
void | ui_init (void) |
Initializes the user interface. More... | |
void | ui_kbd_led (uint8_t value) |
Turn on or off the keyboard LEDs. More... | |
void | ui_powerdown (void) |
Enters the user interface in power down mode. More... | |
void | ui_process (uint16_t framenumber) |
This process is called each 1ms It is called only if the USB interface is enabled. More... | |
void | ui_wakeup (void) |
Exits the user interface of power down mode. More... | |
void | ui_wakeup_disable (void) |
Disables the asynchronous interrupts of the user interface. More... | |
void | ui_wakeup_enable (void) |
Enables the asynchronous interrupts of the user interface. More... | |
Variables | |
struct { | |
bool b_down | |
bool b_modifier | |
uint8_t u8_value | |
} | ui_sequence [] |
#define SEQUENCE_PERIOD 150 |
Sequence process running each SEQUENCE_PERIOD
ms.
Referenced by ui_process().
ISR | ( | PORTF_INT0_vect | ) |
Interrupt on "pin change" from switch to do wakeup on USB Callback running when USB Host enable mouse interface.
Note: This interrupt is enable when the USB host enable remotewakeup feature This interrupt wakeup the CPU if this one is in idle mode
References GPIO_PUSH_BUTTON_0, ioport_pin_to_port(), and udc_remotewakeup().
void ui_init | ( | void | ) |
void ui_kbd_led | ( | uint8_t | value | ) |
Turn on or off the keyboard LEDs.
References HID_LED_CAPS_LOCK, HID_LED_NUM_LOCK, LED2_GPIO, LED3_GPIO, LED_Off, and LED_On.
void ui_powerdown | ( | void | ) |
void ui_process | ( | uint16_t | framenumber | ) |
This process is called each 1ms It is called only if the USB interface is enabled.
framenumber | Current frame number |
References b_down, b_modifier, gpio_pin_is_low, GPIO_PUSH_BUTTON_0, LED1_GPIO, LED_Off, LED_On, SEQUENCE_PERIOD, u8_value, udi_hid_kbd_down(), udi_hid_kbd_modifier_down(), udi_hid_kbd_modifier_up(), udi_hid_kbd_up(), and ui_sequence.
Referenced by main(), and main_sof_action().
void ui_wakeup | ( | void | ) |
Exits the user interface of power down mode.
References LED0_GPIO, and LED_On.
Referenced by main_resume_action().
void ui_wakeup_disable | ( | void | ) |
Disables the asynchronous interrupts of the user interface.
References GPIO_PUSH_BUTTON_0, and ioport_pin_to_port().
Referenced by main_remotewakeup_disable().
void ui_wakeup_enable | ( | void | ) |
Enables the asynchronous interrupts of the user interface.
References GPIO_PUSH_BUTTON_0, ioport_configure_pin(), IOPORT_DIR_INPUT, ioport_pin_to_port(), and IOPORT_PULL_UP.
Referenced by main_remotewakeup_enable().
bool b_down |
Referenced by ui_process().
bool b_modifier |
Referenced by ui_process().
uint8_t u8_value |
Referenced by ui_process().
struct { ... } ui_sequence[] |
Referenced by ui_process().