![]() | Common standard I/O driver that implements the stdio read and write functions on AVR and SAM devices |
![]() ![]() | Common standard serial I/O management driver that implements a stdio serial interface on AVR and SAM devices |
![]() | |
![]() | The Universal Asynchronous Receiver Transmitter features a two-pin UART that can be used for communication and trace purposes and offers an ideal medium for in-situ programming solutions |
![]() | Receiver Transmitter (USART) |
![]() | |
![]() | |
![]() | This module is the test suite framework, which provides a set of standard functions and macros for defining and running test suites |
![]() | Compiler abstraction layer and code utilities for AT91SAM |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | This is a driver for global enabling and disabling of interrupts |
![]() ![]() | |
![]() | This collection of macros identify which series and families that the various Atmel parts belong to |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | |
![]() ![]() | Generic clocks are configurable clocks which run outside the system clock domain |
![]() ![]() | This group contains functions and definitions related to configuring and enabling/disabling on-chip oscillators |
![]() ![]() | This group contains functions and definitions related to configuring and enabling/disabling on-chip PLLs |
![]() ![]() | See Quick Start Guide for the System Clock Management service (SAM4S) |
![]() | This is a stub on the SAM Power Manager Control (PMC) for the sleepmgr service |
![]() | See Quick start guide for Serial Interface service |
![]() | Transmitter (USART) |
![]() | The sleep manager is a service for ensuring that the device is not put to sleep in deeper sleep modes than the system (e.g., peripheral drivers, services or the application) allows at any given time |
![]() | See Quick start guide for the common IOPORT service |
![]() | This stack includes the USB Device Stack, USB Host Stack and common definitions |
![]() ![]() | This module includes USB Stack Device implementation |
![]() ![]() ![]() | The UDC provides a high-level abstraction of the usb device |
![]() ![]() ![]() ![]() | Internal implementation |
![]() ![]() ![]() ![]() | Common prerequisites for all USB devices |
![]() ![]() ![]() ![]() | Common example code for all USB devices |
![]() ![]() ![]() ![]() | Common workflow for all USB devices |
![]() ![]() ![]() ![]() | |
![]() ![]() ![]() | The UDD driver provides a low-level abstraction of the device controller hardware |
![]() ![]() ![]() ![]() | UDP low-level driver for USB device mode |
![]() ![]() ![]() | The UDI provides a common API for all classes, and this is used by UDC for the main control of USB Device interface |
![]() ![]() ![]() ![]() | Common library for all Human Interface Device (HID) implementation |
![]() ![]() ![]() ![]() ![]() | |
![]() ![]() ![]() ![]() ![]() | Common APIs used by high level application to use this USB class |
![]() ![]() ![]() ![]() ![]() ![]() | Structures and functions required by UDC |
![]() ![]() ![]() ![]() ![]() ![]() | Class internal implementation |
![]() ![]() ![]() ![]() ![]() ![]() | The following structures provide the USB device descriptors required for USB Device with a single interface HID keyboard |
![]() ![]() ![]() ![]() ![]() ![]() | The following structures provide predefined USB interface descriptors |
![]() ![]() | This module defines Atmel PID and VIDs constants |
![]() ![]() | This module defines constants and data structures provided by the USB 2.0 specification |
![]() ![]() ![]() | Protocol definitions |
![]() | The generic board support module includes board-specific definitions and function prototypes, such as the board initialization function |
![]() | This is the common API for GPIO |