Microchip® Advanced Software Framework

led.h File Reference

XMEGA-A3BU board LEDs support package.

This file contains definitions and services related to the LED features of the XMEGA-A3BU Xplained board.

To use this board, define BOARD=XMEGA_A3BU_XPLAINED.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include "gpio.h"

Macros

#define LED_Off(led_gpio)   gpio_set_pin_high(led_gpio)
 Turns off the specified LEDs. More...
 
#define LED_On(led_gpio)   gpio_set_pin_low(led_gpio)
 Turns on the specified LEDs. More...
 
#define LED_Toggle(led_gpio)   gpio_toggle_pin(led_gpio)
 Toggles the specified LEDs. More...
 

#define LED_Off (   led_gpio)    gpio_set_pin_high(led_gpio)

Turns off the specified LEDs.

Parameters
led_gpioLED to turn off (LEDx_GPIO).
Note
The pins of the specified LEDs are set to GPIO output mode.

Referenced by ui_init(), ui_powerdown(), and ui_process().

#define LED_On (   led_gpio)    gpio_set_pin_low(led_gpio)

Turns on the specified LEDs.

Parameters
led_gpioLED to turn on (LEDx_GPIO).
Note
The pins of the specified LEDs are set to GPIO output mode.

Referenced by ui_process(), and ui_wakeup().

#define LED_Toggle (   led_gpio)    gpio_toggle_pin(led_gpio)

Toggles the specified LEDs.

Parameters
led_gpioLED to toggle (LEDx_GPIO).
Note
The pins of the specified LEDs are set to GPIO output mode.