Microchip® Advanced Software Framework

ui.h File Reference

Common User Interface for HID Mouse application.

Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.

Functions

void ui_init (void)
 Initializes the user interface. More...
 
void ui_powerdown (void)
 Enters the user interface in power down mode. More...
 
void ui_process (uint16_t framenumber)
 This process is called each 1ms It is called only if the USB interface is enabled. More...
 
void ui_wakeup (void)
 Exits the user interface of power down mode. More...
 
void ui_wakeup_disable (void)
 Disables the asynchronous interrupts of the user interface. More...
 
void ui_wakeup_enable (void)
 Enables the asynchronous interrupts of the user interface. More...
 

void ui_init ( void  )

Initializes the user interface.

References cpu_irq_restore(), cpu_irq_save(), GPIO_JOYSTICK_PUSH, irq_register_handler, LED0, LED1, LED_Off(), and LED_On().

Referenced by main().

void ui_powerdown ( void  )

Enters the user interface in power down mode.

References LED0, LED1, and LED_Off().

Referenced by main(), and main_suspend_action().

void ui_process ( uint16_t  framenumber)
void ui_wakeup ( void  )

Exits the user interface of power down mode.

References LED0, and LED_On().

Referenced by main_resume_action().

void ui_wakeup_disable ( void  )

Disables the asynchronous interrupts of the user interface.

References eic_disable_line(), EXT_NMI, gpio_disable_pin_interrupt(), and GPIO_JOYSTICK_PUSH.

Referenced by main_remotewakeup_disable().

void ui_wakeup_enable ( void  )