Common User Interface for HID Mouse application.
Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | ui_init (void) |
Initializes the user interface. More... | |
void | ui_powerdown (void) |
Enters the user interface in power down mode. More... | |
void | ui_process (uint16_t framenumber) |
This process is called each 1ms It is called only if the USB interface is enabled. More... | |
void | ui_wakeup (void) |
Exits the user interface of power down mode. More... | |
void | ui_wakeup_disable (void) |
Disables the asynchronous interrupts of the user interface. More... | |
void | ui_wakeup_enable (void) |
Enables the asynchronous interrupts of the user interface. More... | |
void ui_init | ( | void | ) |
void ui_powerdown | ( | void | ) |
Enters the user interface in power down mode.
Referenced by main(), and main_suspend_action().
void ui_process | ( | uint16_t | framenumber | ) |
This process is called each 1ms It is called only if the USB interface is enabled.
framenumber | Current frame number |
References ioport_get_pin_level(), LED0, LED_Off, LED_On, MOUSE_MOVE_COUNT, MOUSE_MOVE_RANGE, move_count, move_dir, MOVE_DOWN, MOVE_LEFT, MOVE_RIGHT, MOVE_UP, SW0_PIN, udi_hid_mouse_moveX(), and udi_hid_mouse_moveY().
Referenced by main(), and main_sof_action().
void ui_wakeup | ( | void | ) |
Exits the user interface of power down mode.
Referenced by main_resume_action().
void ui_wakeup_disable | ( | void | ) |
Disables the asynchronous interrupts of the user interface.
References ui_disable_asynchronous_interrupt().
Referenced by main_remotewakeup_disable().
void ui_wakeup_enable | ( | void | ) |
Enables the asynchronous interrupts of the user interface.
References ui_enable_asynchronous_interrupt().
Referenced by main_remotewakeup_enable().