Declaration of main function used by HID mouse example.
Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | main_mouse_disable (void) |
Called by HID interface Callback running when USB Host disable mouse interface. More... | |
bool | main_mouse_enable (void) |
Called by HID interface Callback running when USB Host enable mouse interface. More... | |
void | main_remotewakeup_disable (void) |
Called by UDC when USB Host request to disable remote wakeup. More... | |
void | main_remotewakeup_enable (void) |
Called by UDC when USB Host request to enable remote wakeup. More... | |
void | main_remotewakeup_lpm_disable (void) |
Called by UDC when USB Host request to disable LPM remote wakeup. More... | |
void | main_remotewakeup_lpm_enable (void) |
Called by UDC when USB Host request to enable LPM remote wakeup. More... | |
void | main_resume_action (void) |
Called by UDD when the USB line exit of suspend state. More... | |
void | main_sof_action (void) |
Called when a start of frame is received on USB line. More... | |
void | main_suspend_action (void) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More... | |
void | main_suspend_lpm_action (void) |
Enters the application in low power mode Callback called when USB host sets LPM suspend state. More... | |
void main_mouse_disable | ( | void | ) |
Called by HID interface Callback running when USB Host disable mouse interface.
References main_b_mouse_enable.
bool main_mouse_enable | ( | void | ) |
Called by HID interface Callback running when USB Host enable mouse interface.
true | if mouse startup is ok |
References main_b_mouse_enable.
void main_remotewakeup_disable | ( | void | ) |
Called by UDC when USB Host request to disable remote wakeup.
References ui_wakeup_disable().
void main_remotewakeup_enable | ( | void | ) |
Called by UDC when USB Host request to enable remote wakeup.
References ui_wakeup_enable().
void main_remotewakeup_lpm_disable | ( | void | ) |
Called by UDC when USB Host request to disable LPM remote wakeup.
References ui_wakeup_disable().
void main_remotewakeup_lpm_enable | ( | void | ) |
Called by UDC when USB Host request to enable LPM remote wakeup.
References ui_wakeup_enable().
void main_resume_action | ( | void | ) |
Called by UDD when the USB line exit of suspend state.
References ui_wakeup().
void main_sof_action | ( | void | ) |
Called when a start of frame is received on USB line.
References main_b_mouse_enable, udd_get_frame_number(), and ui_process().
void main_suspend_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
References ui_powerdown().
void main_suspend_lpm_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets LPM suspend state.
References ui_powerdown().