Human interface on SAMV71-Xplained-Ultra :
This example shows how to implement a USB Device HID Mouse on Atmel MCU with USB module. The application note AVR4903 http://ww1.microchip.com/downloads/en/appnotes/doc8409.pdf provides information about this implementation.
The example uses the buttons or sensors available on the board to simulate a standard mouse. After loading firmware, connect the board (EVKxx,Xplain,...) to the USB Host. When connected to a USB host system this application provides a mouse application in the Unix/Mac/Windows operating systems. This example uses the native HID driver for these operating systems.
The example uses the following module groups: